Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

ÖBB puts first new-generation Railjet from Siemens Mobility into service and orders 19 more trains

The new-generation Railjet was developed and is being built by Siemens Mobility in Vienna and is based on the same platform used by the new Nightjet trains. ÖBB originally ordered eight trains but has now ordered an additional 19. Siemens Mobility will be delivering a total of 27 new-generation Railjets. 
Andreas Matthä, CEO ÖBB Holding: “We are delighted that we’re expanding our ÖBB long-distance fleet with 19 more new-generation Railjets. People are traveling more and many prefer to do so by train. In response to this development, which is beneficial for the environment and climate, we are increasing the number of modern trains. With the new travel experience at the Brenner Pass, we are able to further enhance the popularity of this route. The new generation of Railjets offers our passengers a truly first-class travel experience and raises rail comfort to a new level.”  
Albrecht Neumann, CEO Rolling Stock Siemens Mobility: “The new generation of Railjets with their many impressive innovations in the interior provide the highest level of comfort and convenience to passengers. By helping make rail travel more attractive, these trains will make an important contribution toward achieving climate targets. The order for 19 additional trains is a strong signal underscoring the quality and technology of Siemens Mobility.”
Special technical features
The new high-tech lightweight bogies are 30 percent lighter, provide a higher level of comfort than comparable products, and require fewer raw materials in production. They also make operation of the train more economical over its entire lifecycle since it uses less energy, particularly when accelerating and braking.
In addition, the trains have windows panes that are optimally radio-permeable for improved mobile reception. The patented windows have a special laser-beamed structure that is scarcely detectable by passengers. Developed by Siemens in Vienna, the windows conduct signal power that is 50 times stronger than standard glass. Measurements taken on an ÖBB Railjet already in service show that the available time of good 4G reception is increased by 33 percent.
Advanced digitalization technology also ensures smooth, problem-free operation of the trains: Each train continually transmits self-diagnostic data to the maintenance depot via a secure and highly reliable data link. This monitoring makes it easier to plan maintenance work, contributing to higher train availability and ultimately more satisfied passengers.
Further sustainability is achieved by increasing the train’s energy efficiency with features like LED interior lighting, an air conditioning system operating with a heat pump for both cooling and heating, and fresh air ventilation regulated according to the CO2 level of the interior air. The train’s newly developed power distribution system also makes an important contribution to efficiency: It is highly efficient in converting voltage and transporting energy within the train all the way down to the power outlets on the passenger seats.
Greater passenger comfort than ever before
Depending on their preference, passengers have a choice of seating: in compartments, in open-plan cars, or in raised seating areas with slightly higher seat heights. Passengers preferring a quieter ride can sit in designated quiet zones, while families can use the family zones with game board tables. Seat backrests without gaps provide greater privacy between the seat rows, so passengers can, for example, work on their laptops undisturbed. WiFi service is offered throughout the train, and a clear, state-of-the-art passenger information system is provided on ceiling-mounted displays and other screens.
Passenger comfort is further enhanced by an interior lighting concept that automatically adjusts to the time of day. Both the light color and the temperature of the compartments can be individually adjusted.
The new double seats are equipped with folding center armrests, allowing them to be converted into a small sofa if capacity is available. Each seat row is also equipped with three charging options: a USB port, wireless NFC charging, and a 230-volt power outlet. Luggage can be stored securely and unattended in spaces accessed via NFC or individual numerical codes.
For passengers with limited mobility, the train has three wheelchair spaces and barrier-free access via a platform-level, extra-wide entrance in the multifunctional car. Space for storing skis and snowboards is available in the multifunctional car as well, along with six bicycle spaces.

For this press release

Siemens Mobility is a separately managed company of Siemens AG. As a leader in intelligent transport solutions for more than 175 years, Siemens Mobility is constantly innovating its portfolio. Its core areas include rolling stock, rail automation and electrification, a comprehensive software portfolio, turnkey systems as well as related services. With digital products and solutions, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2023, which ended on September 30, 2023, Siemens Mobility posted revenue of €10.5 billion and employed around 39,800 people worldwide. Further information is available at: www.siemens.com/mobility
Read more
Reference Number: HQMOPR202403216898EN

Contact

Eva Haupenthal

Siemens Mobility GmbH

+49 (152) 01654597