Sabrina Soussan (48) and Michael Peter (51) have been appointed to succeed Jochen Eickholt (55) as head of Siemens' Mobility Division, effective October 1, 2017. Eickholt has been appointed integration manager for the announced merger of Siemens' and Alstom's mobility businesses, effective the same date.
Distributed energy systems and digitalization are two trends that reinforce one another and are driving the transformation of the energy world. Siemens is supporting these trends in a variety of ways, including with MindSphere, its cloud-based, open, and scalable operating system for the Internet of Things (IoT). At this year's European Utility Week (EUW), which took place in Amsterdam from October 3 to 5, Siemens presented some of its highlights for this topic. As in past years, Siemens once again invited German and international energy media to a press conference at the trade show. The conference focused on the EnergyIP smart grid application platform whose applications recently began running under MindSphere as well as a new MindSphere application developed by Omnetric, a joint venture of Siemens and Accenture, for an Austrian energy provider.
At the conference, Siemens informed industry media about how MindSphere can help utilities and power grid operators monitor their grids, analyze grid data, and optimize grid operation, and also presented a new controllable and adjustable medium-voltage DC transmission system. This system was developed for gird operators who need to enlarge their infrastructure to handle the increasing volumes of power fed into the distribution system from distributed and renewable energy sources and to keep their network stable.
- Siemens to supply power island with highly-efficient H-class gas turbines
- Around 1.3 gigawatts power generation capacity
- Fast track power generation project to boost capacity in Punjab Province
Siemens has received an order from Pakistan for a complete power island for the new combined cycle Punjab Power Plant Jhang. The order was placed by the China Machinery Engineering Corporation (CMEC). As EPC contractor the Chinese company is building the project for the independent energy provider Punjab Thermal Power (Pvt) Ltd (PTPL). The liquefied natural gas (LNG)-operated plant is being built 250 kilometers southwest of Lahore and will provide a power generating capacity of 1.3 gigawatts.
In many areas of the world, existing power infrastructure is stretched to the limit by growing demand for electricity. Reliable power supply systems are a major enabler of economic development, yet needs are growing at a pace faster than the ability to erect conventional power plants. The task at hand in these regions is to deploy efficient mobile power generating capacity quickly to fuel economic development. In some cases the need is temporary, and after some time the mobile power plant might be relocated to a different location to perform a similar duty.
Siemens has now specially developed its SGT-A45 TR gas turbine for this rapidly growing market – a new aero-derivative gas turbine integrated into a mobile unit that delivers an electrical output of up to 44 megawatts, can be installed and commissioned in less than two weeks and begin generating electricity immediately. This light-weight gas turbine offers outstanding power density, high fuel efficiency and good operational flexibility, making it an ideal choice for customers who urgently need power and regions with less developed infrastructures.
- Digitalization of low-flow measurement
- Sensor program expansion with DN100 and DN150
- Transmitter with Modbus and Profibus PA profile 4.0 communication
- Suitable for new applications in oil and gas, marine, and chemical
To extend the numerous process-optimizing advantages of the digital Coriolis flowmeter platform to low-flow applications such as batching, dosing and filling of both liquids and gases, the Sitrans FCT030 and FCT010 digital transmitters can now be paired with the Sitrans F C MASS 2100 and Sitrans FC300 Coriolis sensors for small line sizes from DI 1.5 to DN 15. With this major enhancement to the product line, a broad range of users from chemical to automotive applications can benefit from market-leading mass flow accuracy of 0.1%, density accuracy of 0.5 kg/m3 and 100 Hz signal processing. The high-speed update rate ensures the highest precision for applications such as the filling of beverage bottles.
- Signed Memorandum of Understanding grants exclusivity to combine mobility businesses in a merger of equals
- Listing in France and group headquarters in Paris area; led by Alstom CEO with 50 percent shares of the new entity owned by Siemens
- Business headquarter for Mobility Solutions in Germany and for Rolling Stock in France
- Comprehensive offering and global presence will offer best value to customers all over the world
- Combined company's revenue €15.3 billion, adjusted EBIT of €1.2 billion
- Annual synergies of €470 million expected latest four years after closing
Today, Siemens and Alstom have signed a Memorandum of Understanding to combine Siemens' mobility business including its rail traction drives business, with Alstom. The transaction brings together two innovative players of the railway market with unique customer value and operational potential. The two businesses are largely complementary in terms of activities and geographies. Siemens will receive newly issued shares in the combined company representing 50 percent of Alstom's share capital on a fully diluted basis.
China's largest acrylic producer, Zhejiang Satellite Energy Co., Ltd, recently selected Siemens to provide a reactor effluent compressor train for Phase II of its propane dehydrogenation (PDH) plant in Pinghu City in China's Zhejian province. The dual-casing compressor train, scheduled for installation in late 2018, consists of two Siemens STC-SH single-shaft compressors driven by a Siemens SGT-750 industrial gas turbine. Plant commissioning is scheduled for early 2019.
- Digitalization allows machine manufacturers to develop new business models
- Openness of MindSphere has an important role to play for machine manufacturers
- Siemens connects 240 machine tools with "Manage MyMachines" on MindSphere across the whole exhibition site
At the EMO 2017, Siemens is demonstrating the various connection and installation options of its high-performance and open cloud-based IoT operating system MindSphere for applications in the machine tool sector. The company is connecting over 240 different machine tools from over 140 manufacturers across the whole exhibition site using its "Manage MyMachines" app on MindSphere. In addition to this, machine manufacturers such as Heller are presenting new services and business models based on MindSphere to, for example, increase efficiency and productivity.
- System offers data transmission rates of up to 2.5 megabit per second
- Replaces traditional systems and can be seamless integrated into existing power line carrier infrastructure
Siemens launches PowerLink IP, a new power line carrier (PLC) system for digital high-voltage substations. This brand new PLC system uses the high-voltage lines between the substations as a channel by overlaying a modulated carrier frequency on the frequency of the transmission voltage in the overhead lines. State-of-the-art, digital substations generate ever-increasing volumes of data that are used to ensure reliable network operation. With PowerLink IP, power grid operators can enjoy the benefits of digitalization for Ethernet/IP communication via overhead lines. Siemens provides proven PLC technology for this purpose – technology which meets the demand for more bandwidth and ensures that the constantly growing volumes of data in high-voltage substations can be used for efficient grid operation.
- Greatly expanded product line of GAMMA instabus switching actuators for lighting and electrical loads
- Numerous control, override and diagnostic functions
- Much shorter installation time, simplified commissioning, lower maintenance costs
The Siemens Building Technologies Division has updated its GAMMA instabus product line with new switching actuators, greatly expanding its range of products for lighting control. The new actuators are available with switching capacities of 6, 10 and 16 or 20 amperes and four, eight and twelve channels each.