As part of formnext 2017, the leading exhibition for additive manufacturing, Siemens presented its comprehensive solution portfolio for consistent digitalization of additive manufacturing, starting with the design and engineering software, via innovative simulation tools to complete machine and factory automation. In addition to this, Siemens demonstrated how the industrialization of additive manufacturing can be further accelerated by using innovative added value services.
- Expanded software toolset integrates additive manufacturing, machining, robotics and quality inspection to digitalize part manufacturing
- Advanced automation capabilities connect end-to-end processes bringing machine shops greater efficiency and shorter time to job delivery
- NX Machining Line Planner uses a digital twin of the complete machining line to optimize high-volume production for complex parts
The latest version of Siemens' NX™ software unites the next generation of tools for additive manufacturing, computer numerical control (CNC) machining, robotics and quality inspection to enable the digitalization of part manufacturing within a single, integrated, end-to-end system. Advanced automation capabilities for computer- aided manufacturing (CAM), including robotic programming, adaptive milling, and tooling design, provide innovative, industry-specific technology to help deliver high- quality products to the market in less time. The new NX Machining Line Planner tool, combined with integrated NX CAM software for feature-based machining, provides new capabilities for industries with high-volume production of complicated parts, such as automotive and industrial machinery. The latest version of NX continues to support end-to-end solutions for additive manufacturing, helping manufacturers realize the goal of using 3D printing for industrial production.
- Industrial Ethernet switches in electrical and optical version
- Direct (24 V) and alternating (24 V) current for industry and building use
- Up to 24 electrical ports for connecting a large number of nodes
- Profinet CC-A conformity ensures reliable data transmission
With its Scalance XB-100 product line, Siemens is launching a new generation of compact unmanaged Industrial Ethernet switches designed to permit the configuration of electrical and optical line and star topologies in networks. This range of switches is particularly suited for use in industry and in building automation applications. Design features include a large number of ports and interfaces, a lightweight plastic enclosure, and a compact design making it ideal for control cabinet mounting. The switches are also approved for use in potentially explosive atmospheres (ATEX Zone 2, IECEx). As unmanaged switches with no pre-configuration, the Scalance XB-100 products are suitable for immediate use, and come with Profinet CC-A conformity to ensure the reliable transmission of Profinet data.
- Scalance SC-600 Industrial Security Appliances – offers protection at the cell level
- Stateful Inspection Firewall with data throughput of 600 Mbit/s
- Configuration via web server, TIA Portal, SNMP and CLI
- Secured remote maintenance in combination with Sinema Remote Connect
Siemens is extending its portfolio offering protection against attacks on software and hardware components at the industrial cell level: The new Scalance SC-600 Industrial Security Appliances have a firewall (Stateful Inspection Firewall) with a data throughput of up to 600 Megabits per second (Mbit/s). Depending on the variant users can also administer VPN tunnels up to 200 IPsec (Internet Protocol Security). Scalance SC-600 also provides convenient options for network structuring via virtual LANs (VLAN) and Network Address Translation (NAT/NAPT). The Scalance SC-600 is configured via the integral web server using the Simple Network Management Protocol (SNMP), Command Line Interface (CLI) or the Step 7 V15 engineering software (TIA Portal). For secured remote access, the new industrial security appliances can be connected via the Sinema Remote Connect management platform.
- New version of the TIA Portal V15 engineering framework with emphasis on applications, digitalization portfolio and engineering efficiency
- Applications enhanced with high-level language programming, integration of additional drive systems and handling functions
- Widening of the digitalization portfolio to include OPC UA functionalities and virtual commissioning
- Standardization and higher engineering efficiency with teamwork, as well as expanded diagnostics of machines and systems
With the new version of the TIA Portal V15 (Totally Integrated Automation Portal), Siemens is extending its engineering framework to include a range of new practical digitalization functions to shorten engineering times. The main features of the innovations are extension of the application possibilities, expansion of the digitalization portfolio, standardization and higher engineering efficiency.
We released our fourth quarter results and preliminary figures for fiscal year 2017 on November 9, 2017. The Press Conference and the Analyst Call were broadcast live.
- Thomas Rathmann leaves company
- Preparations for public listing on schedule
Jochen Schmitz (51) has been appointed CFO of Siemens Healthineers, effective December 1, 2017. Schmitz, who is currently head of Accounting, Reporting and Controlling for the Siemens Group, will succeed Thomas Rathmann, who is leaving Siemens Healthineers by mutual agreement.
- Revenue rose 4%, to €83.0 billion; orders were strong at €85.7 billion, just 1% below the high level a year ago despite substantial, ongoing contraction in markets for the Power and Gas Division which recorded large orders in Egypt totaling €4.7 billion in the prior year; the book-to-bill ratio was 1.03
- On a comparable basis, excluding currency translation and portfolio effects, revenue rose 3% and orders declined 2%
- Industrial Business profit rose 8%, to €9.5 billion, with double-digit increases at Building Technologies, Digital Factory, Mobility and Process Industries and Drives more than offsetting declines at Power and Gas and Siemens Gamesa Renewable Energy (SGRE)
- Industrial Business profit margin reached 11.2%, with a majority of businesses within or above their target ranges
- Net income up 11%, to €6.2 billion, driven by the strong operating performance; basic earnings per share (EPS) of €7.44, well within the guidance range
- Siemens proposes to raise the dividend €0.10 per share, to €3.70 per share
"Our global team delivered excellent results in fiscal 2017, surpassing even the historic success of last year. Most businesses are stronger than ever and well equipped for the digital age. Nevertheless, we have to tackle structural issues in some individual businesses. There is a lot of work ahead of us in fiscal 2018. We will take advantage of our opportunities in the market and handle challenges carefully, responsibly and rigorously."
- Demonstration running in California near two largest U.S. Ports of Los Angeles and Long Beach
- Siemens truck electrification technology has potential to reduce emissions and improve air quality
Siemens and the "South Coast Air Quality Management District (SCAQMD)" are running a one-mile, zero-emission eHighway demonstration in the Californian city of Carson, U.S., near the ports of Los Angeles and Long Beach. Three trucks hauling freight are running along the stretch of highway which uses Siemens technology to electrify select highway lanes via an overhead catenary system. This catenary system supplies the trucks with electric power, similar to how modern-day trolleys or streetcars are powered on many city streets. The system also allows for truck operation outside of the electrified sections of infrastructure.
- New Booksize Motor Modules for Sinamics S120 series
- Version with double (C-type) and triple (D-type) overload factor
- 24A devices close portfolio gap between 18A and 30A
- New variants offer compact design and higher maximum current
The Booksize Motor Module portfolio has been further developed to include compatible new C and D type Sinamics S120 Booksize Motor Modules. Siemens has added a number of new devices to the existing 3A-30A range. The 24A, 45A and 60A Motor Modules are now available with double overload factor (Continuous C-type), and the 24A modules are additionally available with triple overload factor (Discontinuous D-type). With a 33 percent narrower fit than the existing variants, the new 45A und 60A devices are extremely compact, enabling significant space savings in the control cabinet. The maximum current in the 45A devices has also been increased from 85A to 90A, while the 60A devices now come with a 120A maximum current instead of the previous 113A.A completely new addition to the series are the 24A devices, which will be available as either a C or D type. This closes the gap in the portfolio between 18A and 30A.