- New Safety Library (3.0) for faster commissioning and compatibility with a wider range of Simatic-S7 controllers
- Advanced Position Control (APC) function for faster positioning
- New Simotics S-1FG1 servo-geared motors in upper and lower output range
- Cut in energy costs by optimized motion control
Siemens has upgraded its TÜV-certified Safety Library developed specifically for use with storage and retrieval systems. The benefits of Safety Library V3.0 for users include faster commissioning and compatibility with a wider range of failsafe Simatic controllers (from S7-1516F). Boosting the speed of storage cycles are two functions: Vibx (Vibration Extinction) and the more advanced new function Advanced Position Control (APC). APC also requires no additional sensors or actuators, and ensures the permanent prevention of mast vibrations. APC even kicks in under continuously changing vibration conditions, caused for instance by different loading conditions or variable disturbance factors such as wind. Supplementing this function are new additions to the Simotics S-1FG1 portfolio. In the upper output range, external fans now permit highly dynamic traversing processes, allowing a significantly more dynamic configuration of traversing motors. A new Simatic module for energy-optimized traversing enables energy savings despite the improved dynamic performance.
- Siemens implements autonomous stockyard management system in China
- Autonomous stockyard management system combines five automation systems
- Interaction of all components enables control of machines and conveyors
- Improved system efficiency, production capacity and security coupled with lower operating costs
Siemens is supplying an autonomous stockyard management system to be used in a new plant for HBIS Laoting Steel Co. Ltd., a Chinese subsidiary of one of the world's biggest iron and steel producers. The autonomous stockyard management system from Siemens comprises of a material tracking and management system (MAQ), an autonomous stockyard operating system (MOM), a Simatic PCS 7 process control system, industry network, consulting, engineering, project management and commissioning. Interaction between these different components enables control of all the plant's machines and conveying systems, it offers wide-ranging benefits such as the capability for all machines and conveyors to be controlled from a single system. This is achieved using a 3D model of the existing inventory which provides information on the volume and quality of stocked material, enabling autonomous operation of all the plant's storage and retrieval machines. This allows HBIS Laoting Steel Co. Ltd. not only to drive down its operating costs, but also to achieve between a five and ten percent improvement in system efficiency and between three and seven percent higher production capacity. The use of autonomous storage and retrieval machinery also improves safety.
- Bridge Firewall to protect flat networks
- Protection of Service Bridge and other applications
- User-specific firewall for individual protective measures
- Configuration now also possible in the new Sinec NMS management software
Siemens has extended the Scalance SC-600 Industrial Security Appliances to include more functionality for even better and simpler protection of production networks. The devices now have a Bridge Firewall, support redundant network structures, and allow user-specific firewalls. This enables users to increase the availability of their production while also reducing the procurement costs of network components.
Under the motto "Industrialize Additive Manufacturing" Siemens presented its comprehensive solution portfolio for consistent digitalization of additive manufacturing at the formnext 2018, the leading exhibition for additive manufacturing. Starting with the design and engineering software, via innovative simulation tools to complete machine and factory automation, Siemens demonstrated how the industrialization of additive manufacturing can be further accelerated. Furthermore Siemens introduced solutions around peripheral processes, such as automated support removal, surfaces finishing and part removal as well as post processing for intelligent de-powdering solutions. Additional, Siemens presented new business models, which have derived from digitalization in this industry.
- Sidrive IQ improves drive systems along the entire life cycle up to the megawatt range
- Cloud-based application based on networked drive systems from Siemens
- Increased productivity, reliability and ease of maintenance
- Standardized link enabled by Sinamics Connect 500 and Simotics Connect 600 connectivity modules
Sidrive IQ from Siemens provides a digital platform enabling the evaluation and utilization of data gathered from drive systems. On the basis of networked drive systems from Siemens, this cloud-based application is now also available for motors and converters in the medium and high-voltage range. This opens up an array of benefits for plant and machine operators, from optimized maintenance activity and maximum availability to increased productivity, from low outputs through to the megawatt range across the entire life cycle. Connectivity modules such as Simotics Connect 600 and Sinamics Connect 500 enable high-voltage motors and medium-voltage converters to be simply linked up to Sidrive IQ. With the latest generation of its Remote Services and Condition Monitoring Services offered as part of the Sidrive IQ Services portfolio, Siemens is making available corrective measures for fixing faults, preventive maintenance offers and proactive services for optimized performance. The optimized drive systems are used in pumps, fans and compressors across different sectors of industry such as oil and gas, mining, food and beverage, water and wastewater, metals and cement.
The AMB, the International Exhibition for Metalworking, was open from September 18 to 22, 2018 in Stuttgart. Under the motto "Digitalization in Machine Tool Manufacturing - Implement now!", Siemens demonstrated to users and manufacturers of machine tools how end-to-end digitalization solutions work from the machine tool right up to the corporate management level and the cloud.
From September 4 to 7, Siemens was at SMM under the banner "Welcome to the Digitalization at Marine – implement now," with an exciting presentation showcasing the entry of digitalization into its marine portfolio. At Booth 318 in Hall B6, Siemens exhibited its broad spectrum of drive technology, automation and digitalization services and solutions for shipbuilding and marine operations. Highlights of this year's trade fair presentation included a virtual reality representation of the Siship as well as the smart web-based data application Siship EcoMAIN. Siemens also featured integrated solutions for the (partial) electrification of ships using uniform topology with the latest members of its Siship BlueDrive Family. As well as moving over functional features familiar from Siship EcoProp under the name Siship BlueDrive Eco, Siemens also offered visitors a glimpse into its own battery production and presented a partner in the field of fuel cell-based power supplies for the commercial sector.
Siemens exhibited at the automatica 2018 with an array of integrated and user-oriented Digital Enterprise solutions designed to sharpen the competitive edge of both end users and machine builders. Exhibiting under the banner "Digital Enterprise – Implement now!", Siemens focused on ways in which industrial enterprises of all sizes can benefit from the digital transformation – along the entire value chain from product design and production planning through the engineering process to new services.
World Forum and Leading Show for the Process IndustriesUnder the motto "Accelerate the digital transformation – from integrated engineering to integrated operations." we presented at the Achema 2018 trade show specific applications for how to use the potential of digitalization to enhance efficiency, flexibility, and quality – and to shorten time to market. Production can be significantly optimized and made more flexible by integrating all components in instrumentation and control and management systems and by intelligently using all of the process data generated in a common data model – the digital twin of the overall plant. Maintenance effort and costs can also be slashed dramatically by using cloud-based applications and data-based services.