Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release15 November 2018Process Industries and DrivesNuremberg
Industrial Security Appliances with extended functionality for even better network protection

The new Scalance SC-600 Industrial Security Appliances.
The Bridge Firewall allows devices to be used in flat networks. Furthermore, not only Layer 3 but also Layer 2 data can now be filtered. This enables users to securely access automation components in Profinet cells for maintenance purposes, for example. Industrial Security Appliances can be used with the Service Bridge (a correspondingly configured Industrial Ethernet switch from the Scalance XC-200 product line) as well as with other applications.
The devices can also be integrated into redundant network infrastructures. Supporting two redundancy protocols for Layer 2 and Layer 3 eliminates the need for additional switches on the security transitions. The Media Redundancy Protocol (MRP) enables the SC-600 to be integrated on the Layer 2 level as Profinet devices in the Profinet ring redundancy without needing an additional managed Industrial Ethernet switch. In the event of a ring break, all network components in the ring switch to the redundant path within 200 ms and thus avoid a production stoppage in the event of a fault. Furthermore, the support of the Virtual Router Redundancy Protocol (VRRP) allows redundancy on Layer 3. This enables users to group the Scalance SC-600 together with other routers in the network in one logical group. If the router defined as the master fails, another router in the logical group takes over the function of the default router. The network consequently continues to communicate reliably.
The third innovation is support for user-specific firewalls. Specific firewall rules allow not only device-specific but also user-specific filtering of the data. This enables users to assign differing rights. Users consequently benefit from easier access management for network components.
Support of all device versions in the new Sinec NMS network management software allows the complete, uniform configuration of all the Scalance network components on a management platform. Use of the digital input together with the signaling contact allows, for example, the activation and deactivation of the VPN tunnel via the management platform for remote networks, Sinema Remote Connect.
Additional information on the topic of Industrial Security Appliances is available at: www.siemens.com/scalance-s
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
David Petry
Siemens AG
Werner-von-Siemens-Str. 65
91052 Erlangen
Germany
91052 Erlangen
Germany
+49 (9131) 7-26616