The VAG Verkehrs-Aktiengesellschaft Nuremberg has ordered 27 type G1 four-car metro trains from Siemens Mobility. The contract also includes an option for a total of a further 7 trains. These trains are earmarked for service on Nuremberg's U1 line. The trains will be built in the Siemens Mobility plant in Vienna. Core components of the G1 will be manufactured in the Nuremberg metropolitan area and include such products as the drive converters, traction motors, auxiliary converter units and control equipment. The project management, development and service support will be provided from Erlangen.
- Sydney Coordinated Adaptive Traffic System (SCATS) Certification
- Supports cutting-edge intelligent infrastructure
- Certificate given at ITS World Congress
Siemens Mobility’ traffic light controller “Sitraffic sX” is certified as compatible with the urban traffic control system SCATS (a registered trademark Sydney Coordinated Adaptive Traffic System). New South Wales’ agency for road infrastructure and owner of the registered trademark SCATS system, Road and Maritime Services (RMS), has granted Siemens the certification after a substantial period of integration development and testing. The Compatibility Certificate confirms that Siemens Mobility’s “Sitraffic sX” traffic light controller has been tested and evaluated by RMS to functionally operate with SCATS. The official hand-over of the Certificate from RMS to Siemens Mobility took place during a ceremony at the 26th ITS World Congress 2019 in Singapore at Siemens Mobility booth.
- 25 multisystem Vectron MS locomotives for maximum flexibility
- Cross-border operations on the North-South Corridor
- Deliveries begin at the end of 2020
The Swiss rail freight company BLS Cargo has ordered 25 Vectron MS locomotives from Siemens Mobility for planned operation on the North-South Corridor. They will be used in Germany, Austria, Switzerland, Italy, the Netherlands and Belgium. Delivery of the locomotives will be carried out in several phases from the end of 2020 to 2025. With this order, the Vectron fleet operated by BLS Cargo will grow to a total of 40 locomotives. The company previously ordered 15 locomotives from Siemens Mobility in 2015.
With growing populations, cities are becoming increasingly congested, with more traffic and longer commutes. Efficiency and safety of road traffic remain top priority for many cities. By offering autonomous shuttle systems, public transport operators and cities seek to draw passengers and make public transport more attractive. At the ITS World Congress in Singapore, Siemens Mobility is examining how Singapore is transforming its transportation ecosystem, delivering an outlook on intelligent traffic systems (ITS) projects within the Asia-Pacific region as well as showcasing advances in autonomous mobility coming to life at the CETRAN test facility.
- Shared Autonomous Mobility solutions being piloted at CETRAN
- Mobility Operating Systems for Urban Centers
- Artificial Intelligence (AI) for traffic scenarios
Siemens Mobility is showcasing the latest in intelligent traffic systems technology at this year’s ITS World Congress taking place in Singapore. This includes mobility operating systems that are helping reduce gridlock on urban streets, which centralize and control traffic throughout urban areas. By connecting road users to road and infrastructure data captured via smart structures, drivers can optimize their routes and reduce their environmental impact. Through data analysis and prediction, traffic can be regulated in an efficient manner.
- Portfolio serving entire power range from 50 to 600 kW
- Flexible combination with connection options as cable and pantographs
- For fast and secure charging at the depot and en route
- Cloud-based control and monitoring of charging processes
At Busworld 2019, Siemens is presenting its Sicharge UC family for charging electric buses, trucks and duty vehicles at the depot and en route. The Sicharge UC charging system covers the entire power range from 50 to 600 kilowatts (kW) and can be combined with several connection options such as charging plugs and offboard or onboard pantographs. To meet growing demands from the vehicle industry for higher voltages, the station can operate at up to 1,000 volts (V). Electric vehicles with various technologies and batteries can therefore be charged flexibly, either en route or at the depot. The charging processes can be monitored and controlled via a MindSphere application. MindSphere is the cloud-based, open IoT operating system from Siemens.
- Latest advances in depot charging for eBuses and eTrucks to be tested in real-life conditions at the “VDL Charging Test Center” in The Netherlands
- Collaboration to demonstrate how vehicle technologies, energy storage and charging systems work together
- Vehicle-to-grid function enables bidirectional charging
- Capacity can be flexibly combined through special switching matrix
As the number of electric vehicles in the market continues to grow, so do the requirements for a robust charging infrastructure. Recognizing the need for electric buses and trucks to be charged flexibly and efficiently, Siemens and VDL Bus & Coach (VDL), a Dutch bus manufacturer, have joined efforts to come up with innovative solutions for depots. At the VDL Charging Test Center Siemens has installed the latest generation of fast charging stations, combined with a battery storage system. The location is VDL’s interoperability test and validation center in Valkenswaard in The Netherlands. A special switching matrix allows to flexibly combine the capacity of the charging stations. The setup is managed via an energy management application running on MindSphere, the cloud-based, open IoT operating system from Siemens. VDL will use this technology to conduct interoperability and function tests on electric vehicles such as buses and trucks. Interoperability is when technologies of different manufacturers – on the vehicle as well as the charging infrastructure side – can interact and exchange information
- Digital twin of Downtown Line’s signalling system
- Supports troubleshooting, testing and training
- Intelligent infrastructure will minimize service disruptions
Siemens Mobility has been awarded a contract by the Singapore Land Transport Authority (LTA) to design and establish a simulation center for the Downtown Line’s (DTL) signalling system. The center will enable in-depth and faster technical analysis surrounding signalling-related incidents, enhance testing of new signalling features and system functionalities before deployment as well as increase capabilities for training LTA and the operator’s technical staff.
The new Bauhaus Museum Dessau (Germany) opened its doors in September 2019, featuring technology from Siemens Smart Infrastructure to help keep visitors and its extensive collection safe. A comprehensive solution for safe electrical installations extends throughout the museum’s 5,500 square meter footprint, which includes over 1,000 exhibits from the Bauhaus Dessau Foundation’s collection. The latter comprises 49,000 objects, making it the second-largest Bauhaus collection worldwide. It contains numerous student works and teaching documentation, as well as drafts and prototypes from the workshops of the renowned art academy, which celebrates its 100
th anniversary this year.