Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release09 October 2019Smart InfrastructureZug (Switzerland)
Siemens ensures safe electrical installation at the new Bauhaus Museum Dessau

Siemens Smart Infrastructure’s installation includes 17 Alpha distribution boards equipped with residual current protective devices (RCCBs) and miniature circuit breakers (MCBs), plus a total of 257 arc fault detection devices (AFDDs) from its Sentron portfolio. The protection devices prevent electrical accidents and fires, keeping the extremely valuable exhibits at Bauhaus Museum Dessau from harm.
“Insufficiently protected electrical systems can have devastating effects – also, and above all, in museums housing irreplaceable artefacts. To be on the safe side, we implemented an integrated solution from Siemens with the very latest protection devices,” said Frank Assmann, head of the construction department of the Bauhaus Dessau Foundation.
This protection concept from Siemens includes devices to prevent electrical accidents, system downtimes and power outages, as well as arc fault detection devices. Unlike RCCBs and MCBs, AFDDs detect not only parallel but also serial arcing faults. Serial arcing faults are one of the most common causes of electrical fires. These can occur due to damaged cable insulation, crushed cabling, bent connectors or loose contacts in the electrical installation. The result is rapid overheating, which can ultimately spark a cable fire and consequently lead to a fire in the building. Arc fault detection devices significantly increase the safety of people and assets. Based on Siemens' patented SIARC detection technology, the devices continuously measure the high frequency noise of voltage and current for their intensity and duration and the gaps between them. An integrated micro controller analyzes these signals and triggers the disconnection of the connected circuit within fractions of a second if anything unusual is detected.
The technical implementation of the electrical installation solution at the new Bauhaus Museum Dessau was handled by Elektro Schulze GmbH Dessau, and Schaltanlagenbau Förderstedt GmbH Güsten, Germany.
For further information and official press pictures of the Bauhaus Museum Dessau, please see
www.bauhaus-dessau.de/en/press
For further information on Siemens Smart Infrastructure, please see
www.siemens.com/smart-infrastructure
For further information on safe electrical installation, please see
www.siemens.com/protection-concept
www.bauhaus-dessau.de/en/press
For further information on Siemens Smart Infrastructure, please see
www.siemens.com/smart-infrastructure
For further information on safe electrical installation, please see
www.siemens.com/protection-concept
For this press release
Social Media
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and has around 71,000 employees worldwide.
Siemens AG
(Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at
www.siemens.com
.
Contact
Heidi Fleissner
Smart Infrastructure
Siemensstr. 10
93055 Regensburg
Germany
93055 Regensburg
Germany
+49 (941) 790-2212