First call for 70 trains from the 2023
framework agreement
Order worth more than €800 million
Consistent development of the Mireo
platform
Austrian Federal Railways (ÖBB) has ordered the first 70
trains from the framework agreement won by Siemens Mobility at the end of
summer 2023. The trains will be delivered in three different versions from late
2027 onwards. The trains are a further development of the in Europe successfully
established and proven Mireo electric multiple-units. Designed to operate at
speeds up to 160 km/h, the Mireos offer numerous amenities for passengers,
including air conditioning, WiFi service, barrier-free access, electrical plugs,
racks for skis and snowboards, capacity for buggies and wheelchairs near the
doors as well as space for bicycles. The cars will be wider than on previous
Mireos trains to further enhance the passenger experience of ÖBB customers.
And, for the first time, Siemens Mobility is designing the new trains with
inner bearing bogies as a single car concept.
Today, Siemens
Mobility – in partnership with RATP and d’Île-de-France Mobilités – announced
completion of the full automation of Paris Metro Line 4, which is now operated
exclusively using automatic driverless trains. Following a period of mixed
operation during which driver-operated trains ran alongside the automatic
trains, full automation of Line 4 is now a reality. As a leader in the
design and implementation of automated metro systems, Siemens Mobility was
chosen by RATP at the end of 2015 to automate Line 4, three years after the
successful project to automate Line 1 at the end of 2012. With 700,000
passenger each day, Line 4 is the French capital’s second busiest metro line.
Opened in 1908, the route now has 29 stations spread over 14 kilometers.
- Siemens and Salesforce are collaborating to help manufacturers increase service efficiency and create new revenue streams
- Teamcenter Service Lifecycle Management (SLM) app connects Siemens’ leading Teamcenter Product Lifecycle Management (PLM) with Salesforce Manufacturing Cloud and Service Cloud, enabling integrated, cross discipline collaboration that drive digital transformation
- The new AI-based SaaS integration helps manufacturers build feedback loops between service execution and product development, enabling continuous innovation
Siemens Digital Industries Software announced today the new
Teamcenter® SLM app on Salesforce AppExchange. Developed by Siemens in collaboration with
Salesforce, the app connects product engineering and product service operations
by bringing together the Teamcenter Service Lifecycle Management solution from
the Siemens Xcelerator portfolio of industry software with Salesforce Manufacturing Cloud and Salesforce Service Cloud. This new app enables manufacturers to adopt more
service-centric business models, improve the customer experience and increase
service revenue.
- New V6 software generation with new functions like a single positioner to reduce the load of the controller, and EtherNet/IP to allow third-party controllers to be connected
- Simulation via DriveSim Advanced enables virtual commissioning in advance, ensuring drive process requirements are met efficiently and cost-effectively
- New hardware architecture with functional enhancements like a second encoder interface and 3C3 (H2S and SO2) coating increases precision and robustness
Siemens is innovating the well-established Sinamics S210 servo drive system with a new hardware architecture and new V6 software generation that expand the system's range of applications. The servo drive system is especially suitable for applications with high dynamics in the power range between 50 W and 7 kW: for example, machines for packaging, pick & place applications, and digital printing.
Siemens Mobility and Finnish rolling stock owner company Pääkaupunkiseudun Junakalusto Oy have agreed to test the European Train Control System ETCS in Finland. It is part of the Finnish DigiRail
project and is funded by the Finnish Transport Infrastructure Agency
(Väylävirasto).The contract includes equipping two multiple-unit trainsets with
Trainguard OBU and ATO. This marks the first time that ETCS will be tested in
the Scandinavian country in accordance with the latest standard set in the
applicable European technical specification TSI 2023.
- Together with customers and partners including Sony, AWS, Red Bull Racing, Unlimited Tomorrow, and Blendhub, Siemens highlights how technology is transforming the everyday
- Siemens partners with Sony to introduce new solution for immersive engineering that combines Sony head mounted display with Siemens Xcelerator software
- AWS and Siemens to make generative AI more accessible to application developers through combination of AWS Bedrock and Mendix Low-Code platform
- Siemens enhances Siemens Xcelerator open business platform with new capabilities to combine real and digital worlds and drive digital transformation across industries
Siemens
unveiled innovations that are combining the real world and the digital worlds
to redefine reality as it opened CES 2024, the world’s leading technology gathering.
Siemens announced new partnerships and breakthroughs in AI and immersive
engineering to enable the industrial metaverse, and highlighted how these
technologies are empowering the world’s innovators to thrive using its open
digital business platform, Siemens Xcelerator.
- Siemens to integrate Amazon Bedrock into its Mendix low-code development platform to allow customers to create new and upgrade existing applications with the power of generative AI
- Access to Amazon Bedrock’s advanced generative AI technologies will help customers accelerate digitalization and tackle skilled labor shortages
- Mendix is an industry leader in low-code development with 50M end-users and more than 200,000 applications running on AWS across industrial, finance and other sectors
Siemens and Amazon Web
Services (AWS) are strengthening their partnership and making it easier for
businesses of all sizes and industries to build and scale generative artificial
intelligence (AI) applications. Domain experts in fields such as engineering
and manufacturing, as well as logistics, insurance or banking will be able to
create new and upgrade existing applications with the most advanced generative
AI technology. To make this possible, Siemens is integrating Amazon Bedrock - a
service that offers a choice of high-performing foundation models from leading
AI companies via a single API, along with security, privacy, and responsible AI
capabilities - with Mendix, the leading low-code platform that is part of the
Siemens Xcelerator portfolio.
- Zsolt Sluitner to hand over leadership
of the business as of March 1, 2024
- Jörg Vocke has been working at
Siemens for 20 years and has many years of experience in Siemens Real Estate’s business
- Current focus areas: Sustainable and
value-oriented growth as well as transformation of global office and production
locations
Effective
March 1, 2024, Jörg Vocke (55) will become the new CEO of Siemens Real
Estate (SRE), the real estate company of Siemens. In this role, he will report
directly to Ralf P. Thomas, Chief Financial Officer and member of the
Managing Board of Siemens AG. As a corporate real estate manager, SRE is
responsible for Siemens’ global real estate portfolio and continuously drives
the further development of this portfolio in a sustainable, socially
responsible and value-oriented manner. SRE also plays a key role in Siemens’ €2
billion global investment strategy for getting production locations fit for the
future.
- Further 8 percent
stake transferred to Siemens Pension-Trust e. V.
- Transfer strengthens Siemens’
pension assets in Germany
- Move reduces Siemens’ investment in Siemens
Energy AG to 17.1 percent from 25.1 percent
- Prof. Dr. Ralf P. Thomas to resign
from the supervisory board of Siemens Energy AG
Today, on December 18, 2023, Siemens AG is transferring an 8 percent stake in Siemens Energy AG to Siemens Pension-Trust
e. V. As a result, Siemens AG’s stake in Siemens Energy AG is declining to
17.1 percent. With this move, Siemens is executing its previously announced
plans to further reduce its investment in Siemens Energy. By transferring the
shares to Siemens Pension‑Trust e.V., Siemens is strengthening
its pension assets in Germany.
- Major order for 75 regional trains: 41 three-car
Mireo trains, 18 four-car Mireos, and 16 battery-powered Mireo Plus B trains
- MDSB 2025+ project with Leipzig hub
- Planned start
of operations in December 2026
- Order volume of approximately €500 million
- Largest Mireo order to date for Siemens
Mobility
Siemens Mobility has
won an order for the delivery of 75 Mireo trains for the “Central German S-Bahn
Network 2025+” (MDSB 2025+) project with an order volume of approximately €500
million. All in all, 41 three-car Mireo trains were ordered by the operators of
Die Länderbahn DLB, and 18
four-car Mireo trains as well as 16 two-car battery-powered Mireo Plus B trains
by DB Regio AG.