-
World premiere: Existing GoA4 line upgraded to
latest generation CBTC driverless automation system to boost capacity, reliability,
and efficiency for Paris metro operator RATP on behalf of Île-de-France
Mobilités
- Upgraded
line enables driverless automated train operation along the route doubled
in length, now also connecting Orly Airport to central Paris
- Line
remained in operations throughout the project that will serve one million
passengers daily by 2025
Siemens Mobility and RATP (Régie
autonome des transports Parisiens) have successfully modernized and extended the
automated Line 14 of the Paris metro. This world premiere marks the first
migration of an automated driverless (GoA4 – Grade of Automation) metro line to
the latest generation GoA4 driverless automated system “Trainguard MT CBTC”. The
new system, which was implemented during the past six years during passenger
services, enables more efficient and reliable services on the line that has
doubled in length by 14 kilometers due to extensions to the North and South.
With a remarkable headway of 85 seconds along its entire 28 km route, Line 14
is now the longest line in the Paris network and will eventually accommodate
over one million passengers daily. The expansion enables passengers to travel
from Orly Airport to Paris city center in 20 minutes and from the northern business
districts in Saint-Denis Pleyel to Orly Airport in just 40 minutes. With its
improved capacity, reliability, and efficiency, Line 14 serves as the backbone
of Paris' public transportation system, connecting to the future Grand Paris
Express network. Over six years, more than 250 Siemens Mobility engineers
contributed to this project, with over 500,000 hours of engineering.
- Production capacity increased, workforce expanded to meet growing
demand.
- New gearbox production line inaugurated, competence center for converter
cabinets established.
- Cornellà, an important supplier of traction motors, converters, and
converter cabinets, now produces rail gearboxes.
- Traction components (trademark: MoComp) from Cornellà (Barcelona) used
worldwide by numerous rail vehicle manufacturers.
Siemens Mobility has invested in its Cornellà factory to significantly
expand production capacity and the product portfolio
- DB Regio trains speed at 190 kilometers per hour between Bavaria and Thuringia
- Higher capacity, better service, new travel options to the north and south
Germany’s fastest regional train between
Bavaria and Thuringia is set to go. The new Franconia-Thuringia Express (FTX)
operated by Deutsche Bahn (DB) is inaugurating service on the Nuremberg-Erfurt
high-speed line on June 9, with the scheduled so-called small timetable change.
The modern Siemens trains, ordered by the Free States of Bavaria and Thuringia,
will run at a top speed of up to 190 kilometers per hour. To date, only
long-distance trains have operated on the northern section of the VDE 8.1, the
designation for this new and upgraded line.
- New AI-based apps for more efficient operation of water infrastructures available on the Siemens Xcelerator marketplace
- Easy integration into existing infrastructure without specialist knowledge
- Siemens to showcase its digitalization and automation portfolio for more sustainability in the water sector at IFAT 2024
Siemens, a leading technology company, has expanded its software portfolio for the water industry, enabling its customers to optimize their plant operations using artificial intelligence - without the need for technical expertise. These self-service solutions enable users to address the most pressing issues in water and wastewater operations: reducing water loss, preventing pollution from sewers, and ensuring the reliability of treatment assets. The effect of these applications is also a contribution to greater sustainability overall, as the world's water resources can be better protected. "Digital technologies have not yet been widely adopted in the water sector so far," says Anja Eimer, General Manager Global Water Business at Siemens. "The existing OT and IT device landscape of is complex, skilled workers are in short supply, and the business benefits of many digital applications have often been unclear. With our new software offerings, we are adressing these conditions and enabling water companies to perform AI-based operational analyses."
- Workstation provides with software-defined automation unprecedented control over factory automation and security
- At Automate 2024, Siemens highlights how co-creator Ford Motor Company will be the first customer to deploy and scale this technology in its manufacturing operations
Siemens, a leading
technology company, today announced a breakthrough in the longstanding
challenge of closely managing numerous hardware control points throughout the
factory. The solution is the new Siemens Simatic Automation
Workstation, which allows manufacturers to replace a hardware PLC, a
conventional HMI and an edge device with a single, software-based workstation.
This ushers in Information Technology (IT) workflows to Operational Technology
(OT) environments.
- Depot to be expanded to 87,550 m²
- New capacity for meeting growing demand
- 100% system availability thanks to digitalized depot operation
- Creation of attractive jobs in the region
- Up to 250 employees at the location in 2026
Siemens Mobility is investing approximately €150 million to expand its service depot in
Dortmund-Eving to 87,550 m² to meet the growing demand for rail services.
Plans call for constructing an additional 12,300 m² service hall
with storage facility, offices, and workshops to handle the maintenance of
trains up to 400 meters long. Construction
of the new building is scheduled to begin in 2024 and be completed by 2026. The
Siemens Mobility depot in Dortmund previously had a total area of
70,000 m² and will cover 157,550 m² when the project is
completed.
Today,
Brightline announced that Siemens Mobility (Siemens) has been designated the
“preferred bidder” to build train sets for the Brightline West high-speed rail
project that will connect Las Vegas and Southern California. The contract will
include a fleet of ten “American Pioneer 220” (AP 220) train sets to be
manufactured, delivered to Nevada and tested to support Brightline West’s
timeline of initiating service in 2028.
- The Fraunhofer-Gesellschaft commissions a research factory for battery cells with a capacity of up to 200 MWh in Münster, Germany
- Testing, implementation, and optimization of near-series production under real conditions of battery cells – for the automotive industry, among others
- Siemens is a production and building technology partner in this ecosystem
According to a study by
the Fraunhofer Institute for Systems and Innovation Research [Fraunhofer ISI],
battery production capacity in Europe alone will quadruple by 2025 from 124
gigawatt hours in 2022 to over 500 gigawatt hours. By 2030, this figure is expected
to increase tenfold to up to 1.5 terawatt hours.
- ÖBB’s Desiro ML fleet grows to 294 trains
- 21 new Desiro ML trains
will enter service during
Siemens Mobility GmbH has
received an order from Austrian Federal Railways (ÖBB) for an additional 21
Siemens Desiro ML electric trainsets. The order will increase the size of ÖBB’s
Desiro ML fleet to 294 trains, of which 236 are already in service throughout the
country. This order underscores the reliability of the Siemens Mobility Desiro
ML fleet. Beginning in 2026, the trains will serve local routes in the eastern
part of the country, in particular the main line between Vienna Meidling and
Floridsdorf and outer branch lines in Lower Austria.