Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release13 May 2024Digital IndustriesNuremberg
Siemens makes it easier for water utilities to benefit from artificial intelligence

With the Siemens Water (SIWA) applications designed specifically for the water and wastewater industry, operators can optimize energy efficiency, prevent water losses, reduce water pollution, and improve predictive maintenance measures, among other things.
The new offerings include digitalization solutions with pre-integrated hardware and software. This means that AI-based analytics applications have been combined with corresponding sensors from Siemens to make the installment processes as easy as possible and to achieve faster analytics results. To this end, Siemens has launched the new SIWA Leak Finder and SIWA Blockage Predictor apps – available on the Siemens Xcelerator Marketplace.
AI to combat leaks and pipe blockages
The SIWA Leak Finder app uses data from smart
flow meters to reduce water losses from pipe leaks by up to 50 percent. The
app's AI analyzes flow data and identifies leaks as small as 0.2 liters per
second. While data from any flow meter can be used for the app, the integration
of the Siemens Sitrans FM Mag8000 sensor eliminates the need for specialized
knowledge or Siemens services for installation.
Clogged pipes in sewer systems can lead to
pollution that also affects households and the environment. Inflow and
infiltration (I&I) reduce the effectiveness of the wastewater network and
can lead to expensive investments. Siemens' SIWA Blockage Predictor application
applies AI to water level data from sewers collected by sensors such as the Sitrans
LR110 radar level transmitter to detect blockages, inflow and infiltration.
Based on a single sensor installation, the app can be used in the event of
network overflows or in manhole chambers. The application finds nine out of ten
blockages and saves users time by automatically generating performance reports
for regulators.
Both the SIWA Leak Finder and SIWA Blockage
Predictor apps can easily process and analyze operational data from smart
sensors via a connection to the cloud – without the need for additional IT
expertise. In this way, the sensor data is available in the respective
application within two hours. The apps’ AI is automatically trained and
implemented with the sensor data from the day of installation. Cybersecurity is
also taken into account in the design of the apps. Mendix, Siemens' low-code
platform, can also be used to create interfaces to the respective company’s IT making
it possible to connect the data from the SIWA apps to ERP systems. Siemens'
expects these applications to typically pay for themselves in less than 36
months.
Siemens at IFAT 2024
In addition to AI-based applications and their
integration with smart sensors for the more efficient and sustainable operation
of water infrastructures, Siemens will showcase its entire automation and
digitalization portfolio for the water industry at the IFAT 2024 trade fair.
One focus will be on cybersecurity and how water infrastructure operators can protect
themselves from cyberattacks. Siemens will showcase blueprints and guidelines
for secure network and system architectures as well as proven, certified cybersecurity
solutions. Siemens also provides assistance with the implementation of the NIS
2 Directive, which will go into effect in the EU in October 2024.
Furthermore, Siemens offers a standardized
approach to groundwater well monitoring from a single source. Designed as an
end-to-end solution, it includes instrumentation, communication, remote control,
and intelligent data analysis to meet current and future regulatory
requirements and enable scalable and efficient water management. Siemens also offers
a range of technologies for utilities seeking to improve their energy
efficiency, from the Digital Process Twin to multimodal energy optimization.
For more information about Siemens at IFAT 2024, please visit:
https://www.siemens.com/global/en/company/fairs-events/fairs/ifat.html
Learn more about the integrated Siemens portfolio for the water and wastewater industry:
https://xcelerator.siemens.com/global/en/industries/water.html
For this press release
Follow us on X
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 72,000 employees internationally.
Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare.
In fiscal 2023, which ended on September 30, 2023, the Siemens Group generated revenue of €77.8 billion and net income of €8.5 billion. As of September 30, 2023, the company employed around 320,000 people worldwide. Further information is available on the Internet at www.siemens.com.
In fiscal 2023, which ended on September 30, 2023, the Siemens Group generated revenue of €77.8 billion and net income of €8.5 billion. As of September 30, 2023, the company employed around 320,000 people worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: HQDIPR202405106928EN