ÖBB is investing in a new maintenance fleet with 50
low-emission high-performance maintenance vehicles, including 6 cab cars. The Austrian
vehicle manufacturer Plasser & Theurer has been awarded to modernize the
ÖBB fleet and selected Siemens Mobility as trusted ETCS onboard unit partner to
equip the fleet with the latest European train control system (ETCS). The
Trainguard ETCS Level 2 solution that it deployed to ÖBB is based on the latest
Baseline 3 Release 2 standard. To ensure an economical transition to ETCS a
unified cabinet design with standardized interfaces is applied. The new
maintenance fleet is intended to operate throughout the ÖBB network and
cross-border to Germany. To operate in Germany the vehicles will additionally
be equipped with the Siemens PZB solution Trainguard Basic Indusi (TGB-I). TGB-I
with ETCS is a smart combination for operation on both existing and ETCS lines
thanks to proven and harmonized interfaces. By end of 2023 the first vehicles
will operate on the new high-speed Koralmbahn. The contract includes the option
to equip additional 46 high performance maintenance vehicles.
The Berlin
Transport Association (BVG) and Siemens Mobility have signed a contract for the
construction of a Sicas ECC electronic interlocking at Alexanderplatz subway
station. The new interlocking is to cover the approximately 3.5-kilometer route
between the Rosa-Luxemburg-Platz and Spittelmarkt subway stations. In addition
to the indoor system, the scope of order includes new cables, a cable system
and around 150 K140 signals (main, pre, emergency and protection signals). The
line, which comprises a total of five stations, runs underground on two tracks
in a tunnel with a small clearance gauge. The project, which has a total volume
of around €13 million, will start laying cables in November 2021 and will be
completed in summer 2024.
Our state of the art Inspiro trains and Communications
Based Train Control (CBTC) Trainguard MT (TGMT) systems will serve the final
section of Line 3 of the Bulgarian capital, which was opened on the 24th
April 2020.
The products in Siemens Mobility trains meet the
highest cyber security standards. This was recently confirmed by TÜV SÜD, which
approved Siemens Mobility Rolling Stock with the IEC 62443 4-1 certificate.
This award confirms, 18 months after the IEC 62443 2-4 / 3-3 certification, the cyber
security throughout the entire product development process.
Media representatives got a first-hand impression of the new Vienna Metro during a test drive on the 14th April 2021 – in the presence of Public Transport City Councillor Peter Hanke, Wiener-Linien Managing Director Günter Steinbauer and Siemens Mobility CEO Arnulf Wolfram. After the successful approval of operation, the so-called 'X-Wagen' will be in use for all Viennese on the four lines U1 to U4 from 2022. With the completion of the new U5 in 2026, the new vehicles will also be running fully automatically.
Siemens Mobility and DB Systemtechnik have signed a cooperation agreement to modernize a locomotive of the series 101 with an upgraded Siemens ETCS solution Trainguard 200 Onboard Unit system. The locomotive is part of DB Systemtechnik’s fleet and is used for test- and acceptance runs. It will now be upgraded to the European train control system ETCS level 2. At its core, the project aims to develop an interface solution that can be easily implemented for subsequent retrofitting and integration of ETCS and LZB into the vehicle architecture, independent of the train manufacturer. With this technical integration solution, a major step towards the successful retrofitting of entire fleets in the context of the Digital Rail for Germany program is made. Siemens Mobility has demonstrated its retrofit experiences and capabilities already in various retrofit projects throughout Switzerland, Great Britain, Spain and Germany.
Siemens Mobility is investing twelve million euros in the further modernization of its long-established production site in Vienna-Simmering: Together with Vienna's City Economic Councillor Peter Hanke, the groundbreaking ceremony for the construction project took place on Monday, March 1. The investment will focus on the construction of a new train commissioning hall, the expansion of digitalized production, and the optimization of production workflows. This will further increase the competitiveness of the site and secure local jobs and local value creation. Passenger coaches and metro trains are built at the historic Siemens Mobility plant, for example the new night trains for ÖBB or metro trains for Vienna, Munich, Riyadh or Bangkok. ÖBB's popular Railjets were also manufactured here. At the Vienna plant, Siemens Mobility employs about 1,200 people, manufactures about 450 rail vehicles per year and currently trains a total of 88 apprentices.
In a live broadcast between Berlin and London on Thursday, March 4, 2021, Transport for London and Siemens Mobility unveiled the design of the new London Piccadilly line tube trains. 94 state-of-the-art tube trains will replace the current fleet of the Piccadilly line, which was built in the 1970s. The new generation of trains will offer passengers more spacious, air-conditioned walk-through carriages and improved accessibility. The trains are scheduled to be in service on the Piccadilly line from 2025.
Polish
provider of transport and logistics services Laude Smart Intermodal S.A. has
just expanded its fleet with the most modern locomotive in Europe: the Vectron
MS. The vehicle colored in pink was handed over in Poznan Franowo near Posen on
February 3
rd, 2021. It is the 50
th Vectron locomotive
from Siemens Mobility in the hands of Polish carriers.