- Next generation of Simatic ET
200eco PN: New functions for modern machine concepts and requirements
- For use in redundant,
high-availability systems thanks to S2 redundancy
- High current-carrying capacity with
power supply via L-coded plug
- High-quality industrial enclosure with IP65/67
protection for outdoor use
Siemens has launched a new generation of machine-level block I/O
devices in the form of the Simatic ET 200eco PN. The new I/O family with
IP65/67 degree of protection includes five digital I/O devices as well as an IO-Link master device and offers users a whole range of new
functions for modern machine concepts and requirements. In their new industrial
metal enclosure, the devices are reliably protected from UV radiation and
harmful substances even under adverse environmental conditions, making it
possible to use the devices outside of factory buildings. The devices are
supplied with power via an L-coded plug, resulting in a considerably higher
current-carrying capacity. In turn, this enables longer cable routes in the
field, and the supply and connection of more energy-intensive components (such
as valve terminals) without the need for more supply cables.
- Siemens
industrial gas turbines will provide peaking power to help improve the
reliability and flexibility of the Belarusian power grid
Siemens will deliver the power generation equipment for two
new peaking power plants in the Republic of Belarus. The customer is the
state-owned utility company RUE Vitebskenergo. The new plants will be operated in
conjunction with the existing Lukomlskaya and Novopolotskaya power
plants in
the Vitebsk region in northern Belarus and will help ensure the
reliability and flexibility of the country’s power grid. The plants are expected to go into
operation in the end of 2021.
- Simatic S7-1500
firmware V2.8: Secure data integration, versatile diagnostics function for OPC
UA server
- Simatic S7-1200 firmware V4.4:
Improved cross-platform data transfer, OPC UA Data Access as server, OPC UA
Modelling Editor
Siemens announces the release of two firmware updates for
Simatic controllers that provide new functions. The Simatic S7-1500 firmware
V2.8 from Siemens improves cross-device capabilities for data integration and
diagnostics functions. The new Simatic S7-1200 firmware V4.4 extends the
communication functions of the Simatic S7-1200, enhancing cross-platform data
transfer with other controllers and higher-level or cloud-based systems such as
ERP, SCADA and Mindsphere. The applications are numerous, ranging from
industrial use to agriculture and infrastructure projects.
- Cooperation aims to test renewable fuels at the Rya CHP plant located in the energy port of Gothenburg
- First phase with Göteborg Energi is to validate 3D-printed burners at the Rya plant
By 2030, the ambition is that all district heating in Gothenburg, Sweden, will be produced by renewable or recovered energy sources. With this in mind Göteborg Energi and Siemens have come together in a cooperation agreement with the aim of testing state-of-the-art gas turbine technology that enables the operation of renewable fuels in the Rya combined heat and power (CHP) plant, which is today powered by natural gas.
- Digital solutions provide for improved operational efficiency and reduced emissions
Siemens will equip Lalitpur Power Generation Company Limited (LPGCL), a Bajaj Group company, with advanced digital solutions for its power plant located in Lalitpur, Uttar Pradesh, India.
- New Version V16 of the TIA Portal engineering framework with focus on standardization and continuous integration
- Enhanced engineering efficiency with distributed working in the developer team
- Increased software quality thanks to integrated Test Suite
- Transparent operation with cross-vendor OPC UA communication
With the new TIA Portal V16 (Totally Integrated Automation Portal), Siemens has expanded its engineering framework with practical new functions for various phases from planning, to engineering, to commissioning. The innovations concentrate on the continuous integration of the development process. These include standardization, integrated engineering spread across teams and an integrated function test. This enables users to increase the quality of their software, shorten commissioning times and reduce engineering costs.
- Digital Enterprise portfolio aimed at meeting increasing requirements for greater productivity and flexibility as well as environmental efficiency
- New platform innovations ensure integration and flexibility across all stages of the value chain
- Growing ecosystem for Industrial Edge and Cloud enables scalability from the shop floor to the Cloud
Through innovations and the integration of cutting-edge technologies into the Digital Enterprise portfolio, Siemens helps companies from all sectors to achieve a more flexible and environmentally efficient production. “The Digital Enterprise portfolio is already well established globally in all industries for the implementation of Industrie 4.0. Many applications demonstrate the tangible benefits of these solutions for our customers,” explains Klaus Helmrich, Member of the Managing Board of Siemens AG and CEO of Digital Industries, at SPS. “Now we are taking the next step: with numerous innovations und cutting-edge technologies, we are taking the Digital Enterprise portfolio and therefore Industrie 4.0 to a new level.”
- Sustainable technological cooperation for the future of industrial wireless communication
- Joint Proof of Concept in a real industrial environment using the 3.7-3.8 GHz band
- Researching the capabilities of 5G standalone networks for industrial applications
Siemens and Qualcomm Technologies, Inc. have implemented the first private 5G standalone (SA) network in a real industrial environment using the 3.7-3.8GHz band. Both companies have joined forces in this project: Siemens is providing the actual industrial test conditions and end devices such as Simatic control systems and IO devices and Qualcomm Technologies is supplying the 5G test network and the relevant test equipment. The 5G network was installed in Siemens’ Automotive Showroom and Test Center in Nuremberg. Automated guided vehicles are (AGV) displayed here which are primarily used in the automotive industry. New manufacturing options and methods are also developed, tested and presented before they are put into action on customer sites. This allows Siemens’ customers, such as automated guided vehicle manufacturers, to see the products interact live.
- Siemens Industrial Edge closes the gap between local and Cloud computing and enables high-frequency data exchange at field level
- Edge apps for intelligent data analysis and increased productivity
- Industrial Edge includes a backend, Edge devices and Edge apps in Edge Management
With Siemens Industrial Edge, Siemens offers a digitalization solution that adds machine-level data processing to automation devices, by taking the intelligence of Edge computing and thus, sophisticated analytics securely to manufacturing level. Siemens Industrial Edge offers users the opportunity to execute a wide range of descriptive, diagnostic, predictive and prescriptive analytics applications. Cloud connectivity is used in conjunction with Edge apps from Siemens, from third-party providers or from users themselves in an integrated hardware and software ecosystem for automation components.
- New devices for electrical installations in industrial and infrastructure environments with a lower nominal current of 0.1 to 0.4 amperes
- Firmware update with improved control and diagnostic functions
- Failsafe group shutdown function without additional wiring
Siemens Smart Infrastructure is adding four new devices to its portfolio of Simatic ET 200SP motor starters, which can be used to start electric drives with a power output from 0.1 to 0.4 amperes (A). These types of drives are found in fans and coolant pumps, for example. The compact motor starters are installed in control cabinets and are designed to start single and three-phase motors of machines and systems, protecting them against overloads and short-circuits. They are each available in standard and safety variants.