- AnalyzeMyWorkpiece /Monitor enables continuous monitoring of workpiece production
- Quality control takes place immediately during production
- New application extends the range of existing applications for quality assurance
With AnalyzeMyWorkpiece /Monitor, Siemens is extending its software portfolio for machine tools for workpiece quality. The Edge application based on high-frequency data, which will be presented at EMO 2019, enables continuous monitoring of workpiece production in machine tools. Measured values such as position data, torque values or control deviations together with context information, for example the tool currently being used, are acquired from the machine with high frequency and without feedback via Sinumerik Edge. The measured values are compared continuously with a reference model. In the event of deviations that exceed a predefined level, the application logs the result, sends it to the machine tool and enables prompt responses by the operator. This means, for example, that unique process-parallel quality control is supported during production.
- Siemens drives forward digital transformation in the machine tool industry with a brand new Sinumerik generation
- Sinumerik ONE enables seamless interaction between virtual and real world for significantly increased productivity in the production and use of machine tools
- Scalable CNC-portfolio for highest performance requirements and optimum surface quality
With Sinumerik ONE, the first digital native CNC, Siemens is driving forward digital transformation in the machine tool industry. The new controller works with software to create the machine controller and associated digital twin from one engineering system and thus contributes to the seamless integration of hardware and software. Thanks to its seamless interaction between virtual and real world as well as high-performance hardware, Sinumerik ONE is setting new standards in terms of productivity, performance and digitalization. It is the future-proof CNC for machine tools in the increasingly digital world of manufacturing. Both machine manufacturers and machine operators benefit from the universal digital twin for the product, production and performance.
- Slogan: "Digitalization in Machine Tool Manufacturing – Thinking further!"
- New Sinumerik ONE controller generation as a digital native
- Software portfolio for workpiece quality extended to include another Edge app
Under the slogan "Digitalization in Machine Tool Manufacturing – Thinking further!", Siemens is presenting numerous extensions to its Digital Enterprise portfolio for the machine tool industry in around 1700 square meters at EMO in Hanover in Hall 9, Booth H50. The company has already integrated future technologies in its portfolio, such as its new machine tool controller specifically designed for digitalization, Edge and cloud computing, artificial intelligence and additive manufacturing, and is leading the machine tool world to the next level of digital transformation. "With our unique range of digitalization solutions, we are paving the way for the future of the machine tool industry and helping our customers, machine builders and machine users, to find new and more comprehensive ways of using rapidly growing data volumes to increase their productivity, quality and competitive edge", explains Dr. Wolfgang Heuring, CEO of Business Unit Motion Control. The basis for innovative technologies is the availability and transparency of data which can be used to create digital twins – of the product, production and performance – and which map and link together all the steps of industrial manufacturing processes in a virtual environment. "The key is to use this data innovatively and to convert it into valuable knowledge in order to improve performance and flexibility and reduce the time to market", Heuring continues.
His Royal Highness The Prince of Wales has visited the headquarters of Siemens AG while on a trip to Germany. The Prince's trip is focused on the bilateral relations between the United Kingdom and Germany. During his roughly 45-minute tour of the company's headquarters, Prince Charles learned about topics such as sustainability, the new world of work and Siemens' Cents4Sense initiative. He also signed the company's visitors' book.
- Visit highlights the importance of bilateral relations between the United Kingdom and Germany
- His Royal Highness Prince of Wales gains insights into sustainability and the new world of work
- CEO Joe Kaeser: "Our relationship is strong, resilient and geared to a common future."
His Royal Highness The Prince of Wales has visited the headquarters of Siemens AG while on a trip to Germany. The Prince's trip is focused on the bilateral relations between the United Kingdom and Germany. During his roughly 45-minute tour of the company's headquarters, Prince Charles learned about topics such as sustainability, the new world of work and Siemens' Cents4Sense initiative. He also signed the company's visitors' book.
- New firmware adds Fast PTI mode for precise positioning at even higher speeds
- Fast PTI mode comes with auto-tuning function
- Firmware update opens up new applications for Sinamics V90
New functions are being added to the proven Sinamics V90 servo drive system with the V1.11 version of the Sinamics firmware. The Fast PTI mode is now available for the drive system, increasing Pulse Train Input (PTI) performance by 70 percent. This improves the reaction time from the Pulse Train Input command to the actuation of the motor. The improved reaction time opens up new application areas for the Sinamics V90 which require higher dynamic performance such as high speed labeling as well as in the field of LED production (LED pick & place).
- Orders grew 6%, to €23.6 billion, and revenue rose 4%, to €20.9 billion, for a book-to-bill ratio of 1.13 and record high order backlog of €142 billion
- On a comparable basis, excluding currency translation and portfolio effects, orders increased 4% and revenue was up 2% compared to Q2 FY 2018
- Adjusted EBITA for Industrial Business climbed 7% to €2.4 billion, with most businesses increasing their performance; Industrial Business Adjusted EBITA margin reached 11.4%, even with severance charges taking 0.3 percentage points
- Net income reached €1.9 billion, near the prior-year level which benefited substantially from a €0.7 billion Adjusted EBITA from Centrally managed portfolio activities; the current period benefited from a lower income tax rate, and basic EPS of €2.24 was burdened by €0.08 from severance charges
"We delivered on our promises again this quarter, and even exceeded expectations in many areas. Now, we enter into a new era to become an even stronger and more focused Siemens."
We released our second quarter results for fiscal year 2019 on May 8, 2019. The press conference was broadcast live.
Klaus Patzak (54), currently Managing Partner of the Siemens Portfolio Companies, has been appointed Chief Financial Officer (CFO) of the new Siemens Gas and Power business (GP). In this role, Patzak will be responsible for building the Finance governance structures, steering the activities required for carving out and listing, and helping to shape the format of the future stand-alone Siemens energy business. In his new role, he will report directly to Lisa Davis, Chief Executive Officer (CEO) of the Gas and Power Business that is to be created. Via a functional reporting line, he will also report to Siemens CFO, Ralf P. Thomas.
- Creation of new major player on the energy market with business volume of €30 billion and over 80,000 employees through spinoff of Gas and Power and transfer of Siemens' SGRE stake
- Spinoff to give shareholders direct participation in success and enable rapid implementation
- Future industrial core: Digital Industries and Smart Infrastructure
- Ambitious medium-term goals refined and long-term aspiration outlined
- Savings of €2.2 billion by 2023 through structural efficiency gains planned
- Growth in future-oriented fields to generate net increase of over 10,000 jobs despite efficiency measures
Siemens intends to meet its medium-term growth and profit targets by clearly focusing its portfolio on dynamic growth markets and efficiency gains. To this end, the Supervisory Board of Siemens AG today unanimously approved the next steps in the company's Vision 2020+ strategy concept, including the spinoff of Siemens' Gas and Power (GP).