- 27 battery-powered trains for Landesanstalt
Schienenfahrzeuge Baden-Württemberg (SFBW)
- Innovative and energy-efficient battery-powered hybrid platform that
can be operated with or without overhead lines
- Siemens Mobility delivers
further 38 Mireo Plus B trains to Niederbarnimer Eisenbahn (NEB) and Midtjyske
Jernbaner in Denmark
Siemens
Mobility presents the Mireo Plus B battery train to the public for the first
time at InnoTrans 2022. The Landesanstalt Schienenfahrzeuge
Baden-Württemberg (SFBW) has ordered 27 Mireo Plus B trains from Siemens
Mobility in 2020. The two-car electric trainsets with
120 seats can operate on rail routes with or without overhead power lines
thanks to their battery hybrid drive and are scheduled to operate in Network 8
of the Ortenau regional system. Delivery of the multiple units is scheduled
between June and December 2023.
- Line B of the
Rennes metro enters revenue service
- Siemens Mobility
has equipped the entire line with the Cityval, a turnkey driverless automatic
metro system
- The Cityval of
Rennes Line B is a world premiere
With the commissioning of the new state-of-the-art
automated metro Line B in Rennes, Siemens Mobility has once again demonstrated
its leading expertise in delivering fully automated turnkey metro systems. Crossing
the Rennes metropolitan area along a South-West axis, Line B has 15 stations
spread over 13 km. 20 years after the first metro line in Rennes opened with
VAL technology (Line A), Rennes Métropole and SEMTCAR renewed their trust in
Siemens Mobility to equip the second metro line in the city with the new
generation of the automated metro system, Cityval.
- Siemens
Mobility to
retrofit 176 ViRM double deck rail vehicles with the latest ETCS onboard
technology
- Siemens Mobility will provide seven years of
maintenance services for ETCS system
Siemens Mobility has been
awarded a contract by NS Group N.V, the Dutch Railways, to retrofit 176 ViRM trains
with the latest European Train Control System (ETCS) Level 2 technology. With
the ETCS Level 2 upgrade, the fleet will be able to operate with a greater
degree of efficiency for the remainder of its lifetime, while also meeting the
latest European standards for rail safety interoperability. Siemens Mobility
will provide the ETCS onboard unit
equipment and installation support, as well as seven years of maintenance
services for the system. The retrofitted vehicles will be delivered in the
period 2023–2027.
- Siemens Mobility supported RATP and Ile-de-France
Mobilités in the complete automation of Line 4
- Siemens Mobility fully automated the line with its digitalized
systems and CBTC signaling technology
- The automation of Line 4 will centralize control of operations, increase availability, reliability, and
capacity
The
modernization of Line 4 of the Paris Metro has been completed with the highest
grade of automation and the automatic driverless metros have now begun revenue
service. The digitalization
and optimization of Line 4 will allow RATP to safely increase frequency by reducing intervals
between trains from 105 to 85 seconds. Chosen in
2015 by RATP to automate Line 4, Siemens Mobility supplied their digitalized
communication and CBTC signaling systems to modernize the network. After a
trial run with no passengers that began in June, the automation of Line 4 is now
a reality. More automatic driverless shuttles will be introduced into the
line's traffic over time to achieve full automation by the end of 2023.
-
Next milestone in the “H2goesRail” project
- Siemens CEO Roland Busch, DB CEO Richard Lutz and
State Secretary Hartmut Höppner take first test ride in the Mireo Plus H and test
the refueling process
- Innovative complete hydrogen system will be used in regular passenger service
as of 2024 and replace diesel trainset
- Hydrogen train and mobile fueling
station can be viewed at the InnoTrans2022
(Wegberg-Wildenrath,
September 9, 2022) Premiere ride in the new hydrogen train: Dr. Roland
Busch, CEO of Siemens AG, Dr. Richard Lutz, CEO of Deutsche Bahn, and Hartmut
Höppner, State Secretary in the Federal Ministry for Digital and Transport (BMDV),
are taking their first ride in the Mireo Plus H hydrogen train today and will
then demonstrate the train’s refueling procedure using the mobile hydrogen
fueling station. The event will be held at the Siemens Test and Validation
Center in Wegberg-Wildenrath, North Rhine-Westphalia. It is planned to have
hydrogen technology replace diesel-powered trainsets in regional transport in
the future and make a significant contribution to phasing out diesel fuel. Hydrogen
trains are a particularly climate-friendly drive technology since they operate
emission-free with green hydrogen and emit only water vapor.
- World
premiere of the interior of the new sleeping and couchette car
- Modern
design, greater comfort and privacy for travelers
- Total
of 33 next-generation Nightjets on the rails by 2025
ÖBB and
Siemens Mobility unveil the next generation of Nightjet sleeping and couchette
cars at the Siemens Mobility plant in Vienna. The new cars are designed to
optimally accommodate the needs of customers and score points with modern
design, greater comfort and increased privacy. By the end of 2025, a total of
33 next-generation ÖBB Nightjets will be on the rails, connecting European
cities overnight at speeds of up to 230 kilometers per hour in a
climate-friendly way. The first trains are scheduled to be in use by the end of
summer 2023 on the popular routes from Austria and Germany to Italy.
- 65 Vectron AC and Vectron MS
locomotives called from existing framework agreement
- Delivery includes locomotives with a
top speed of 230 km/h
- Milestone
reached: 1,500 Vectrons sold
Akiem, the
leasing rolling stock specialist company for rail vehicles, has ordered 65
Vectron AC and Vectron MS locomotives from Siemens Mobility. The order was
placed as part of a framework agreement for the purchase of locomotives that
was signed in December 2021. The first locomotives from this call are to be
delivered in mid-2024. Akiem previously ordered 20 Vectron locomotives from
Siemens Mobility last December.
- Delivery of 14 Vectron MS
multisystem locomotives
- MRCE fleet includes 147 Vectron
locomotives
Mitsui Rail
Capital Europe (MRCE), a full-service locomotive leasing company, has ordered
14 Vectron MS multisystem locomotives from Siemens Mobility on the basis of an
existing contract. With this order, MRCE will have a fleet of 147 Vectrons.
MRCE plans to use the locomotives in Germany, Austria, Hungary, Poland, the
Czech Republic, Slovakia, Romania, and the Netherlands.
InnoTrans 2022, September 20-23, 2022, Messe Berlin, hub27, booth 230
- Siemens Mobility presents Siemens Xcelerator, the open digital business platform
- Fair highlights: Next-generation hydrogen train Mireo Plus H; infrastructure in the cloud; 100% system availability with Railigent X; unique software portfolio Mobility Software Suite X
- Motto of the company’s show: “Destination Digital”
Siemens Mobility is presenting its new digital business platform Siemens Xcelerator at InnoTrans 2022. Siemens Xcelerator is an open digital business platform with the ambition to create a powerful ecosystem of partners who can jointly accelerate digital transformation and sustainability in mobility at scale. By opening interfaces for all participants of the mobility ecosystem, Siemens Xcelerator helps connect the real with the digital worlds – a first-of-its-kind innovation in the rail industry.
- Latin America’s first fully automated metro line (GoA 4)
- Siemens Mobility digitalized CBTC technology installed across entire 15 km of track,11 stations, and 29 trains
- Automated signaling provides greater availability, enhanced operations, and passenger experience
ViaQuatro has successfully begun full operation of São Paulo’s entire Metro Line 4 with Siemens Mobility’s Communications-Based Train Control (CBTC) signaling. Since its first stretch opened in 2010, it has been the first fully automated metro line in South America that can operate with GoA 4, the highest grade of automation that allows trains to be automatically controlled and operated. The digitalized and optimized system allows for a more efficient and centralized control of operations, while also increasing the safety, availability, and capacity across the entire network.