The information contained
herein is not for publication or distribution, directly or indirectly, in or into
any jurisdiction where to do so would be prohibited by applicable law.
- Extraordinary Shareholders’ Meeting to be held in virtual format
- Siemens AG to spin off 55 percent of Siemens Energy to shareholders
- One Siemens Energy share for every two Siemens shares
- Siemens Energy to start with S&P Global investment-grade rating of “BBB”
- Initial listing of new shares planned for September 28, 2020
Siemens shareholders will vote on the spin-off of Siemens AG’s energy business at an Extraordinary Shareholders’ Meeting today. Due to the restrictions imposed on public events by the coronavirus crisis, the shareholders’ meeting will be held in a virtual-only format – that is, without the shareholders or their proxies being present in person. To ensure complete transparency, a livestream atwww.siemens.com/agm-servicewill provide shareholders and their proxies with audio and video coverage of the entire event via the Internet. Siemens shareholders had until July 7, 2020, to submit questions electronically. The proposal to approve the Spin-off and Transfer Agreement that Siemens AG and Siemens Energy AG concluded on May 22, 2020, is the only item on the meeting agenda.
- 1.3-gigawatt turnkey combined cycle power plant
- Long-term service program and operation & maintenance (O&M) services included
- Largest LNG-to-power development in Latin America
- Total project volume of €1 billion
Siemens has secured an order for the turnkey construction of a new combined cycle power plant for the integrated LNG-to-Power project GNA 1 of Gás Natural Açu in the Port of Açu in the state of Rio de Janeiro, Brazil. Siemens is providing an equity investment and owns one-third of the project company Gás Natural Açu (GNA) together with Brazil logistics company Prumo Logística S.A. and BP. In addition, Siemens signed a long-term service agreement and will operate and maintain the plant to help ensure reliability, availability and operational performance. The order is the first application for the highly efficient and proven Siemens H-class gas turbine in Brazil. With a capacity of approximately 1.3 gigawatts (GW), the power plant will provide affordable and clean energy for Brazil. Total project volume for GNA 1 is approximately €1 billion (R$4.5 billion).
- Cooperation aims to test renewable fuels at the Rya CHP plant located in the energy port of Gothenburg
- First phase with Göteborg Energi is to validate 3D-printed burners at the Rya plant
By 2030, the ambition is that all district heating in Gothenburg, Sweden, will be produced by renewable or recovered energy sources. With this in mind Göteborg Energi and Siemens have come together in a cooperation agreement with the aim of testing state-of-the-art gas turbine technology that enables the operation of renewable fuels in the Rya combined heat and power (CHP) plant, which is today powered by natural gas.
- Gas turbine rotor exchange allows for increased output and efficiency
- Control system upgraded to latest version of SPPA-T3000
The Dunamenti Power Plant in Százhalombatta, Hungary, is the largest gas-fired power plant in the country with a capacity of 794 megawatts (MW), making it a major source of reliable electricity in Hungary. Recently, in collaboration with the customer and plant owner, MET Asset Management AG, and within the scope of an overhaul project, Siemens Gas and Power replaced the entire rotor of the plant's SGT5-2000E gas turbine and installed a new, state-of-the-art SPPA-T3000 control system.
Arja Talakar has been appointed CEO of Siemens Oil & Gas, effective April 1, 2019. He will be based in Houston, Texas, the global headquarters for Oil & Gas and its parent operating company, Siemens Gas and Power.
- Green hydrogen project launched in May 2020
- Decarbonizing a paper factory by modernizing an existing combined heat and power plant in France
With the HYFLEXPOWER project, a consortium made up of Engie Solutions, Siemens Gas and Power, Centrax, Arttic, German Aerospace Center (DLR) and four European universities are implementing a project funded by the European Commission under the Horizon 2020 Framework Program for Research and Innovation (Grant Agreement 884229). The implementation of this project, the world's very first industrial-scale power-to-X-to-power1 demonstrator with an advanced hydrogen turbine, will be launched at Smurfit Kappa PRF’s site - a company specialized in manufacturing recycled paper - in Saillat-sur-Vienne, France. The purpose of this project is to prove that hydrogen can be produced and stored from renewable electricity and then added with up to 100 percent to the natural gas currently used with combined heat and power plants. For this an existing Siemens SGT-400 industrial gas turbine will be upgraded to convert stored hydrogen into electricity and thermal energy.
- Power plants Termoeléctrica del Sur, de Warnes, and Entre Ríos inaugurated in August and September
- Upgrade to combined cycle power plants increase the generation capacity by one gigawatt
- Expansion provides reliable energy supply and will allow export of value-added products
With the official inauguration of the Termoeléctrica de Warnes power plant in mid-September, all three power plants in Bolivia were inaugurated within a few weeks in August and September. Since the contract signing in 2016, Siemens has expanded Bolivia’s three largest thermal power plants to efficient combined cycle mode. The power plants are owned and operated by Ende Andina SAM. Together, all three add more than one gigawatt of electrical power to its current maximum capacity and to the Bolivian national grid.
- Aeroderivative gas turbine will drive RFBB36 pipeline compressor
- Siemens compressor train for Winchell Lake Compressor Station for additional pipeline capacity
Siemens received an order from North American pipeline operator, Nova Gas Transmission Ltd. (NGTL), a wholly owned subsidiary of TransCanada Corporation, to supply a gas turbine-driven compressor train for the Winchell Lake Compressor Station in Alberta, Canada. The turbo-compressor train will be a critical part of the NGTL pipeline expansion to transport natural gas to export markets. Commercial operation is expected to begin in the fourth quarter of 2019.
Siemens has received an order from Israel
for the first time for the turnkey construction of two industrial combined
cycle power plants. The two natural gas-fired power plants, Alon Tavor and
Ramat Gabriel, are to be built in northern Israel. Alon Tavor will supply a
creamery with electricity and process steam, while Ramat Gabriel will supply a
fiber factory. The Israeli energy provider, RD Energy, is the customer for both
power plants. Commissioning of the plants is scheduled for mid-2018.
Siemens has received its first order from
China for the
delivery of four SGT-800 gas turbines and the
associated generators.
The turbines will be installed in the Shanxi Guoxin
Baode and Xiyang decentralized
energy projects in Central China. The two combined cycle power plants with heat
extraction will have an overall capacity of 308 megawatts (MW). The
customer is Shanxi Natural Gas Limited Company, a subsidiary of ShanxiProvincial
Guoxin Energy Development Group Co., Ltd.. Commercial
operation of the plants is scheduled for July 2017.