Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
HYFLEXPOWER: The world’s first integrated power-to-X-to-power hydrogen gas turbine demonstrator
A world’s first: Industrial-scale power-to-X-to-power demonstrator
The purpose of HYFLEXPOWER is to prove that hydrogen can be produced and stored from renewable electricity and then added with up to 100 percent to the natural gas currently used with combined heat and power plants.
An exclusively European technology
- Engie Solutions will build the hydrogen production and storage facility, including the natural gas/hydrogen mixing station prior to the turbine
- Siemens Gas and Power will supply the electrolyser for hydrogen production and develop the hydrogen gas turbine
- Centrax will upgrade the package for hydrogen operation and install the new turbine
- German Aerospace Center (DLR) together with the University College London, University of Duisburg-Essen and Lund University will support the hydrogen turbine technology development
- National Technical University of Athens will perform economic, environmental and social assessments of the concept
- Arttic will support the operational project management and the project’s communication activities.
- May 2020: Contract finalization and start of engineering development.
- 2021: Installation of the hydrogen production, storage and supply facility at pilot demonstration site.
- 2022: Installation of the gas turbine for natural gas/hydrogen mixtures and initial demonstration of advanced pilot plant concept.
- 2023: Pilot demonstration with up to 100 percent hydrogen for carbon-free energy production from stored excess renewable energy.
As part of a consortium, Siemens Energy will upgrade an existing SGT-400 industrial gas turbine to generate electricity and thermal energy with stored hydrogen and demonstrate an industrial-scale power-to-H2-to-power solution.
Siemens Gas and Power helping to increase level of decarbonization
Engie Solutions, a stakeholder committed to hydrogen
Centrax Ltd. developing Hydrogen ready solutions
1 According to the ADEME (France's agency for environment and energy management), “Power to X” (or “P2X”) is the act of converting electricity into another energy vector. For the HYFLEXPOWER project, the “X” vector is hydrogen.
The project's partners:
For this press release
Contact
Alfons Benzinger
Siemens Gas and Power GmbH & Co. KG
91058 Erlangen
Deutschland
+49 9131 17-34549
Lise Forest
Engie Solutions
1 place Samuel de Champlain
Faubourg de l’Arche
92929 Paris La Défense
France
+33 6 32 47 62 48
Maureen Palfrey
Centrax Ltd.
Newton Abbot
TQ12 4SQ
England
+44 1626 358212