- Sinumerik One Dynamics - three technology packages to increase the efficiency of CNC users when programming in the shopfloor and executing CAM-generated CNC programs
- Top Surface and Top Speed Plus for excellent motion control and perfect workpiece surfaces
With the software version NCU-SW 6.14, Siemens is launching three powerful technology packages exclusively for the CNC Sinumerik One. The Sinumerik One Dynamics packages are available in three different packages: One Dynamics Operate, One Dynamics 3-axis milling and One Dynamics 5-axis milling. The software functions contained in the technology packages support users from machine-oriented programming in the jobshop to high-performance machining of CAD-CAM-programmed workpieces with high surface quality.
- Order worth almost €400 million
- Avenio HF light rail vehicles provide highest passenger comfort
- 24-year contract for service and spare parts to guarantee availability
Düsseldorfer Rheinbahn AG and Duisburger Verkehrsgesellschaft AG have jointly ordered 109 Avenio HF high-floor light rail vehicles from Siemens Mobility, including an option for an additional 48 units. The contract also includes the maintenance and servicing of the Duisburg vehicles for 24 years and an option for a further eight years. A 24-year spare parts supply contract was signed for the Düsseldorf vehicles. The order has a volume of almost €400 million.
- Improvement of machine tool availability through predictive maintenance with Analyze MyMachine /Condition
- Analyze MyMachine /Condition for Sinumerik Edge creates a mechanical fingerprint of the machine tool
- Condition evaluation, analysis and comparison of all connected machines using the Mindsphere application
Siemens is extending its edge application Analyze MyMachine /Condition with a corresponding Mindsphere application and thus demonstrating how edge computing and cloud computing can be intelligently combined. The Sinumerik Edge Application Analyze MyMachine /Condition, which the company presented last year at the EMO, uses high-frequency CNC data to create the mechanical fingerprint of a machine tool. In the application, users can capture and evaluate various parameters such as stiffness, friction, and backlash in the individual axes with the help of flexibly configurable measurement series. The measurement results can then be visualized and compared with reference data.
- Adaptable modular solution to deal with short-term needs of hospitals, e.g. during epidemic or temporary construction works
- Ergonomic solution ensuring safety of patients and medical staff
- Compliant with healthcare facilities regulations
- Autonomous care units, fast to deploy, deliver high added value
Siemens Smart Infrastructure has teamed up with Toutenkamion Group to jointly develop an agile container system of highly innovative mobile intensive care units, designed to take pressure off hospital infrastructure. The solution was a response to the Covid-19 pandemic, which forced nursing staff, doctors and hospital managers to urgently come up with practical solutions to ensure adequate care was provided to extremely contagious patients, while maintaining other emergency and conventional care. One of the major challenges of the epidemic has been the need to equip and increase the number of resuscitation and intensive care beds.
Labeled as the project of the century for the German metropolitan region, the Rhine-Ruhr express (RRX) will help alleviate the continuously worsening transportation issues along the Rhine and Ruhr from 2018. The municipalities involved in the new RRX rail transport concept commissioned Siemens to supply 82 electric multiple units, type Desiro HC, and to provide maintenance services for a period of 32 years. With a total volume of more than 1.7 billion euros, this is the largest regional rail service order in Germany so far for Siemens.
The region is one of the largest conurbations in Europe, with a population of approximately ten million and numerous transit routes. On the main section between Cologne and Dortmund in particular, mobility has been heavily restricted for years now by overstretched public transport networks and train connections. Through a targeted extension of the railway network and the shift of traffic from road to rail this enables, the RRX is expected to replace roughly 31,000 individual car trips every working day. The first RRX trains will begin operating punctually with the change of the rail system's timetable on December 9, 2018. Commercial operation will begin on Line RE 11 that connects Düsseldorf, Essen, Dortmund, Hamm, Paderborn and Kassel. During rush hours the eventual target is one train every 15 minutes.
Digitally networked Rhine-Ruhr Express (RRX) convinces jury of experts
The “RRX – digital and optimally networked” project from Siemens Mobility has won the German Mobility Award 2020. A jury of high-ranking experts selected the project from around 300 applicants. According to the jury, the project is a valuable contribution toward achieving flexible, fully networked and future-oriented mobility, and represents a shining example of Germany’s strength as a location for business.
- High-frequency radar ensures
reliable readings in challenging environments
- Optional
HMI delivers easy commissioning and diagnostic
support
- Wide
range of liquids and solids applications in practically all market segments
including energy, mining, aggregates and water
Siemens presents two new additions
to the Sitrans LR100 series of 80 GHz radar transmitters. These high-frequency,
compact transmitters deliver robust, reliable measurements even in the most
challenging environments. Both deliver fast and easy setup. Sitrans LR140
features 4-20 mA simplicity and is configured via Bluetooth wireless technology
and the Sitrans mobile IQ App.
- Memorandum of Understanding for joint holistic hydrogen system for rail
- Siemens Energy and Siemens Mobility decarbonize the mobility sector
Siemens Energy and Siemens Mobility have signed a Memorandum of Understanding (MoU) to jointly develop and offer hydrogen systems for trains. The agreement was signed by Albrecht Neumann, CEO of Rolling Stock at Siemens Mobility and Armin Schnettler, Executive Vice President (EVP) of New Energy Business at Siemens Energy. The project aims at jointly developing holistic hydrogen solutions for rail transport and offering them to customers to promote the hydrogen economy in Germany and Europe and support decarbonization in the mobility sector.
- Calibrant Energy to bundle latest distributed energy technologies and financing expertise of global leaders Macquarie and Siemens
- The joint venture will create Energy-as-a-Service solutions from a full range of energy technologies for corporate and municipal clients
Macquarie’s Green Investment Group (GIG), Siemens Smart Infrastructure and Siemens Financial Services (SFS) today announced the formation of Calibrant Energy (Calibrant), a joint venture that offers comprehensive onsite Energy-as-a-Service (EaaS) solutions at no up-front cost for its customers, which include corporate and industrial clients, as well as municipalities, universities, schools and hospitals.
The photo artist Herlinde Koelbl presents her international “Fascination of Science” project for the first time. She portrays 60 renowned Nobel Prize winners and scientists. Siemens Arts Program supports the project. The opening ceremony will take place at the Berlin-Brandenburg Academy of Sciences and Humanities in Berlin on October 2, in the presence of the artist and the Managing Board of Siemens AG.