- One single device for lines of up to 500 km
- Monitoring for powered, unpowered or grounded lines
- Highly precise localization of line faults
- Simplifies maintenance and increases network reliability
Siemens Smart Infrastructure recently launched its new PowerLink CM, a condition monitoring solution for high-voltage AC and DC transmission lines. To ensure reliable power supply, optimize grid utilization and prevent blackouts the device is designed to precisely locate faults in the transmission grid and continuously track line conditions. One single PowerLink CM device is sufficient to monitor line lengths of up to 500 km. Faults as well as line condition can be detected in powered, unpowered or grounded lines. Fault reports are received by the affected substation and are forwarded from there to the control room. For continuous line monitoring, the device can be connected to MindSphere, the open cloud-based Internet of Things (IoT) platform from Siemens, which facilitates transparent processing of all line data in the cloud. This allows grid operators to analyze status reports and optimize maintenance activities.
- Charging, medium and low-voltage technology for two carports at Hamburger Hochbahn AG’s Alsterdorf bus depot
- Space-saving installation as technical center on carport’s roof
- Important step for transitioning to climate-friendly local transport in Hamburg
Siemens Smart Infrastructure won a major contract from Hamburger Hochbahn, the largest local transport provider in the Hanseatic city. Siemens will equip two of the six carports at the Alsterdorf bus depot with a total of 96 charging points as well as medium and low-voltage technology. Operations are scheduled to start in summer 2021. With a total of 240 parking spaces, it is one of the largest and most modern bus depots for electric buses in Europe.
- Siemens and Hassan Allam Construction to build new control center located in Egypt’s New Administrative Capital
- Customer is Egyptian Electricity Transmission Company
- Latest software to monitor, manage and control extra-high voltage transmission networks and power generation plants across the country
- Contract worth more than EUR 45 Mio.
Egyptian Electricity Transmission Company has awarded a contract to the consortium consisting of Siemens Smart Infrastructure and Hassan Allam Construction to build the new National Energy Control Center in the New Administrative Capital of Egypt. The country’s new power grid control center will deploy advanced software and equipment to monitor, manage and control extra-high voltage (220 kV and 500 kV) transmission networks and power generation stations across Egypt. The necessary technologies will be included in the new control center for future grid expansion while maintaining secure energy supply, including intermittent renewable energy sources and storage. The project is expected to be completed by the end of 2022.
- FIA and Siemens extend partnership to provide the ‘FIA Mobility Advocate’— a unique software and hardware toolkit — for FIA Mobility Member Clubs to strengthen advocacy of future transport solutions
As an
“Official Supplier of Urban Mobility Advocacy Solutions” for the Fédération Internationale de l’Automobile (FIA), the governing body of world motor sport and
the federation of the world's leading motoring organisations, Siemens plans to
develop a toolkit of software solutions for FIA Member Clubs to help them
provide an evidence-based approach to advocate for the implementation of mobility
policies and strategies. The ‘FIA Mobility Advocate’ combines modeling for
mobility, autonomous vehicles, and the environment, with enhanced analysis
outputs to help meet current future mobility goals.
- Sitrans CC240 IOT gateway provides standardized access to the lifecycle data of HART® devices
- Reduced service effort thanks to faster identification and removal of measuring and parameterization errors without additional parameterization tools
- Compatible with all OPC UA client applications
- Direct connection to Siemens MindSphere
- Numerous possible applications for on and off-premise solutions
Siemens presents the Sitrans CloudConnect 240: a new IOT gateway for the process industry. It provides a second data channel, completely independent of the control system, which is used to transmit data from any HART®-based field devices to the IT world.
- Closed system operation for patients and medical personnel’s safety
- Contamination protection with flexible, scalable HVAC control solution
- Compliant with healthcare industry standards
- Easy installation and operation from anywhere
Siemens Smart Infrastructure (SI) has teamed up with Auto-Info to jointly develop a modular COVID-19 examination unit. The mobile lab structure and system have been designed to avoid contamination among patients or from patients to medical staff by using the Climatix IC platform, a flexible and scalable advanced HVAC control solution from Siemens.
-
White Space Cooling Optimization for highly efficient greenfield data center in Paris region
- Intelligent, continuously learning solution to support data center’s 24/7 availability and energy efficiency
Siemens Smart Infrastructure is supplying the first Tier IV-certified data center in the region of Paris, France. The “Thésée” data center will meet the highest industry standards for availability and energy efficiency. Siemens will install its White Space Cooling Optimization (WSCO) smart solution to optimize the building’s energy efficiency as well as the thermal protection of the server rooms by automatically adjusting the operation of the cooling systems.
- Charging technology for 37 new electric buses installed at West London depot
- Fully electric-enabled bus garage incorporates power infrastructure, maintenance and charging facilities
- Supplying 11 megawatt hours to 37 double-decker buses daily
In partnership with Tower Transit, a bus operator in London and part of
the SeaLink Travel Group, Siemens Smart Infrastructure provided the charging
infrastructure for 37 new fully-electric double decker buses in London.
Westbourne Park garage, on the Great Western Road, is the operator’s first
depot in London incorporating fully electric routes with power infrastructure,
maintenance and charging facilities. Bus routes 23 and C3 operate from the
Westbourne Park site, with the first few Optare Metrodecker zero-emission
double-deckers already in operation, the remaining fleet is expected to be in
service in the next months.
- Siemens and Merck announce project partnership
- Cooperation will drive forward modular production (Plug&Produce) based on the MTP and POL standard
- Quick adaptation to process requirements with little effort
- A one stop solution with hardware and software components from Siemens
Siemens and science and technology company Merck will work together in future at Merck's headquarters in Darmstadt to develop a technical backbone for the modular production of the future. The aim is to create a production line that flexibly combines various individual process modules and to use Module Type Package (MTP) and Process Orchestration Layer (POL) technology to drastically reduce engineering effort. At the same time, it should be possible to adapt quickly to process requirements. With its integrated product range covering all production levels (field to MES), Siemens is able to provide all the necessary hardware and software components from its own product portfolio.
- Early detection of anomalies in the drivetrain with the support of artificial intelligence
- Trend Prediction for optimized maintenance efficiency
- Higher productivity and reduced machine and system downtime
Siemens has supplemented the Mindsphere application Predictive Service Assistance with an AI-based module. The new Artificial Intelligence module identifies concrete fault patterns in motors at an early stage, such as misalignment or a defective bearing. The application thus helps users to reduce downtimes and further improve spare parts and maintenance processes. The new Artificial Intelligence module for motors uses a neural network to solve what was previously implemented using a defined KPI limit value. This enables the module to detect anomalies even before the defined limit value and provides clear indications of the type and severity of faults and their development. As soon as the application detects signs of an error, it warns the user and generates a due date that indicates when the error should ideally be corrected and what corrective action is recommended to prevent an unplanned downtime. Predictive Service Assistance with the new AI-based Artificial Intelligence module is offered as part of a Predictive Service Assessment. The package includes a customized configuration service that ensures that the Mindsphere application with the new AI-based module runs optimally according to the customer's requirements.