Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Simply digital: Siemens process instrumentation presents new Sitrans CC240 IOT gateway

Siemens presents the Sitrans CloudConnect 240: a new IOT gateway for the process industry. It provides a second data channel, completely independent of the control system, which is used to transmit data from any HART®-based field devices to the IT world.

In the process industry, field instrumentation is a central source of data, when it comes to digitalization. The Sitrans CC240 IOT gateway establishes a second data channel, which makes field level data that was previously hidden available to the user – without adversely affecting the existing control technology. The system creates a direct connection between the field device and IT or the cloud and reads not only basic process values but also identification, configuration, and diagnostics parameters – for any HART® device of Version 5 or later. The system then makes this data available via an OPC UA server or the Siemens MindSphere IoT-as-a-Service solution. 
The data is harmonized in line with the Namur Open Architecture information model. This creates a standard perspective on the installed base - regardless of the technology and manufacturer - which means that digital applications can be created for the first time, for both on and off-premise environments. For example, asset monitoring and management solutions can be implemented, particularly for smaller plants. Sitrans CC240 supports the connection of up to 64 devices and has an on-board web server with the necessary configuration options and management views so that additional tools are not required.
The available connectivity options also mean that it can be integrated into existing systems. OPC UA can be used to transfer field device values and data directly to automation or IT systems, for example for performing calculations or analyses outside the actual control task. The connection to MindSphere supports the distributed use of several Sitrans CC240 systems – ideal for monitoring globally distributed assets on a central instance. 
With Sitrans store IQ from Siemens, the user has an app for stock monitoring and management in production and logistics. Filling levels of tanks, silos, racks or other storage facilities are measured and acquired, then transmitted via the Sitrans CC240 or familiar MindConnect gateways to Siemens MindSphere. Sitrans store IQ visualizes the acquired data and also generates alarms and events. The application is available for desktop and mobile devices.
These can be user-defined and could for example trigger notifications via SMS or e-mail. The open system has many advantages – it is possible to customize the structure and display, and to acquire and process any desired variables. For the management of materials and the necessary infrastructure, the user often requires not only the central filling level information but also supporting measurements such as temperature, pressure, humidity, or binary inputs. The cloud technology supports full scalability, which goes hand in hand with the flexibility of Sitrans CC240. Sitrans store IQ can therefore be used for anything from a few local containers to larger tank farms or even globally distributed infrastructures.  The structure and presentation can be individually configured according to the user’s requirements.
For further information about Sitrans CC240, please visit
www.siemens.com/sitranscc240
For further information regarding the Digital Enterprise SPS Dialog 2020, please see
www.siemens.com/sps-dialog
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Read more

Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. Active around the world, the company focuses on intelligent infrastructure for buildings and distributed energy systems and on automation and digitalization in the process and manufacturing industries. Siemens brings together the digital and physical worlds to benefit customers and society. Through Mobility, a leading supplier of intelligent mobility solutions for rail and road transport, Siemens is helping to shape the world market for passenger and freight services. Via its majority stake in the publicly listed company Siemens Healthineers, Siemens is also a world-leading supplier of medical technology and digital health services. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power that has been listed on the stock exchange since September 28, 2020.

In fiscal 2020, which ended on September 30, 2020, the Siemens Group generated revenue of €57.1 billion and net income of €4.2 billion. As of September 30, 2020, the company had around 293,000 employees worldwide. Further information is available on the Internet at www.siemens.com.

Read more
Reference Number: HQDIPR202011266074EN

Contact

Evelyne Kadel

Digital Industries

+49 (173) 56 48 709