Control rooms of process engineering plants are usually
as old as the plant itself, often 30 years and more. Today, digital
transformation is placing new demands on automation: Simatic PCS neo is a brand-new system software, which
offers companies in the process industry unique opportunities in the age of
digitalization. Main features include global web-based collaboration in
engineering and operation and intuitive handling representing all relevant
information in a single workbench.
Bane NOR, the state-owned agency responsible for the Norwegian national railway infrastructure, has contracted Siemens to upgrade the signaling equipment of the entire Norwegian rail network to the European Train Control System (ETCS). Commissioning of the rollout lines is scheduled to be completed by 2034. The contract also includes services for 25 years and is worth around 800 million euros in total.
The VAG Verkehrs-Aktiengesellschaft Nuremberg has ordered 27 type G1 four-car metro trains from Siemens Mobility. The contract also includes an option for a total of a further 7 trains. These trains are earmarked for service on Nuremberg's U1 line. The trains will be built in the Siemens Mobility plant in Vienna. Core components of the G1 will be manufactured in the Nuremberg metropolitan area and include such products as the drive converters, traction motors, auxiliary converter units and control equipment. The project management, development and service support will be provided from Erlangen.
Let the good times roll: Starting September 21, about six million people from all around the world will be enjoying themselves at the Oktoberfest in Munich for two weeks. Traditionally, Siemens supplies drives and control systems as well as energy distribution for the festival's rides. Automation solutions from Siemens also control special beer pipelines – the only ones of its kind worldwide –that supply the Hacker, Winzerer Faehndl and Braeurosl festival tents with their tasty Oktoberfest brews. Because many breweries use Siemens technologies within their brewing process, Siemens doesn't only ensure fresh beer at the Oktoberfest.
Austrian Federal Railways (ÖBB) has ordered a total of 189 Desiro ML regional trains from Siemens. The trains will operate under the name "Cityjet".
The trains will be produced at the Siemens Mobility plants in Krefeld, Germany, and Graz, Austria, and final assembly will take place at ÖBB's Technical Services factory in Jedlersdorf, Austria.
Two design alternatives of the Desiro ML are built: the urban train design for large metropolitan areas such as Vienna and the regional train design. The ÖBB cityjet also offers a variable, low-floor seating arrangement as well as spacious entrance and intercar gangway areas, an attractive, innovative design and maximum riding comfort, and barrier-free entrance to all 550-mm station platforms in Austria.
Austrian Federal Railways (ÖBB) and Siemens Mobility are jointly investing in the future of passenger transport and are developing an electro-hybrid battery drive for trains. Operating as a battery-powered train, the Cityjet eco is an alternative for non-electrified rail lines primarily served at present with diesel-powered passenger trains. Battery operation can reduce CO2 emissions by up to 50 percent compared to diesels. Following extensive testing of the prototype train, it is expected to first be used in passenger service in the second half of 2019.
On August 26, the joint project reached its next milestone: The battery driven EMU got the homologation and is starting passenger service beginning of September 2019, bringing more sustainability to non-electrified tracks in Austria.
Wiener Linien commissioned Siemens at the end of 2017 with the delivery of 34 fully automated metro trains. The contract also includes the maintenance of the trains for a period of 24 years and an option for an additional eleven trains. The "X cars" will be operated fully automated on the new U5 line in Vienna beginning in 2024. The trains can also operate semi-automated or manually on previously existing lines. Delivery of the trains is scheduled to begin in mid-2020 and to be completed by 2030. The trains will be manufactured at the Siemens factory in Vienna.
As urban populations continue to grow, the need to provide
reliable and efficient transportation that allows passengers to connect
seamlessly door-to-door becomes more critical. From public transportation to
ride-sharing, bike-sharing and scooter-sharing, passengers are increasingly
looking for options that allow them to select their transportation options on
demand, planning and paying for their commutes in one easy-to-use application.
Together, Siemens Mobility, HaCon, eos.uptrade, Bytemark and Padam are
providing these digital solutions that are making commutes easier and faster.
In September 2012, Munich city utility company (SWM) was the first customer to order the new Avenio for the light rail network of the MVG (Munich transport company). In the meantime, SWM has continually expanded its Avenio fleet.
Siemens Water Solutions successfully installed and started up a Zimpro® wet air oxidation (WAO) system at a global petrochemical company’s olefins plant in the Southern U.S.
The order, received in November 2017, is the second Zimpro® wet air oxidation system supplied to the customer. The first system was supplied in 2004.
The Zimpro® WAO system will treat spent caustic generated in the production of ethylene by destroying odorous and high chemical oxygen demand (COD) pollutants. The system also generates an effluent that can be safely neutralized and sent to a biological treatment plant, where it is further treated for discharge.
Siemens Water Solutions addresses water and wastewater needs of the oil and gas industry with a portfolio that includes physical and chemical separation, biological treatment, and complex hydrothermal technologies.