- Voltage variant of Sinamics G120X for USA and Latin America
- Save space with new size for the Sinamics V20
- Adapter kit to physically and thermally separate power module and control unit for Sinamics G120
With numerous innovations, Siemens is extending its drive portfolio, improving user-friendliness and offering space-saving installation options. The Sinamics G120X converter, designed specifically for use in water/wastewater applications and in HVAC systems, is now also available in a three-phase 3AC 200V voltage variant in the power range up to 55 kW. This means that the converters can now be integrated seamlessly into applications in the USA and in Latin America. Due to its robust construction and the coating of the PCBs according to 3C3 standard the converter is suitable for harsh environments. The new module for extending the digital and analog inputs and outputs increases the flexibility and the optimal control of converter-guided applications. The Sinamics G120X now also supports the communication protocols Profibus, Modbus RTU, USS and BACnet MS/TP. It is equipped with extensive interfaces and can be easily integrated into existing or new systems.
- Intelligent infrastructure used on three bus routes in Manhattan and Brooklyn
- Helps ease congestion and improve efficiency
- Sophisticated solution identifies violations and length of stay
Siemens Mobility has successfully launched an Automatic Bus Lane Enforcement (ABLE) solution in New York City, representing the first-ever application of this technology to be mounted on buses. The ABLE systems are installed on M15 Select Bus Service buses that operate on bus lanes benefitting more than 44,000 daily customers. The technology is playing a key part in New York City’s drive to improve bus speed and efficiency and to keep traffic moving on the city’s congested streets.
- Seven four-car Desiro Mainline trainsets ordered
- To serve in the Verkehrsgesellschaft Mecklenburg-Vorpommern rail network
- Subsequent capacity expansion to four-car trainsets ensures sustainable value creation over the entire lifecycle
Alpha Trains, the European continent’s largest leasing company for rail rolling stock, has ordered seven Desiro Mainline (ML) regional trains from Siemens Mobility. Ostdeutsche Eisenbahn GmbH (ODEG) will lease the trains for service in the rail network Baltic coast east operated from December 2019 onwards by the ODEG on behalf of Verkehrsgesellschaft Mecklenburg-Vorpommern (VMV). The production has already started at the Siemens Mobility train manufacturing facility in Krefeld. “Alpha Trains ordered the Desiro ML as its first customer many years ago and we are pleased that this proven and reliable platform is also used for this project” said Thomas Schmidt, Managing Director of Alpha Trains Europa GmbH.
- New power output module boosts HCS4300 heating control system performance
- HCS4200: space-saving solution for use in flat control cabinets with new CIM4210C central interface module
- Simple, convenient engineering and commissioning of industrial heating processes with TIA Portal
Siemens
has equipped the modular Siplus HCS heating control systems for
switching and controlling heater fields and elements with a new power output
module (POM) and a central interface module (CIM). With more power per output
and a space-saving solution for mounting in flat control cabinets, the flexible
heating control system is now even more versatile, and can be used for example
in applications with heat registers.
- Shorter development and commissioning times
- Software libraries enable standardization
- Commissioning tests on virtual test rack
The new Sinumerik One CNC generation is at the heart of digital transformation for machine tools. As a digital native, the controller features not only a new hardware platform, but also versatile software for the creation of a digital twin. It closes the gap between the virtual and the real world and helps to reduce development and commissioning times considerably.
- ETCS approval for Baseline 3 in Germany and Sweden
- Improved availability thanks to intelligent infrastructure
- Approval for other countries to follow
Germany’s Federal Railway Authority (EBA) has approved the Vectron locomotive for operating in Germany with the European Train Control System (ETCS) Baseline 3. Approval for Sweden has already been received. Additional countries will follow.
- Next generation of Simatic ET
200eco PN: New functions for modern machine concepts and requirements
- For use in redundant,
high-availability systems thanks to S2 redundancy
- High current-carrying capacity with
power supply via L-coded plug
- High-quality industrial enclosure with IP65/67
protection for outdoor use
Siemens has launched a new generation of machine-level block I/O
devices in the form of the Simatic ET 200eco PN. The new I/O family with
IP65/67 degree of protection includes five digital I/O devices as well as an IO-Link master device and offers users a whole range of new
functions for modern machine concepts and requirements. In their new industrial
metal enclosure, the devices are reliably protected from UV radiation and
harmful substances even under adverse environmental conditions, making it
possible to use the devices outside of factory buildings. The devices are
supplied with power via an L-coded plug, resulting in a considerably higher
current-carrying capacity. In turn, this enables longer cable routes in the
field, and the supply and connection of more energy-intensive components (such
as valve terminals) without the need for more supply cables.
- Siemens
industrial gas turbines will provide peaking power to help improve the
reliability and flexibility of the Belarusian power grid
Siemens will deliver the power generation equipment for two
new peaking power plants in the Republic of Belarus. The customer is the
state-owned utility company RUE Vitebskenergo. The new plants will be operated in
conjunction with the existing Lukomlskaya and Novopolotskaya power
plants in
the Vitebsk region in northern Belarus and will help ensure the
reliability and flexibility of the country’s power grid. The plants are expected to go into
operation in the end of 2021.
- Simatic S7-1500
firmware V2.8: Secure data integration, versatile diagnostics function for OPC
UA server
- Simatic S7-1200 firmware V4.4:
Improved cross-platform data transfer, OPC UA Data Access as server, OPC UA
Modelling Editor
Siemens announces the release of two firmware updates for
Simatic controllers that provide new functions. The Simatic S7-1500 firmware
V2.8 from Siemens improves cross-device capabilities for data integration and
diagnostics functions. The new Simatic S7-1200 firmware V4.4 extends the
communication functions of the Simatic S7-1200, enhancing cross-platform data
transfer with other controllers and higher-level or cloud-based systems such as
ERP, SCADA and Mindsphere. The applications are numerous, ranging from
industrial use to agriculture and infrastructure projects.
- Cooperation aims to test renewable fuels at the Rya CHP plant located in the energy port of Gothenburg
- First phase with Göteborg Energi is to validate 3D-printed burners at the Rya plant
By 2030, the ambition is that all district heating in Gothenburg, Sweden, will be produced by renewable or recovered energy sources. With this in mind Göteborg Energi and Siemens have come together in a cooperation agreement with the aim of testing state-of-the-art gas turbine technology that enables the operation of renewable fuels in the Rya combined heat and power (CHP) plant, which is today powered by natural gas.