- Hybrid project based on biofuel and solar energy inaugurated on the Galapagos island of Isabela
- First of its kind local energy system, developed for carbon-neutral operation
- Remotely monitored from the Siemens-Mindsphere Application Centers in Munich and Austin, Texas
After only ten months of planning and ten months of construction, the hybrid power plant installed by Siemens on the Galapagos island of Isabela was inaugurated. The aim of the project was to convert the current power generation structure, which is based on fossil fuels, to a hybrid system with several primary energy sources. The system is designed to run carbon-neutral with biofuel and solar energy and supplies almost 900 households on the by far largest Galapagos Island with electricity.
- Hybrid power plant solution with integrated battery energy storage
- Power supply with a capacity of 145 megawatts
- Scheduled to start operation in Santo Domingo in spring 2021
Siemens and the marine arm of ST Engineering in Singapore have jointly received an order for a SCC-800 2x1C SeaFloat barge-mounted power plant from Seaboard Corporation subsidiary Transcontinental Capital Corporation (Bermuda) Ltd., an Independent Power Producer (IPP) with operation in Dominican Republic. The project Estrella del Mar III in the Dominican Republic will provide the customer with a highly efficient power generation facility.
- Improved accuracy and repeatability
- Increased asset utilization and decreased operational waste
- Wide range of applications in environmental, chemical, and food and beverage industries
- Hart 7 communications
Siemens presents Sitrans Probe LU240, its newest ultrasonic level measurement Hart transmitter, a hardworking and rugged device that provides reliable level, volume, and flow measurements. Engineered for the challenges of the environmental industry, this transmitter is also suited for the chemical and food and beverage applications. Field-proven Process Intelligence echo processing separates true material level echoes from false, providing reliable readings while still allowing rapid response to actual changes in the material level. The device's reduced blanking distance decreases waste in applications while boosting asset utilization by providing continuously accurate readings even with high levels of material.
- Trafikverket awards 75 million Euro contract
- Siemens Mobility, with Eltel Networks Infranet, to deliver intelligent infrastructure technology
- Communications, control and monitoring systems for tunneling
The Swedish Transport Administration, Trafikverket, has announced that it awarded Siemens Mobility a 75 million Euro contract to deliver communications, control and monitoring technologies for a section of the European route number four (E4), the Stockholm Bypass. The new bypass will connect the southern and northern parts of the surrounding Stockholm communities. The bypass is a 21-kilometer road, including 18 kilometers of tunneling around one of Europe's busiest capitals. It will relieve intercity and main thoroughfare congestion, significantly reducing delays for residents and visitors. The construction of the tunnel started in 2014 and is expected to be completed in 2026. Installation and testing of Siemens Mobility technologies will begin in 2021.
Aker Solutions and Siemens have signed a strategic collaboration agreement to further develop digital offerings in engineering, operations and services. The collaboration focuses on the creation of software applications and joint service offerings including the development of industrial digital twins that will drive efficiency throughout the entire plant lifecycle. In addition, the companies will further develop specific offerings for the oil and gas sector based on Siemens' Comos engineering platform. These solutions will help customers to reduce engineering and operational cost and enable improved decision making. The agreement builds on a long-standing, successful relationship between both companies by combining individual strengths and promoting joint offerings.
- The new plant comprises three compression trains for uninterrupted gas supply to Abu Dhabi industries and Northern Emirates
- ADNOC Gas Processing to utilize up to 450 million standard cubic feet per day (mmscfd) of sales gas, delivered via Maqta-Taweelah pipeline
The Abu Dhabi National Oil Company (ADNOC) inaugurated its Taweelah Gas Compression Plant, ensuring uninterrupted gas supplies to major Abu Dhabi industries and the UAE's Northern Emirates. The plant, located 50 kilometers north of Abu Dhabi, will utilize up to 450 mmscfd of sales gas, delivered to the facility by ADNOC Gas Processing's recently installed Maqta-Taweelah pipeline.
- TÜV Süd certified process for system integration and solution project processing in conformity with IEC 62443-2-4 and -3-3
- Security documentation in conformity with IEC 62443
- Implementation of certified solutions with Simatic PCS 7
- Standardized processes reduce outlay for customers
Siemens is the world's first company to gain TÜV SÜD certification for the secure system integration of process automation and drive solutions in compliance with the international IEC 62443-2-4 standards. The integration projects, verified on the basis of two standard solutions in the oil & gas processing industry and in a waste incineration plant, have been certified in conformity with IEC 62443-2-4 and -3-3 and were implemented using the Simatic PCS 7 process control system. The projects involved process automation, drive solutions and comprehensive security measures and functions designed to deliver secure plant operation. The certification has a whole range of advantages to offer for customers: plant operators benefit from the precise definition of requirements, the implementation of standardized automation solutions and processes, and from the availability of documentation in conformance with standards. This documentation provides a vital foundation for verifying compliance with the technical requirements of the IT Security Act and other cyber security standards, for the sustainable improvement of IT and OT system security, and for guaranteeing the security of general supplies. The system solutions are used in sectors involving a critical infrastructure, such as waste management and the oil and gas industry.
- Edge Devices to collect and process large data volumes directly at the machine
- Secure, future-proof basis for the execution of Industrial Edge applications
- Simple update procedure and software rollouts through secure link to central Edge Management System
- Savings through edge computing in the Siemens Electronics Factory Amberg
At the SPS IPC Drives 2018 in Nuremberg, Siemens will be showcasing a newly developed hardware platform for edge applications as part of its Siemens Industrial Edge concept: The compact Simatic Edge Device works on the basis of the embedded industrial PC Simatic IPC227E, and features integrated connectivity to automation on the machine level. This allows manufacturing data to be captured and processed directly at the point of production. If there is a change to the framework conditions underlying the industrial application, Industrial Edge offers facility to adjust software applications on the Edge Device, keeping them right up to date using functional, feedback-free updates. The hardware comes with a closed all-metal housing, ensuring maximum industrial functionality for flexible, maintenance-free use under even the harshest of conditions. Rapid commissioning is guaranteed using pre-installed Edge software.
The Supervisory Board of Siemens AG has extended the appointment of Managing Board member Lisa Davis (55) ahead of schedule. Her term of office will now continue until the end of October 2020. This move is a sign of continuity in the context of the implementation of the company's new Vision 2020+ strategy program. Her contract will subsequently extend automatically by one year until the end of October 2021, provided that neither Lisa Davis nor the Supervisory Board objects.
- Industrial PC for use as an IoT gateway enables data to be managed directly in the production environment
- Based on Windows or Linux, for networking machinery of different manufacturers and of different technological versions
- Fitted with up to 3 LAN interfaces for high connectivity
- Pre-configured versions available from stock
Siemens has expanded its product portfolio of Simatic industrial PCs to include the Simatic IPC127E. The newly developed industrial PC is suitable, for example, for use as a gateway and enables data to be managed directly in the production environment. Whether it is based on Windows or Linux, the Simatic IPC127E makes it possible to network existing systems with machinery of different manufacturers and different technological versions. Thanks to the compact enclosure of just 0.3 liters, it can be integrated with a minimum space requirement in the cabinet or directly at the machine.