Under the motto "Industrialize Additive Manufacturing" Siemens presented its comprehensive solution portfolio for consistent digitalization of additive manufacturing at the formnext 2018, the leading exhibition for additive manufacturing. Starting with the design and engineering software, via innovative simulation tools to complete machine and factory automation, Siemens demonstrated how the industrialization of additive manufacturing can be further accelerated. Furthermore Siemens introduced solutions around peripheral processes, such as automated support removal, surfaces finishing and part removal as well as post processing for intelligent de-powdering solutions. Additional, Siemens presented new business models, which have derived from digitalization in this industry.
- Sidrive IQ improves drive systems along the entire life cycle up to the megawatt range
- Cloud-based application based on networked drive systems from Siemens
- Increased productivity, reliability and ease of maintenance
- Standardized link enabled by Sinamics Connect 500 and Simotics Connect 600 connectivity modules
Sidrive IQ from Siemens provides a digital platform enabling the evaluation and utilization of data gathered from drive systems. On the basis of networked drive systems from Siemens, this cloud-based application is now also available for motors and converters in the medium and high-voltage range. This opens up an array of benefits for plant and machine operators, from optimized maintenance activity and maximum availability to increased productivity, from low outputs through to the megawatt range across the entire life cycle. Connectivity modules such as Simotics Connect 600 and Sinamics Connect 500 enable high-voltage motors and medium-voltage converters to be simply linked up to Sidrive IQ. With the latest generation of its Remote Services and Condition Monitoring Services offered as part of the Sidrive IQ Services portfolio, Siemens is making available corrective measures for fixing faults, preventive maintenance offers and proactive services for optimized performance. The optimized drive systems are used in pumps, fans and compressors across different sectors of industry such as oil and gas, mining, food and beverage, water and wastewater, metals and cement.
The AMB, the International Exhibition for Metalworking, was open from September 18 to 22, 2018 in Stuttgart. Under the motto "Digitalization in Machine Tool Manufacturing - Implement now!", Siemens demonstrated to users and manufacturers of machine tools how end-to-end digitalization solutions work from the machine tool right up to the corporate management level and the cloud.
From September 4 to 7, Siemens was at SMM under the banner "Welcome to the Digitalization at Marine – implement now," with an exciting presentation showcasing the entry of digitalization into its marine portfolio. At Booth 318 in Hall B6, Siemens exhibited its broad spectrum of drive technology, automation and digitalization services and solutions for shipbuilding and marine operations. Highlights of this year's trade fair presentation included a virtual reality representation of the Siship as well as the smart web-based data application Siship EcoMAIN. Siemens also featured integrated solutions for the (partial) electrification of ships using uniform topology with the latest members of its Siship BlueDrive Family. As well as moving over functional features familiar from Siship EcoProp under the name Siship BlueDrive Eco, Siemens also offered visitors a glimpse into its own battery production and presented a partner in the field of fuel cell-based power supplies for the commercial sector.
Siemens exhibited at the automatica 2018 with an array of integrated and user-oriented Digital Enterprise solutions designed to sharpen the competitive edge of both end users and machine builders. Exhibiting under the banner "Digital Enterprise – Implement now!", Siemens focused on ways in which industrial enterprises of all sizes can benefit from the digital transformation – along the entire value chain from product design and production planning through the engineering process to new services.
World Forum and Leading Show for the Process IndustriesUnder the motto "Accelerate the digital transformation – from integrated engineering to integrated operations." we presented at the Achema 2018 trade show specific applications for how to use the potential of digitalization to enhance efficiency, flexibility, and quality – and to shorten time to market. Production can be significantly optimized and made more flexible by integrating all components in instrumentation and control and management systems and by intelligently using all of the process data generated in a common data model – the digital twin of the overall plant. Maintenance effort and costs can also be slashed dramatically by using cloud-based applications and data-based services.
Industry is advancing in giant strides towards digitalization and the utilization of IoT functions and applications. With MindSphere, Siemens has developed a cloud-based open IoT operating system with high performance capability to meet this growing demand.
To provide optimum support for companies facing individual, industry-specific challenges surrounding the digital transformation, January 24, 2018 saw the launch of a worldwide IoT initiative by MindSphere users and Siemens.
Scandinavia is the first region in the world to rely increasingly on battery-powered and thus environmentally-friendly technologies in the shipbuilding industry. After "Ampere", the world's first electrical ferry in Norway, and a follow-up order of the Finnish shipping company FinFerries, Siemens has now received an order from Norwegian ferry operator Fjord1. Ampere was put into operation in Norway in May 2015, and has traveled a distance equivalent to more than 1.5 times around the equator. With the change from diesel propulsion to battery, Norwegian ship owner Norled has reduced the cost of fuel by 60 percent. Now Siemens has tailor-made a suitable technical solution for Fjord1. With this contract, the first four battery-driven ferries in the world will run on technology developed and manufactured by Siemens.
"Elektra" - the newest member of the electric ferry fleet: In June 2017, the Elektra began regular operation between Nauvo and Parainen in the Turku archipelago. Battery packs, which are charged via the land-based charging stations in the harbor for use by the ferry, serve as the primary source of energy, with Diesel engines used as emergency power units. The Elektra is also Europe's largest car ferry. At nearly 98 meters long and 16 meters wide, the Elektra can transport up to 90 cars per trip. The ferry purchased by FinFerries will now be traveling this route every 15 minutes. The batteries will be charged in roughly five minutes while cars move off and onto the ferry. The two lithium-ion batteries each have a capacity of 530 kWh.