- Siemens to supply 19 net-gas, off-gas and recycle gas compressors for crude flexibility project
- The project will enable the refinery to process up to 420,000 barrels per day of offshore crude oil
Siemens was recently selected to provide 19 process reciprocating compressors for ADNOC Refining’s crude flexibility project at Ruwais Refinery-West. The project is intended to increase the refinery’s crude processing flexibility, enabling the site to process up to 420,000 barrels of oil per day of the local crude grade known as Upper Zakum, which is found offshore. The upgrade will improve the value of each barrel of oil and allow ADNOC to export more of its main onshore, lighter-grade Murban crude.
- ETCS Baseline 3 train equipment for cross-border operation
- Commissioning approved for 12-car train
- Service on the Berlin – Munich route planned for timetable change in December 2018
Germany's Federal Railway Authority (EBA) has approved the ICE 4 for operation with the European Train Control System (ETCS) in Germany. With this approval, the passenger service can begin as planned on the Berlin – Munich route, which is equipped with the system. The ICE 4 is scheduled to operate on this line when German train operator Deutsche Bahn (DB) changes its timetable on December 9, 2018.
- Awarded Suzhou Metro Line 5 and Nanjing Metro Line 7 fully automated signaling system projects
- Trainguard MT is the state-of-the-art Communications Based Train Control (CBTC) system
Siemens Mobility was recently awarded the fully automated CBTC system for two key Chinese metro lines in Eastern China: Suzhou Metro Line 5 and Nanjing Metro Line 7. The cities, which collectively have more than 12 million residents, are two of the largest cities in the region. China's rapid urbanization in both cities requires fast and intelligent planning of transportation systems that will ease congestion and provide passengers a more reliable and efficient commute. Initial operations for both lines are planned for 2021.
- Research project for an optimized transport system (OTS)
- Mobility offering for the first and last mile
- Testing the interplay of intelligent infrastructure, cloud-based software services and autonomous electric vehicles
Siemens Mobility is launching a field test for autonomous driving at the Siemens campus in Munich-Perlach, Germany. Working with partners IAV GmbH, Institute for Climate Protection, Energy and Mobility (IKEM) e.V., emm Solutions GmbH, UTB Projektmanagement GmbH and the Technical University of Munich (TUM), Siemens Mobility is initiating a research project and field test. The test route runs through the campus and enables traffic simulation in a variety of real-life situations.
- Fulcrum's municipal solid waste-to-fuels plant will contribute to a sustainable future
Abengoa, a Spanish engineering, procurement and construction (EPC) contractor, recently selected Siemens to supply a compressor train for Fulcrum BioEnergy's Sierra BioFuels Plant that will use gasification technology to produce low-carbon fuels from municipal solid waste. The plant will be located in Storey County outside of Reno Nevada and is expected to produce approximately 11 million gallons of biofuel per year that will be used by the aviation industry.
- Padam is a fast-growing Software as a Service (SaaS) provider for on-demand transport
- Padam closes an investment round with strategic investment of Siemens Mobility
- Enhances Siemens Mobility's intelligent infrastructure portfolio for intermodal mobility
- The transaction was executed in October 2018
- Padam remains a standalone, founder-led company
Siemens Mobility and Padam, headquartered in Paris, France and a fast-growing turnkey AI-powered technology provider that operates on-demand transport (microtransit) services, are launching a partnership to enhance demand responsive transportation options and improve passenger experience. The investment will enhance Siemens Mobility's intelligent infrastructure portfolio that is focused on intermodal transportation, offering public transportation operators a first/last mile transportation solution that optimizes vehicle utilization at lower costs. Siemens has made a significant investment in Padam. Both companies have agreed to maintain confidentiality regarding financial details of the deal. Padam's white-label platform, Padam Live, is a software platform that is rebranded by public transportation operators to integrate microtransit services. It offers cities worldwide an advanced management system.
- Siemens' Sitraffic ESCoS roadside unit set to become a new industry standard for V2X technology
Siemens Mobility, Inc. is pleased to announce it has received OmniAir Certification for its Sitraffic ESCoS roadside unit (RSU), the first roadside unit to receive OmniAir's commercial, connected vehicle certification. Siemens' RSU is one of the few RSUs today that meet U.S. Department of Transportation FHWA specification version 4.1. Now with OmniAir's certification, this roadside unit is well-positioned to become the established standard and a key component for V2X device communications today.
- Metro Automation for Paris' future metro lines 15, 16 and 17 awarded
- The three new lines include 125 kilometers of tracks and 50 stations
- The project entails 12 phased sections and commissioning by 2030
- Most advanced signaling technology to equip 159 passenger trains and 27 work trains
- Associated maintenance services for 30 years
The Société du Grand Paris (SGP), which owns the Grand Paris Express project, awarded the Siemens Mobility and Thales consortium with the delivery of the Automated Train Control system that uses wireless Communications-Based Train Control (CBTC) technology and the Operating Control Centers for the future new lines 15, 16 and 17, which will be completed by 2030. Siemens Mobility will design and implement the most advanced generation of its CBTC fully automated technology. It will complete the integration of the entire transportation system. Thales will design and implement the Operating Control Centers (centralized supervision of train traffic, energy systems, auxiliary equipment and digital information systems), as well as trackside equipment and a secure communication network.
- Order for 18 7-car trainsets and 50 power cars
- Delivery to begin in summer 2021
- Power car principle provides maximum flexibility
New trains for growing number of long-distance passengers: Deutsche Bahn (DB) is expanding its fleet and has ordered an additional eighteen 7-car ICE 4 trainsets and 50 more power cars from Siemens Mobility. With these new power cars, 50 ICE 4 trainsets, previously ordered in a 12-car configuration, can be extended to 13 cars. This flexible configuration is made possible by the train’s innovative traction drive technology and its completely new train control system. Delivery of the ordered 7-car trainsets is expected to begin in the summer of 2023. Delivery of the 13-car trainsets will begin after delivery of the 50 12-car trains is completed in 2021. The order has a total value of around €610 million. Bombardier Transportation will supply approximately one-third of the order.
- Siemens Mobility provides intelligent road infrastructure including, Road Side Unit (RSU), communications networking and telematics for near-real-time exchange of information between vehicles and infrastructure
- Facility uses automated and connected vehicle technology to prepare for tomorrow's roads
Today, the city of Düsseldorf officially opened a cutting-edge automated and connected vehicle test track, which is a 20 km road dedicated to the advancement of connected and autonomous vehicle technology. Featuring Siemens Mobility technology, the digital test field highlights the latest intelligent traffic technologies, which is preparing the region for automated and autonomous traffic of the future.