- New order will bring eight S70 low-floor streetcars to the OC Streetcar project
Siemens Mobility today announced that it has been awarded a contract from the Orange County Transportation Authority (OCTA) for eight streetcars. The contract includes spare parts and tools, and comes with the option to purchase up to 10 additional streetcars at a later date. Siemens will provide systems support and training to operators and maintenance technicians once the vehicles are delivered, expected early 2021.
- Heat and power for the Rhine-Ruhr metropolitan region
- Fuel efficiency exceeding 85 percent
- Long-term service agreement
Siemens and STEAG GuD Herne GmbH signed an agreement today on the turnkey construction of a combined cycle power plant with district heat extraction. They also entered into a long-term service agreement. The Herne 6 plant will have an electrical capacity of more than 600 megawatts (MW). Steam will also be extracted, and the thermal energy obtained will be used for the district heating grid of Germany's Rhine-Ruhr metropolitan region. Never before has a single power plant unit been able to provide 400 MW of (thermal) district heat with combined cycle operation. The overall fuel efficiency of the natural gas used thus climbs to more than 85 percent, making the power plant one of the world's most efficient and most environmentally friendly plants. The investment volume for Herne 6 is in the mid-triple-digit euro range.
- Siemens' Travel Sense application allows RSUs to collect anonymized data from passing vehicles -- via Wi-Fi, Bluetooth or DSRC -- and make it available on the cloud, eliminating the need for additional hardware.
Siemens Intelligent Traffic Systems announced it is now making travel time and traffic congestion gathering capability available on its popular ESCoS Roadside Unit (RSU) via a new cloud application called Siemens Travel Sense, an easy-to-use data analytics platform and a game-changer for agencies wanting to consolidate units offering different capabilities. This additional capability now adds to Siemens' impressive lineup of already-supported CV RSU applications which includes: Time-to-Change, Curve Speed Warning, Variable Speed Limit, Wrong Way Entry, Exit Ramp Deceleration Warning, Work Zone Warning, Transit Signal Priority, Emergency Vehicle Preemption and Pedestrian Collision Warning.
On March 2nd, 2017, German Chancellor Angela Merkel, Egyptian President Abdel Fattah El-Sisi, Siemens CEO Joe Kaeser and further high-ranking representatives witnessed the symbolic inauguration of the first phase of Siemens' megaproject in Egypt. The event marked an important milestone towards the completion of the project.
In collaboration with the Egyptian Ministry of Electricity and Renewable Energy, Siemens and its consortium partners, Orascom Construction and Elsewedy Electric, announced on July 24, 2018 the completion of the Egypt Megaproject in record time. The parties celebrated the combined cycle commissioning and the start of operations at the Beni Suef, Burullus and New Capital power plants. The stations will add a total of 14.4 gigawatts (GW) of power generation capacity to Egypt's national grid, enough power to supply up to 40 million people with reliable electricity. With this milestone, Egypt and Siemens have set a new world record for execution of modern, fast-track power projects, delivering 14.4 GW of power in only 27.5 months. A single combined cycle power plant block with a capacity of 1,200 megawatts typically takes approximately 30 months for construction. For the Egypt Megaproject Siemens in parallel built twelve of these blocks in record time and connected them to the grid.
Following the delivery of several Siemens SGT5-8000H gas turbines, the first steam turbine for the Egypt Megaproject began its journey in December 2016 from the Siemens factory in Muelheim to the power plant Beni Suef in Egypt. The main components of the 670-ton cargo were lifted with a heavy-duty crane from the production hall onto a transport vessel standing by at the plant's inland harbor facilities. The vessel transported the SST-5000 steam turbine from Muelheim to the deep-water port of Antwerp where it was loaded onto a heavy cargo ship and transported to Egypt.
After the steam turbines installation, the waste heat from the gas turbines will be used to produce steam that will then drive the steam turbine, thus increasing the overall power output and efficiency of the power plant. In total, Siemens will deliver twelve SST-5000 steam turbines for the Egyptian power plants Beni Suef, Burullus and New Capital. All of these steam turbines will be manufactured at the Siemens factory in Muelheim.
Siemens has introduced a new SGT-800 performance enhancement that is applicable to all existing SGT-800 units with 43-47.5-MW ratings. The new upgrade is designed to provide owners and operators with significant fuel savings and CO2 emissions reduction for improved sustainable energy production.
The North County Transit District (NCTD) Board of Directors approved the purchase of five new Siemens locomotives at the June Board meeting. The five locomotives being replaced were originally built between 1975-1992 and were purchased as used by NCTD. These five locomotives have reached the end of their useful life.
- Finance proves crucial for Siemens Gamesa customers across the globe
- Preferred finance agreement with Siemens Financial Services offers bundled equipment, service and capital solutions for wind industry
- Bosco Le Piane project in Italy benefits from collaboration
Helping wind energy customers overcome funding obstacles, Siemens Gamesa Renewable Energy has teamed up with Siemens Financial Services (SFS) to offer bundled solutions that include equipment and service with financing options. Finance is one of the biggest barriers facing clients as it varies from market to market, and the ability to offer financial solutions has proved to be a win-win in bringing clean energy projects online for Siemens Gamesa customers worldwide. Most recently, the Bosco Le Piane wind project in Italy benefited from this Siemens Gamesa-SFS collaboration. This is the fourth large-scale onshore wind farm in Italy financed by SFS in support of key clients that incorporate Siemens Gamesa technology. The other projects were Melfi, Tricarico and E-Vento.
Siemens has completed extensive service operations on the gas turbines at Jebel Ali K-station in a record time of only 29 working days, a notable accomplishment for a project of this scale. The power plant is located in Dubai and owned by Dubai Electricity and Water Authority (DEWA) and in operation since 2002. The outage featured the application of the "rotor-swap"; a pioneering concept that has been developed by DEWA to utilize a spare rotor and other critical parts, stored at the plant's site, to maximize each unit's availability and reduce idle time while waiting for the completion of rotor assembly work.Under terms of the agreement, Siemens provided supervisory services for three of Jebel Ali K-station's gas turbines to enable further efficient and reliable operation for approximately 100,000 hours – equivalent to about 15 years. The upgrades also increased power output by 62.6 megawatts (MW) and improved power plant efficiency by about 0.5 percent."The new project is built on over 30 years of trust and partnership with Siemens. We are very pleased to work with the company again and successfully complete services of Jebel Ali K-station's power assets so quickly, which allowed the plant to reduce the length of maintenance outage and return the turbines to service as early as possible," said Nasser Lootah, Executive Vice President of DEWA. "With this project, we will enhance the power output and the long-term availability of our power generation assets."After a certain number of operating hours, all gas turbines need to be dismantled for maintenance services. Typically, an outage of this kind would take up to 45 working days to complete, involving over 100 personnel with different areas of technical expertise. By implementing a newer outage concept, Siemens was able to perform the services within just 29 working days, setting a new benchmark in the global power service industry."DEWA puts a great importance on the availability and sustainability of power for Dubai's population, which results in their continuous commitment to innovative ideas and proactive approach for accomplishing the best results," said Gianluigi Di Giovanni, Senior Executive Vice President of Siemens Power Generation Services in the Middle East. "This project reflects our commitment to bringing the company's latest and most-advanced technologies to the UAE to help boost the efficiency and sustainability of its energy sector."Recently, Siemens and Dubai Electricity and Water Authority (DEWA) have signed an agreement to collaborate on an advanced data-driven project. Siemens and DEWA are working together to identify ways to improve thermal efficiency, provide cost-effective solutions for performance optimization, manage costs and reduce fuel consumption and emissions.
- Standard locomotive for freight transport in Germany
- Smart concept: One version, one contract, one price
- Already approved for operation
Siemens is offering a new locomotive for service in Germany: The Smartron is tailored for a specific transport function and utilizes all the advantages provided by standardization. As a preconfigured locomotive, the Smartron has been conceived for transporting freight in Germany and ensures customers cost-efficient operation and the highest safety standards. The Smartron has already received approval for operating in Germany. The locomotives can now be ordered and will be delivered beginning late in 2018. The first locomotive of the new series is immediately available to customers for test runs and demonstration.
Mitsui Rail Capital Europe (MRCE), a full-service locomotive leasing company, has ordered 136 Vectron type locomotives from Siemens in total. MRCE therefore owns one of the biggest Vectron fleets. In March 2018 Siemens and MRCE have agreed to found a joint venture for the maintenance of locomotives. Together, the companies will not only maintain the MRCE fleet, but also reliably service and guarantee the maximum availability of third-party fleets with their innovative maintenance technologies. Both partners are jointly investing in the joint venture, primarily to build a new workshop for locomotives. The groundbreaking ceremony is planned for the current calendar year. The new workshop is scheduled to open in the summer of 2019.