Additive manufacturing has the potential to become a new key technology. For example it opens up new attractive prospects in the manufacture of gas turbines. This is why Siemens has been investing in this innovative technology right from its inception, and is now driving the industrialization and commercialization of these processes. Additive Manufacturing is a process that builds parts layer-by-layer from sliced CAD models to form solid objects. This enables highly precise solutions to be formed from powdered high-performance materials. Siemens is a pioneer in Additive Manufacturing and already uses the technology for rapid prototyping. Furthermore the company is now developing solutions ready for series-production for manufacturing gas turbine burner nozzles and repairing burner heads. Just recently Siemens achieved yet another breakthrough: the first gas turbine blades ever to be produced using Additive Manufacturing have successfully finished performance testing under full-load conditions.
The need for electromobility is growing, as is the need for an efficient charging infrastructure. As a pioneer in electromobility, Siemens has global experience, maintains a strong portfolio along the entire value chain, and plays an active role in advancing the development and standardization of charging solutions worldwide.Siemens is part of the "FastCharge" research project together with BMW Group as consortium leader, Allego GmbH, Phoenix Contact E-Mobility GmbH as well as Dr. Ing. h.c. F. Porsche AG. This project is investigating the technological requirements that vehicles and infrastructure must meet in order to be able to use extremely high charging capacities. The industrial companies involved in the research project presented the latest advancements in the field of fast and convenient energy supply for electrically powered vehicles on December 12, 2018. The prototype of a charging station with a capacity of up to 450 kW was inaugurated in Jettingen-Scheppach, Bavaria. At this ultra-fast charging station, electrically powered research vehicles created as part of the project are able to demonstrate charging times of less than three minutes for the first 100 kilometres of range or 15 minutes for a full charge (10-80 % State of Charge (SOC)).The energy supply system of Siemens used in the project contains both high-power electronics for the charging connections as well as the communication interface to the electric vehicles. For the connection to the public power grid, a charging container was implemented with two charging connections for CCS-compatible vehicles. One connection has an unprecedented charging capacity of max. 450 kW while the second can deliver up to 175 kW.
The digital transformation of the producing industry is gaining momentum. Companies from a wide variety of industries are already unlocking this potential – they are using end-to-end digitalization to create a lasting competitive edge by reducing time to market and increasing flexibility, efficiency, and quality. With Siemens Digital Enterprise solutions the technical prerequisites for the implementation of Industrie 4.0 are available and can be deployed in every application and companies of all sizes. At the SPS IPC Drives in Nuremberg, Germany, from November 27 to 29, 2018 – which took place this year under the motto "Digital Enterprise – Implement now" – Siemens showed in hall 11 how this can be done.
- Siemens to supply 19 net-gas, off-gas and recycle gas compressors for crude flexibility project
- The project will enable the refinery to process up to 420,000 barrels per day of offshore crude oil
Siemens was recently selected to provide 19 process reciprocating compressors for ADNOC Refining’s crude flexibility project at Ruwais Refinery-West. The project is intended to increase the refinery’s crude processing flexibility, enabling the site to process up to 420,000 barrels of oil per day of the local crude grade known as Upper Zakum, which is found offshore. The upgrade will improve the value of each barrel of oil and allow ADNOC to export more of its main onshore, lighter-grade Murban crude.
Agility is the ability to adjust rapidly to changing market conditions, capitalize on emergent business opportunities, and reduce costs or increase revenue streams in the process. In the wake of decarbonization, decentralization, and digitalization, it is the basis for grid operators' and utilities' future business success.
The Siemens booth at EUW 2018 presented combined solutions for electrification, automation, and digitalization that pave the way for multilayered, distributed, and connected grids, this way enabling the required degree of agility.
- Siemens successfully completed the first phase of its shallow water test of the Subsea Power Grid.
- The development program was conducted in collaboration with industry partners Chevron, Equinor, ExxonMobil, and Eni Norge.
- This will be the world's first Subsea Power Grid for medium voltage power distribution using pressure compensated technology.
Siemens has successfully concluded the first phase of its Subsea Power Grid shallow water test in Trondheim, Norway. Siemens, in collaboration with industry partners Chevron, Equinor, ExxonMobil, and Eni Norge, is in the final stages of a program to develop a barrier-breaking system that will become the world’s first Subsea Power Grid designed for distribution of medium voltage power using pressure compensated technology.
- Fulcrum's municipal solid waste-to-fuels plant will contribute to a sustainable future
Abengoa, a Spanish engineering, procurement and construction (EPC) contractor, recently selected Siemens to supply a compressor train for Fulcrum BioEnergy's Sierra BioFuels Plant that will use gasification technology to produce low-carbon fuels from municipal solid waste. The plant will be located in Storey County outside of Reno Nevada and is expected to produce approximately 11 million gallons of biofuel per year that will be used by the aviation industry.
• Agreement is Siemens' largest O&M deal in terms of power generated • Sites to serve as model for other utilities in reliability and efficiency• Digital services and data analytics to optimize plants and ensure reliabilityIn a new milestone agreement, Siemens announced today that it has been selected by the Egyptian Electricity Holding Company (EEHC) to provide comprehensive operation and maintenance services (O&M) for the Beni Suef, New Capital and Burullus power plants, for the next eight years. The agreement, which is the largest ever for the Siemens Power Generation Services in terms of power generated, includes the implementation of the company's Omnivise digital service solutions.Each of the three 4.8GW power plants is considered to be the largest gas-fired combined-cycle plant ever built and operated. Together the plants represent approximately 40 percent of Egypt's power capacity, at the time of signing contracts, generating 14.4GW – enough to supply 40 million Egyptians with electricity."The new agreement aligns with our energy production goals to ensure sustainable growth and maximum reliability and efficiency of new and existing combined-cycle generating facilities," said Eng. Gaber El Desouki, Chairman of the EEHC. "Strategically, it makes sense for us to enlist a single trusted and credible service provider to help operate and manage our large-scale power assets."The multi-year agreement covers all on-site equipment including 24 gas turbines, twelve steam turbines, 36 generators, 24 heat recovery steam generators and three 500 kV gas-insulated switchgear systems. "The new agreement reconfirms our focus to work with Egypt on developing the right mix of solutions to support the country's dynamic needs. It also underscores the tangible cost benefits that digital technologies can bring to the power industry," said Gianluigi Di Giovanni, Senior Executive Vice President of Siemens Power Generation Services in the Middle East and North Africa. "As a key development partner to the country we are committed to contributing to the sustainable growth, diversification and efficiency of the Egyptian energy industry." Siemens will also implement its services portfolio to improve asset visibility, reliability and availability of the three power plants. Data from the plant operation will be collected, analyzed and transformed into actionable insights such as accurate diagnostics, troubleshooting and condition forecasting, improving plant reliability and reducing downtime. Additionally, the data processed can help to balance maintenance costs, optimize inspection intervals and provide valuable insights into operational risks.Building on more than 30 years of experience in power plant operation and maintenance, Siemens currently manages more than 35 GW in 17 countries. The company's global resources and fleet expertise enable it to provide complement plant services and management, along with sharing best practices and technical knowledge with power plant owners.
During the conference, Siemens introduced the new SGT-400 PL Compressor Package, a highly integrated, turnkey gas turbine and centrifugal compressor solution. With field-proven, efficient, and reliable components, this new package offers a single-lift, one baseplate configuration for fast deployment, DLE combustion technology for emissions compliance even at low loads, and expert, 24x7 support for responsive service.
With the DynaGridCenter project, Siemens worked alongside partners in science and research to develop the next generation of grid control centers. For the first time, assistant systems visualize dynamic processes that bring the energy transition to the power grid and provide targeted recommendations for actions to optimize the grids and prevent blackouts.