- Siemens building technologies to be integrated across the Expo 2020 Dubai site, powered by and integrated into MindSphere
- 137 buildings will be connected via cloud-based energy analytics platform; one of the world's largest installations of Siemens Navigator
- Buildings in three Thematic Districts will be digitalized with smart building management system, Desigo CC
- Digitalized infrastructure will support Expo 2020 Dubai in meeting sustainability, comfort, safety and security targets
Dubai is on its way to creating one of the most connected and sustainable World Expos in history, as Siemens begins one of the world's largest installations of its building technologies at Expo 2020 Dubai. The digital solutions will connect, monitor and control buildings across the site with MindSphere, the cloud-based operating system for the Internet of Things, powering the collection and analysis of data for intelligent decision-making and actions. The smart technologies will support Expo 2020 Dubai's targets for energy efficiency, comfort, safety and security.
Additive manufacturing has the potential to become a new key technology. For example it opens up new attractive prospects in the manufacture of gas turbines. This is why Siemens has been investing in this innovative technology right from its inception, and is now driving the industrialization and commercialization of these processes. Additive Manufacturing is a process that builds parts layer-by-layer from sliced CAD models to form solid objects. This enables highly precise solutions to be formed from powdered high-performance materials. Siemens is a pioneer in Additive Manufacturing and already uses the technology for rapid prototyping. Furthermore the company is now developing solutions ready for series-production for manufacturing gas turbine burner nozzles and repairing burner heads. Just recently Siemens achieved yet another breakthrough: the first gas turbine blades ever to be produced using Additive Manufacturing have successfully finished performance testing under full-load conditions.
- Managing Board and Supervisory Board approve change as of January 1, 2015
- Current CEO Johannes Milde to continue serving in advisory capacity for some time to come
Siemens' Building Technologies Division will have a new CEO on January 1, 2015. Matthias Rebellius (49) is succeeding Johannes Milde (61), who is resigning as Division CEO at the end of this year. Milde will continue to support the company for some time to come.
Aker Solutions and Siemens have signed a strategic collaboration agreement to further develop digital offerings in engineering, operations and services. The collaboration focuses on the creation of software applications and joint service offerings including the development of industrial digital twins that will drive efficiency throughout the entire plant lifecycle. In addition, the companies will further develop specific offerings for the oil and gas sector based on Siemens' Comos engineering platform. These solutions will help customers to reduce engineering and operational cost and enable improved decision making. The agreement builds on a long-standing, successful relationship between both companies by combining individual strengths and promoting joint offerings.
- Improved accuracy and repeatability
- Increased asset utilization and decreased operational waste
- Wide range of applications in environmental, chemical, and food and beverage industries
- Hart 7 communications
Siemens presents Sitrans Probe LU240, its newest ultrasonic level measurement Hart transmitter, a hardworking and rugged device that provides reliable level, volume, and flow measurements. Engineered for the challenges of the environmental industry, this transmitter is also suited for the chemical and food and beverage applications. Field-proven Process Intelligence echo processing separates true material level echoes from false, providing reliable readings while still allowing rapid response to actual changes in the material level. The device's reduced blanking distance decreases waste in applications while boosting asset utilization by providing continuously accurate readings even with high levels of material.
- Edge Devices to collect and process large data volumes directly at the machine
- Secure, future-proof basis for the execution of Industrial Edge applications
- Simple update procedure and software rollouts through secure link to central Edge Management System
- Savings through edge computing in the Siemens Electronics Factory Amberg
At the SPS IPC Drives 2018 in Nuremberg, Siemens will be showcasing a newly developed hardware platform for edge applications as part of its Siemens Industrial Edge concept: The compact Simatic Edge Device works on the basis of the embedded industrial PC Simatic IPC227E, and features integrated connectivity to automation on the machine level. This allows manufacturing data to be captured and processed directly at the point of production. If there is a change to the framework conditions underlying the industrial application, Industrial Edge offers facility to adjust software applications on the Edge Device, keeping them right up to date using functional, feedback-free updates. The hardware comes with a closed all-metal housing, ensuring maximum industrial functionality for flexible, maintenance-free use under even the harshest of conditions. Rapid commissioning is guaranteed using pre-installed Edge software.
The Supervisory Board of Siemens AG has extended the appointment of Managing Board member Lisa Davis (55) ahead of schedule. Her term of office will now continue until the end of October 2020. This move is a sign of continuity in the context of the implementation of the company's new Vision 2020+ strategy program. Her contract will subsequently extend automatically by one year until the end of October 2021, provided that neither Lisa Davis nor the Supervisory Board objects.
- TÜV Süd certified process for system integration and solution project processing in conformity with IEC 62443-2-4 and -3-3
- Security documentation in conformity with IEC 62443
- Implementation of certified solutions with Simatic PCS 7
- Standardized processes reduce outlay for customers
Siemens is the world's first company to gain TÜV SÜD certification for the secure system integration of process automation and drive solutions in compliance with the international IEC 62443-2-4 standards. The integration projects, verified on the basis of two standard solutions in the oil & gas processing industry and in a waste incineration plant, have been certified in conformity with IEC 62443-2-4 and -3-3 and were implemented using the Simatic PCS 7 process control system. The projects involved process automation, drive solutions and comprehensive security measures and functions designed to deliver secure plant operation. The certification has a whole range of advantages to offer for customers: plant operators benefit from the precise definition of requirements, the implementation of standardized automation solutions and processes, and from the availability of documentation in conformance with standards. This documentation provides a vital foundation for verifying compliance with the technical requirements of the IT Security Act and other cyber security standards, for the sustainable improvement of IT and OT system security, and for guaranteeing the security of general supplies. The system solutions are used in sectors involving a critical infrastructure, such as waste management and the oil and gas industry.
- Industrial PC for use as an IoT gateway enables data to be managed directly in the production environment
- Based on Windows or Linux, for networking machinery of different manufacturers and of different technological versions
- Fitted with up to 3 LAN interfaces for high connectivity
- Pre-configured versions available from stock
Siemens has expanded its product portfolio of Simatic industrial PCs to include the Simatic IPC127E. The newly developed industrial PC is suitable, for example, for use as a gateway and enables data to be managed directly in the production environment. Whether it is based on Windows or Linux, the Simatic IPC127E makes it possible to network existing systems with machinery of different manufacturers and different technological versions. Thanks to the compact enclosure of just 0.3 liters, it can be integrated with a minimum space requirement in the cabinet or directly at the machine.
- Integration of artificial intelligence and edge computing into Digital Enterprise portfolio
- Networking concepts from factory floors to corporate offices
- Growing ecosystem surrounding MindSphere
By expanding its Digital Enterprise portfolio and integrating future technologies, Siemens is driving forward the digital transformation of the discrete and process industries. "An ever-increasing number of industrial enterprises, particularly SMEs, are well on the way towards Industrie 4.0, and are already improving their competitive standing with digital solutions," explained Klaus Helmrich, Member of the Management Board of Siemens AG, at the SPS IPC Drives. "This applies to all sectors of industry with rapidly changing market demands in which products have to be manufactured ever more quickly, flexibly and in diminishing quantities. With the further integration of technologies such as artificial intelligence (AI) and edge computing into our portfolio, we're paving the way for the future of industry." Siemens will be present at the fair with an array of innovations and industry-specific applications, ranging from automation and edge devices using artificial intelligence in applications such as machine tools, production machinery and process plants through to integrated networking concepts from factory floors to corporate offices. These all help to drive forward the use of innovative automation and software solutions.