Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release28 March 2019Digital Factory Nuremberg
TIA Portal engineering – goes cloud!

The picture shows TIA Portal Engineering.
Using the TIA Portal in the cloud provides fast, flexible, and web-based access to pre-installed environments using any type of hardware, without any need for installation, and at any time and place. This substantially reduces the effort required for testing new TIA Portal innovations, and so enables the TIA Portal to adapt flexibly to the user's hardware and way of working. Integrating the widest range of PC and tablet hardware into the development process of machines and plants increases flexibility while reducing the engineering hardware requirements to a minimum. There is no need for local installation on the hardware as access is web-based.
The scalability of the cloud architecture enables customized adaptions to the user's requirements. This includes not only the performance, but also the individual adaption for users who would like to access pre-installed TIA Portal environments. This enables users to adapt very quickly without any waiting time. It can also substantially reduce the costs of installation and software maintenance.
The central storage of project data in a cloud-based FileShare permits fast, easy access no matter where the user is located. It also makes it significantly easier to distribute project data throughout the team. This can completely eliminate the need to copy data from one device to another.
Background information:
Launched in 2010, the Siemens TIA Portal (Totally Integrated Automation Portal) enables users to perform automation and drive tasks quickly and intuitively through efficient configuration. The software architecture is designed for high efficiency and ease of use, and is suitable for both new and experienced users. It offers a standardized operating concept for controllers, human machine interfaces (HMI) and drives, as well as for shared data storage and consistency, for example during configuration, communication and diagnostics, and also offers powerful libraries for all automation objects. The simple engineering in the TIA Portal facilitates full access to the entire spectrum of digitized automation, from digital planning and integrated engineering up to transparent operation. Alongside PLM (Product Lifecycle Management) and MES (Manufacturing Execution Systems) within the Digital Enterprise Software Suite, the TIA Portal complements the holistic range of software available from Siemens for companies on the path toward Industrie 4.0.
More information on Siemens at the Hannover Messe 2019 is available at www.siemens.com/press/hm19 and www.siemens.com/hannovermesse
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Andreas Friedrich
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (1522) 2103967