Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release28 February 2019Process Industries and DrivesNuremberg
Sidrive IQ: Greater efficiency with Simotics Connect 400 connectivity module

The picture shows low-voltage motors.
At this year's Hannover Messe; Siemens will be using a brownfield application to demonstrate how plant availability can be optimized in future using Simotics Connect 400. The connectivity module comes with all the sensors required for capturing motor vibration or temperature-related data, a WLAN communication module and a battery to enable independent operation. The module processes and saves the operating data, and sends it to the Sidrive IQ Fleet App for cloud-based analysis. Special algorithms use the data to generate meaningful key performance indicators (KPIs) which describe the status of the motors, and are used to determine any concrete need for action. If required, the modules can be retrofitted to legacy motors to improve reliability and availability and boost performance.
Sidrive IQ: IoT digitalization portfolio for drive systems
Sidrive IQ is an essential component of the Siemens digitalization portfolio which opens up wide-ranging scope for IoT (Internet of Things) optimization across the entire drive train – from production through to servicing. Sidrive IQ MindSphere offers a variety of different applications and customized services. Sidrive IQ Fleet is used predominantly in process industry applications, and Analyze MyDrives is designed in the main for the discrete manufacturing industry. Both applications enable the visualization, analysis and monitoring of drive data.
Sidrive IQ is an essential component of the Siemens digitalization portfolio which opens up wide-ranging scope for IoT (Internet of Things) optimization across the entire drive train – from production through to servicing. Sidrive IQ MindSphere offers a variety of different applications and customized services. Sidrive IQ Fleet is used predominantly in process industry applications, and Analyze MyDrives is designed in the main for the discrete manufacturing industry. Both applications enable the visualization, analysis and monitoring of drive data.
The Sidrive IQ application Analyze MyDrives additionally allows the operating status of Sinamics low-voltage converters to be reliably and conveniently monitored, while gathering and analyzing their operating data. By continuously monitoring power consumption, torque and frequency and also measuring energy flows, users can identify any optimization and maintenance requirement and so initiate any necessary actions in good time. This reduces the need for fixed-interval maintenance, making for greater machine productivity and allowing energy saving potential to be identified.
As a result, plant operators benefit from improved plant availability. A range of connectivity modules for low-voltage and medium-voltage converters as well as low-voltage and high-voltage motors are available from Siemens for linking drive systems to the cloud.
For further information on Sidrive IQ, please see
www.siemens.com/sidrive-iq
www.siemens.com/sidrive-iq
For further information on Siemens at the Hannover Messe 2019, please see
www.siemens.com/hannovermesse and www.siemens.com/press/hm19
www.siemens.com/hannovermesse and www.siemens.com/press/hm19
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Stefan Rauscher
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7952