Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release01 April 2019Digital IndustriesHanover
Highest computing and graphic performance for future technologies
The picture shows the industrial PC platform Simatic IPC1047.
The Simatic IPC1047 is optionally available with an Intel Xeon E5-2620v4 2.1 GHz with 8 cores or the Intel Xeon E5-2658v4 2.3 GHz with 14 cores; both versions are preconfigured for multicore technology and thus provide high performance and better multitasking in industrial environments. The use of two processors makes it optimally suitable for data acquisition and image processing for quality testing, the visualization of production sequences, and the virtualization of computers. The IPC can even run several demanding applications simultaneously, such as visualization applications with demanding graphics or programs with extensive calculations.
The Simatic IPC1047 is equipped with up to two extremely powerful Nvidia Quadro P5000 GPUs (Graphics Processing Units). The multidisplay architecture enables several screens to be connected so that user models with large modules and renderings with high image quality and a resolution of up to 5K can be created.
The device is offered optionally with up to 2TB DDR4 ECC RAM memory, a 2TB HDD 3.5" SATA storage medium, 4 x 3.5" drives (internal mount), or 8 x 2.5" drives (internal mount), as well as a maximum of 6 PCIe slots (3 PCIe x8 and 3 x PCIe x16), six USB interfaces, and a serial port.
The 19" full-metal installation enclosure (4U) of the Simatic IPC1047 provides both high mechanical ruggedness (vibration/shock) – and thus protection in harsh industrial environments – and electromagnetic compatibility. The deep, rugged, enclosure is prepared for mounting on a telescopic rail.
Thanks to its outstanding thermal design, the rack PC can even run at an ambient temperature of up to 50 °C without any loss in performance.
The Simatic IPC1047 is used with a 860W or 700W redundant power supply designed for industrial environments.
Thanks to its outstanding thermal design, the rack PC can even run at an ambient temperature of up to 50 °C without any loss in performance.
The Simatic IPC1047 is used with a 860W or 700W redundant power supply designed for industrial environments.
For further information, refer to www.siemens.com/ipc
For further information on Siemens at the Hannover Messe 2019, please see www.siemens.com/press/hm19 and www.siemens.com/hannovermesse
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI's unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 75,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Andreas Friedrich
Siemens AG
Gleiwitzer Str. 555
90475 Nürnberg
90475 Nürnberg
+49 (1522) 2103967