Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release19 September 2017MobilityMunich
Blue Line in Bangkok to be extended with Siemens technology
The initial Blue Line in Bangkok was delivered as a turnkey rail system by Siemens in 2004 and was the first metro line in Thailand's capital. Around 320,000 passengers a day use the 20-kilometer metro line with 18 stations. The line is now being extended by a further 28 kilometers and 19 additional stations. A large part of the extension, from Hua Lamphong to Lak Song in the south and from Bang Sue in the north to Tha Pra, will run above ground. When the line's extension is completed, experts forecast that Bangkok's metro will transport up to 500,000 passengers per day.
"We have decisively helped develop and shape Bangkok's urban transport system over recent decades. This is the fifth major order we've received for expanding the city's urban transport system," says Jochen Eickholt, CEO of Siemens Mobility Division.
Bangkok's population has been booming for years. In order to cope with this growth, the city wants to increase the share of urban transport users from 40 percent at present to 60 percent by 2021. This requires the consequent expansion of the city's rapid transit systems.
The trains from Siemens that will be used on the Blue Line are an evolution of existing Bangkok metro trains and are capable of carrying more than 800 passengers each. The trains have a top speed of 80 km/h. They will be built at Siemens' factory in Vienna, Austria.
Siemens Mobility Division has conceived and completed three high-performance turnkey rail systems for Bangkok to date. In addition to the Blue Line, which has been operating since 2004, Siemens also delivered the Skytrain and the Airport Rail Link. A connection between the Blue Line and the Purple Line was inaugurated in August. In 2016, Siemens received an order for 22 four-car metro trains to operate on the city's Green Line. Delivery of the first trains is scheduled for the coming year.
This press release and further material are available at: www.siemens.com/press/bangkok
For this press release
@SiemensMobility
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Eva Haupenthal
Siemens AG
Werner-von-Siemens-Straße 1
80333 Munich
Germany
80333 Munich
Germany
+49 (89) 636-24421