- Siemens Mobility begins extensive test program
- DB Regio to operate the Rhine Valley network as of 2020
- Profitable over the entire lifecycle with enhanced passenger comfort
The first trainset of the new Mireo regional train platform has been completed. In the coming months, a total of eight pre-production trains will be commissioned at the company's Test and Validation Center (PCW) in Wegberg-Wildenrath. Before the train is allowed to operate for the first time in Germany's rail network, an extensive test program must be completed at the PCW. In June 2020, the Mireo is scheduled to begin service in the Rhine Valley network in Southwest Germany that is operated by the DB Regio Regional Business Unit of Deutsche Bahn. DB Regio AG has ordered a total of 24 Mireo trains, the first order Siemens Mobility received for the newly developed platform.
- Hybrid power plant solution with integrated battery energy storage
- Power supply with a capacity of 145 megawatts
- Scheduled to start operation in Santo Domingo in spring 2021
Siemens and the marine arm of ST Engineering in Singapore have jointly received an order for a SCC-800 2x1C SeaFloat barge-mounted power plant from Seaboard Corporation subsidiary Transcontinental Capital Corporation (Bermuda) Ltd., an Independent Power Producer (IPP) with operation in Dominican Republic. The project Estrella del Mar III in the Dominican Republic will provide the customer with a highly efficient power generation facility.
- Improved accuracy and repeatability
- Increased asset utilization and decreased operational waste
- Wide range of applications in environmental, chemical, and food and beverage industries
- Hart 7 communications
Siemens presents Sitrans Probe LU240, its newest ultrasonic level measurement Hart transmitter, a hardworking and rugged device that provides reliable level, volume, and flow measurements. Engineered for the challenges of the environmental industry, this transmitter is also suited for the chemical and food and beverage applications. Field-proven Process Intelligence echo processing separates true material level echoes from false, providing reliable readings while still allowing rapid response to actual changes in the material level. The device's reduced blanking distance decreases waste in applications while boosting asset utilization by providing continuously accurate readings even with high levels of material.
- Trafikverket awards 75 million Euro contract
- Siemens Mobility, with Eltel Networks Infranet, to deliver intelligent infrastructure technology
- Communications, control and monitoring systems for tunneling
The Swedish Transport Administration, Trafikverket, has announced that it awarded Siemens Mobility a 75 million Euro contract to deliver communications, control and monitoring technologies for a section of the European route number four (E4), the Stockholm Bypass. The new bypass will connect the southern and northern parts of the surrounding Stockholm communities. The bypass is a 21-kilometer road, including 18 kilometers of tunneling around one of Europe's busiest capitals. It will relieve intercity and main thoroughfare congestion, significantly reducing delays for residents and visitors. The construction of the tunnel started in 2014 and is expected to be completed in 2026. Installation and testing of Siemens Mobility technologies will begin in 2021.
- Nemo Link is the first transmission link between the two countries
- It enables transmission of 1,000 MW electricity using Siemens HVDC Plus technology
- Siemens built converter stations housing the state of the art HVDC equipment in both Herdersbrug (Belgium) and Richborough (UK)
- Official opening ceremony on December 5 in Herdersbrug with Belgian and UK dignitaries
Nemo Link® interconnector is a joint venture between the Transmission System Operators Elia (Belgium) and National Grid (UK), to exchange electricity up to 1,000 MW between the two countries, using high voltage direct current (HVDC) technology. Nemo Link connects the Belgian and the British power grid with a combination of subsea and underground cables. This new 140 kilometers (km) long HVDC interconnection increases security of supply for both countries, allowing the import and export of electricity, as well as supporting the integration of renewable energy in the grid. The European Commission designated it a Project of Common Interest as it contributes to an integrated European energy market.
- Hybrid project based on biofuel and solar energy inaugurated on the Galapagos island of Isabela
- First of its kind local energy system, developed for carbon-neutral operation
- Remotely monitored from the Siemens-Mindsphere Application Centers in Munich and Austin, Texas
After only ten months of planning and ten months of construction, the hybrid power plant installed by Siemens on the Galapagos island of Isabela was inaugurated. The aim of the project was to convert the current power generation structure, which is based on fossil fuels, to a hybrid system with several primary energy sources. The system is designed to run carbon-neutral with biofuel and solar energy and supplies almost 900 households on the by far largest Galapagos Island with electricity.
- Siemens Minerals Operation Management Solution eliminates information silos by integrating data at all levels, even ERP and automation
- Provides transparency of entire production process from raw materials to finished products for leading supplier to China’s stainless-steel industry
- Improves quality, efficiency, plus speed and accuracy of decision making
Minimum downtime and the optimum use of staff and resources are key to sustainable success in the minerals and mining industries. To achieve this, the Mintal Group Ferrochrome Science and Technology Co. Ltd. is closing the often-significant information gap regarding production planning, quality, production execution and material logistics that can exist between customer Enterprise Resource Planning (ERP) software and plant automation systems. For this, Siemens will design, engineer and commission a new production management system (PMS), based on the Siemens Minerals Operation Management Solution. With technology-based services throughout the lifecycle of an industrial plant, Siemens provides the basis for greater productivity, flexibility, and efficiency – reliably, globally and around-the-clock.
Aker Solutions and Siemens have signed a strategic collaboration agreement to further develop digital offerings in engineering, operations and services. The collaboration focuses on the creation of software applications and joint service offerings including the development of industrial digital twins that will drive efficiency throughout the entire plant lifecycle. In addition, the companies will further develop specific offerings for the oil and gas sector based on Siemens' Comos engineering platform. These solutions will help customers to reduce engineering and operational cost and enable improved decision making. The agreement builds on a long-standing, successful relationship between both companies by combining individual strengths and promoting joint offerings.
- Moray East project has a capacity of 950 MW representing Siemens' largest UK grid access project to date
- Siemens to deliver onshore substation and three offshore transformer modules (OTM®)
- After commissioning Moray East will provide enough clean energy to power almost one million UK homes
Siemens has been awarded an order to connect the Moray East offshore wind farm to the grid. Moray East is being developed by a joint venture company owned by EDP Renewables, a subsidiary of the Portuguese utility Energias de Portugal, ENGIE, a global energy and services group based in Paris, and Diamond Generation Europe Ltd., a subsidiary of Mitsubishi Corporation. The Siemens' scope of supply covers all necessary components, such as the offshore transformer modules (OTM®) which transform the output of the wind turbines from 66 kilovolts (kV) to the transmission voltage of 220 kV, as well as the onshore station which transforms the electricity into 275 kV for feeding it into the national transmission grid. This project will be the 11th offshore wind farm to be connected to the mainland by Siemens in the UK. Moreover, Moray East marks the largest offshore grid connection in terms of transmission capacity and order entry Siemens has delivered or been awarded in the UK to date.