- Siemens to supply 19 net-gas, off-gas and recycle gas compressors for crude flexibility project
- The project will enable the refinery to process up to 420,000 barrels per day of offshore crude oil
Siemens was recently selected to provide 19 process reciprocating compressors for ADNOC Refining’s crude flexibility project at Ruwais Refinery-West. The project is intended to increase the refinery’s crude processing flexibility, enabling the site to process up to 420,000 barrels of oil per day of the local crude grade known as Upper Zakum, which is found offshore. The upgrade will improve the value of each barrel of oil and allow ADNOC to export more of its main onshore, lighter-grade Murban crude.
- Fulcrum's municipal solid waste-to-fuels plant will contribute to a sustainable future
Abengoa, a Spanish engineering, procurement and construction (EPC) contractor, recently selected Siemens to supply a compressor train for Fulcrum BioEnergy's Sierra BioFuels Plant that will use gasification technology to produce low-carbon fuels from municipal solid waste. The plant will be located in Storey County outside of Reno Nevada and is expected to produce approximately 11 million gallons of biofuel per year that will be used by the aviation industry.
- Heat and power for the Rhine-Ruhr metropolitan region
- Fuel efficiency exceeding 85 percent
- Long-term service agreement
Siemens and STEAG GuD Herne GmbH signed an agreement today on the turnkey construction of a combined cycle power plant with district heat extraction. They also entered into a long-term service agreement. The Herne 6 plant will have an electrical capacity of more than 600 megawatts (MW). Steam will also be extracted, and the thermal energy obtained will be used for the district heating grid of Germany's Rhine-Ruhr metropolitan region. Never before has a single power plant unit been able to provide 400 MW of (thermal) district heat with combined cycle operation. The overall fuel efficiency of the natural gas used thus climbs to more than 85 percent, making the power plant one of the world's most efficient and most environmentally friendly plants. The investment volume for Herne 6 is in the mid-triple-digit euro range.
- Finance proves crucial for Siemens Gamesa customers across the globe
- Preferred finance agreement with Siemens Financial Services offers bundled equipment, service and capital solutions for wind industry
- Bosco Le Piane project in Italy benefits from collaboration
Helping wind energy customers overcome funding obstacles, Siemens Gamesa Renewable Energy has teamed up with Siemens Financial Services (SFS) to offer bundled solutions that include equipment and service with financing options. Finance is one of the biggest barriers facing clients as it varies from market to market, and the ability to offer financial solutions has proved to be a win-win in bringing clean energy projects online for Siemens Gamesa customers worldwide. Most recently, the Bosco Le Piane wind project in Italy benefited from this Siemens Gamesa-SFS collaboration. This is the fourth large-scale onshore wind farm in Italy financed by SFS in support of key clients that incorporate Siemens Gamesa technology. The other projects were Melfi, Tricarico and E-Vento.
- Siemens H-class gas turbines debut on the Mainland China market
- Most efficient power plant in China
Siemens secured its first H-class gas turbine order in Mainland China. The company will supply two H-class gas turbines, two steam turbines and four generators for a power plant project in Guangdong Province. The customer is Huadian Fuxin Energy Corporation Limited (Huadian Fuxin), a subsidiary of China Huadian Corporation Ltd (CHD), one of the five state-owned power producers in China. The components will be installed at the CHD Guangzhou Zengcheng combined cooling, heat and power plant (CCHP) project located in Zengcheng District of Guangzhou City. After completion the project will be the most efficient gas-fired power plant in China. Commercial operation is scheduled for the end of 2019.
Petroecuador, Ecuador’s national oil company, recently selected Siemens to supply an 8-MW SGT-300 gas turbine for power generation for its Shushufindi refinery. The refinery is located in the province of Sucumbios, in the eastern part of Ecuador. Commissioning of the new unit is scheduled for the end of this year.
Siemens was recently selected to supply another SGT-700 mechanical drive compression train for the Camisea gas-condensate asset located in Peru. The equipment, identical to that Siemens supplied in 2011, is essential to the continuing exploration and production of hydrocarbons in Block 88, operated by Pluspetrol Peru Corporation S.A. Due to the natural gas pressure decline of the reservoirs, the Camisea production plan includes a centralized wellhead compression system for all fields.
- Modularized, high-pressure LNGo system helps bridge gap between remote gas supply and remote gas demand via "virtual pipeline"
- Altagas producing approximately 30,000 gallons of LNG per day, with capability to expand
Siemens' Dresser-Rand business recently commissioned an LNGo-HP (high-pressure) micro-scale natural gas liquefaction system for Altagas Ltd. in Dawson Creek, British Columbia, Canada. The modular, expandable LNGo technology enables efficient installation, especially in a demanding environment like Dawson Creek. The Dawson Creek facility, with a capacity of approximately 30,000 gallons of LNG per day, commenced production on January 25, 2018.
- Exclusive equipment provider at each site which includes a long-term service agreement
- Project part of energy reform program to stimulate Mexico's economic growth
Siemens recently delivered five gas turbine-driven compressor trains to Fermaca Enterprises (Fermaca) for two pipeline stations in Mexico. The pipeline projects, which also include a long-term service agreement, are part of the Comision Federal de Electricidad de Mexico's (CFE) ongoing energy reform program intended to increase the availability of low-cost energy and stimulate the country's economic growth.
- From February 5-9, Siemens will present concrete solutions for ways that companies and investors can shape the digital future.
- Digitalization opens up huge potential for small and mid-sized companies in the manufacturing industry – with productivity gains of up to 10 percent.
- In the energy and infrastructure markets, efficiency gains are used to attain a large degree of sustainability.
- These efforts will require extensive investments, which are made easier with innovative financing solutions like pay-per-outcome financing, software financing and project financing.
During the opening session of Siemens Finance Week in the Siemens Technology and Application Center in Erlangen, about 60 decision-makers from small- and medium-sized enterprises learned about the potential of digitalization and ways that new, customer-centric business models can be introduced with the help of financing solutions. The Company Barometer prepared by the German Chambers of Commerce and Industry shows that 68 percent of small and medium-sized enterprises in Germany see opportunities for new digital business models. The optimization potential is enormous: In the manufacturing industry alone, according to the results of a Siemens Financial Services white paper, productivity can be boosted by up to 10 percent through continued digitalization. Figures from the United Nations Committee on Trade and Development (UNCTAD) indicate that this would amount to business volume of approx. €650 billion globally and €60 billion in Germany.