Hagemeyer, a leading German electronics wholesaler, has commissioned Siemens with installing a cloud-based power monitoring system. The system will create transparency about energy flow in the Hagemeyer sales and logistics center in Maisach near Munich and will show saving potential at the facility in an effort to achieve long-term improvements in energy efficiency. The objective here is to lower overall energy consumption by up to 15 percent per year. Hagemeyer will deploy more than 100 measuring devices of the 7KM PAC series from the Sentron portfolio in Sivacon 8MF1 system cubicles and Alpha 3200 low-voltage power distribution boards and implement the powermanager power monitoring software on site. In addition, it also connects to MindSphere, the open Internet of Things (IoT) operating system from Siemens.
- Siemens successfully completed the first phase of its shallow water test of the Subsea Power Grid.
- The development program was conducted in collaboration with industry partners Chevron, Equinor, ExxonMobil, and Eni Norge.
- This will be the world's first Subsea Power Grid for medium voltage power distribution using pressure compensated technology.
Siemens has successfully concluded the first phase of its Subsea Power Grid shallow water test in Trondheim, Norway. Siemens, in collaboration with industry partners Chevron, Equinor, ExxonMobil, and Eni Norge, is in the final stages of a program to develop a barrier-breaking system that will become the world’s first Subsea Power Grid designed for distribution of medium voltage power using pressure compensated technology.
- Siemens implements autonomous stockyard management system in China
- Autonomous stockyard management system combines five automation systems
- Interaction of all components enables control of machines and conveyors
- Improved system efficiency, production capacity and security coupled with lower operating costs
Siemens is supplying an autonomous stockyard management system to be used in a new plant for HBIS Laoting Steel Co. Ltd., a Chinese subsidiary of one of the world's biggest iron and steel producers. The autonomous stockyard management system from Siemens comprises of a material tracking and management system (MAQ), an autonomous stockyard operating system (MOM), a Simatic PCS 7 process control system, industry network, consulting, engineering, project management and commissioning. Interaction between these different components enables control of all the plant's machines and conveying systems, it offers wide-ranging benefits such as the capability for all machines and conveyors to be controlled from a single system. This is achieved using a 3D model of the existing inventory which provides information on the volume and quality of stocked material, enabling autonomous operation of all the plant's storage and retrieval machines. This allows HBIS Laoting Steel Co. Ltd. not only to drive down its operating costs, but also to achieve between a five and ten percent improvement in system efficiency and between three and seven percent higher production capacity. The use of autonomous storage and retrieval machinery also improves safety.
- Comprehensive monitoring of large, complex networks
- Rule-based configuration of the network infrastructure
- Central firmware management with topology-based rollout
- For cross-sector use in all industries
Siemens is launching Sinec NMS, a powerful, future-proof network management system (NMS). It enables users to master the growing demands placed upon industrial communication networks, such as the increasing degree of networking, larger quantities of data, and the complexity of network structures. Networks with between 50 and 12,500 participants can be centrally configured, managed and monitored round-the-clock with the software. This facilitates forward-looking planning and a quick response time to prevent possible failures and so increase productivity. The software can be used across all industries.
- New Safety Library (3.0) for faster commissioning and compatibility with a wider range of Simatic-S7 controllers
- Advanced Position Control (APC) function for faster positioning
- New Simotics S-1FG1 servo-geared motors in upper and lower output range
- Cut in energy costs by optimized motion control
Siemens has upgraded its TÜV-certified Safety Library developed specifically for use with storage and retrieval systems. The benefits of Safety Library V3.0 for users include faster commissioning and compatibility with a wider range of failsafe Simatic controllers (from S7-1516F). Boosting the speed of storage cycles are two functions: Vibx (Vibration Extinction) and the more advanced new function Advanced Position Control (APC). APC also requires no additional sensors or actuators, and ensures the permanent prevention of mast vibrations. APC even kicks in under continuously changing vibration conditions, caused for instance by different loading conditions or variable disturbance factors such as wind. Supplementing this function are new additions to the Simotics S-1FG1 portfolio. In the upper output range, external fans now permit highly dynamic traversing processes, allowing a significantly more dynamic configuration of traversing motors. A new Simatic module for energy-optimized traversing enables energy savings despite the improved dynamic performance.
- Distributed Simatic automation controllers for standard and fail-safe applications up to Performance Level e
- Compact devices with functions of a PC-based software controller, visualization, Windows applications and central I/Os
- World's only software controller with fail-safe, PC-based control which is operated independently of the operating system
Siemens is extending its Simatic automation controller series for PC-based applications. The distributed automation controllers now include the new, more powerful Simatic ET 200SP Open Controller CPU 1515SP PC 2 – for standard and fail-safe applications up to Performance Level e. The new Open Controller, which is particularly suitable for series machine building, combines the functions of a PC-based software controller with visualization, Windows applications and central I/Os (inputs/outputs) in a single compact device The new, fail-safe CPU1516pro-2 PN for the Simatic ET 200pro Distributed Controller also performs standard and fail-safe automation tasks up to Performance Level e in a single device.
- Integrated motor portfolio of Simotics reluctance motors from 0.55 to 45 kilowatts
- Additional shaft heights 90 and 225
- Encoderless closed-loop control down to a standstill
- Reluctance motor portfolio rounded off with rated speeds of 1500 and 3000 revolutions per minute
Siemens is extending its portfolio of Simotics synchronous-reluctance motors to include the two new shaft heights, AH90 and AH225. With these new additions, the company is addressing calls from renowned manufacturers of pumps, fans, compressors and machine builders in general for different shaft heights. The motors are available in a power range of 0.55 to 45 kilowatts (kW), and now also with rated speeds of 1500 and 3000 revolutions per min-1. In conjunction with the recently launched Sinamics Reluctance Control License, precise encoderless closed-loop torque control is possible down to a standstill. The license enables field-oriented (vector) closed-loop control even when at a standstill – reliably eliminating the possibility of the synchronous motor "stalling" at any time even if the load inertia is not known.
- Siemens Mobility will manage contract from the Singapore MindSphere Application Center
- Rail Enterprise Asset Management System to enhance availability
Siemens Mobility and consortium partner ST Engineering Electronics Limited have been awarded an 18.8 million Singapore dollars contract by the Singapore Land Transport Authority (LTA) to develop and implement a Rail Enterprise Asset Management System (REAMS). This digital program will be managed from the MindSphere Application Center in Singapore, one of Siemens' digitalization hubs. The facility was the first to integrate multi-disciplinary digitalization specialists from different Siemens businesses.
- Three new redundancy CPUs for the Simatic S7-1500 Advanced Controller range
- Simple engineering just as with standard CPUs
- Back-up CPU takes control of the process automatically and quickly – without data loss
- Connection of field devices via Profinet ring
Siemens is expanding its Simatic S7-1500 Advanced Controller range with three new CPUs for redundant automation applications. The CPU1513R and CPU1515R are used for small to medium-sized projects with a focus on CPU redundancy. If one CPU fails, the back-up CPU automatically takes control of the process with no data loss and the process continues very quickly. As with the standard CPUs, the engineering of the redundancy CPUs is especially easy for users. The TIA Portal engineering framework and the redundant CPUs synchronize programs and data without the user having to intervene. The CPU1517H is used for larger applications and higher performance requirements. Here, dedicated synchronization modules enable faster, smooth switchover.