- Safer and more efficient: Catania Airport is updated with integrated building automation by Siemens
- More reliable and accurate fire detection using Sinteso connected to the Desigo CC building management software
- Cloud-based Navigator software to optimize energy consumption
With almost ten million passengers in 2018, Catania Airport is continuing to grow, solidifying its number one position in southern Italy. This makes the hub an increasingly important strategic part of the Mediterranean aviation network. As a result, however, it faces greater security and energy efficiency challenges. This is the context in which the Sicilian airport made the decision to entrust Siemens with its integrated building automation project, intended to increase security levels and monitor overall energy consumption at the hub.
- New version SW 4.8 SP3 release for Sinumerik 828Dand Display Manager for Sinumerik 840D sI
- External PC remote control for 828D enables operation via external PC with Sinumerik Operate
- 828D operation simplified by multi-touch display and side screen
- Second control channel and Collision Avoidance Eco simplify handling
- New Display Manager for 840D sI enables integration of standard and machine-specific functions into user interfaces
Siemens has updated its proven Sinumerik 828D and 840D sI machine tool controls. For 828D, a software update SW 4.8 SP3 with Panel Processing Unit (PPU) 4 has now been released. Users benefit not only from exceptionally robust hardware but also improved connectivity through the ability to access central data and programs, increasing operating safety. Another feature of the update is an external PC remote control facility for the simplified connection of other authorized PCs via Virtual Private Computing (VPC). In addition, the application for MindSphere ManageMyMachines now enables connection of Sinumerik 828D controls to the cloud based open IotT operating system MindSphere. For exceptionally simple operation, Siemens offers Smart Operation, a robust multi-touch display used in conjunction with a side screen. The CNC Sinumerik 828D now also offers a second control channel for use during milling operations, making available additional integration and control possibilities for automation systems or handling robots. Another invaluable feature is the Collision Avoidance Eco, which works on the basis of protected areas and distances which can be configured by the user. There is also a new update designed to make life more convenient for users of the Sinumerik 840D sl. The new Sinumerik Operate Display Manager allows the operator to fully leverage the possibilities offered by larger widescreen monitors, as both standard and machine-specific functions can be integrated into the user interface. These innovations allow rapid and comprehensive access to all the relevant data and allow more efficient, simpler machine control, as well as speeding up and simplifying process workflows. This saves both time and costs throughout the entire milling process.
- New development – Simatic PCS neo sets new standards in process automation
- Intuitive usability and a single workbench for all tasks
- Consistent object-oriented data management
- Unique, global, web-based collaboration in engineering and operation
- Scalable from small process modules up to the largest process plants in the world
Siemens sets new standards in process automation and is launching an innovative web-based process control system for all industries at the Hannover Messe. Simatic PCS neo is a brand-new system software, which offers companies in the process industry unique opportunities in the age of digitalization. Main features include global web-based collaboration in engineering and operation and intuitive handling representing all relevant information in a single workbench.
- Spectrum Power ADMS to provide reliable energy supply for 1.5 million people
- One multi-site system to handle all voltage levels
Hafslund Nett, Norway's largest grid company has contracted Siemens to supply a new Advanced Distribution Management System (ADMS) for the operation of the regional power grid in Akershus, Oslo and Østfold. The fully integrated grid operating center will enable monitoring and control of the complete power grid covering all (high-, medium-, low-) voltage levels. At the same time, it will allow easy integration of third-party IT/OT systems, such as customer information systems, workforce management or geographical information systems. The project is expected to be operational at the beginning of 2022.
- Simatic PCS 7 Plant Automation Accelerator V3.0 plant and automation engineering software closes the gap between plant engineering and the process control system
- More powerful, more open version
- Increased system openness based on GSDML and NE150 standards
- Seamless engineering through the integration of various Simatic components
Siemens has extended its engineering software for planners and automation engineers, Simatic PCS 7 Plant Automation Accelerator 3.0 (PAA), to include new functions for even more flexible and integrated automation engineering. With this latest software version, Simatic PCS 7 automation projects can be configured even more easily and efficiently. With Version 3, the PAA software closes the gap between plant engineering and the process control system. The entire plant structure including measuring point data can be generated easily and synchronized between the systems. Automation engineers are supported in all phases from tender preparation (such as bills of material), automatically generated process control data from electrical engineering in the Siemens Simatic PCS 7 process control system (including controlled mass data engineering), to as-is documentation of the process automation.
- New firmware V5.2 for even easier operation of Sinamics S120 drive systems
- Integration of the web server with new, responsive design and no special commissioning tools for diagnostics, maintenance and servicing
- Parallel connection of Active Line Modules (ALM) provides an extended performance range for booksize versions
- Users benefit from increased rated power without additional chassis unit and energy exchange in the DC link
Siemens offers new features in the firmware and hardware for the Sinamics S120 drive system. Operation is made much easier in firmware V5.2 through the integration of the web server. The web server in version V5.2 has a new, responsive design, which reacts via standard web browsers regardless of the end device used (notebook, PC, tablet or smartphone). For commissioning typical diagnostics and maintenance functions or servicing, no special tools are required. The web pages are available in six standard languages and feature error indicators and warning messages including meaningful help texts and suggestions for possible solutions. Users can intuitively create, manage and delete parameter lists - even across axes - and can perform firmware updates and system restores with the old firmware version. Backups of parameter settings can be stored on the clients using the web server and browser, and reloaded in the Sinamics converter using the Restore function. In order to test functions that are subject to license, it is possible to activate a temporary trial mode. In addition, a complete overview of all functions that are subject to license is clearly displayed in the web server. For optimum display on any Internet-capable end device, the best browsers are Microsoft Edge, Mozilla Firefox, Google Chrome and Safari. Navigation is via menu or breadcrumbs.
- Edge application Optimize MyMachining /Trochoidal allows real-time data processing for high availability and productivity
- Siemens Industrial Edge closes the gap between local and cloud computing in the industrial sector
- Sinumerik Edge facilitates high-frequency control data processing
As part of Siemens Industrial Edge, Siemens is launching applications for Sinumerik Edge, the machine-level platform specially designed for the machine tool industry, at AMB 2018 in Stuttgart. This is the first opportunity to see the Edge application Optimize MyMachining /Trochoidal for use in trochoidal milling.
- Higher performance, increased accuracy, full utilization of the stockyard area, and optimized energy consumption compared to staffed operation
- Pilot project for Jiangsu Binxin Special Steel Material Co. Ltd. is a first step towards intelligent upgrading of plants
To improve air quality in China's urban centers, part of the country's counter measures has resulted in stockyard of iron, steel and the production of other industrial activities to move to indoor facilities instead of traditional outdoor locations. To take an industry leadership role, while continuing to meet expanding market needs by increasing production capacity, the Jiangsu Binxin Special Steel Material Co. Ltd. (Binxin Steel) decided to upgrade its plant intelligence by moving to an innovative autonomous stockyard management system from Siemens. This also has the advantage of overcoming the challenge of hiring and retaining skilled workers and engineers, while simultaneously providing continuous, safe, secure, and reliable operations. This project is a first step towards upgrading of the company's plant intelligence.
- TÜV Süd certified process for system integration and solution project processing in conformity with IEC 62443-2-4 and -3-3
- Security documentation in conformity with IEC 62443
- Implementation of certified solutions with Simatic PCS 7
- Standardized processes reduce outlay for customers
Siemens is the world's first company to gain TÜV SÜD certification for the secure system integration of process automation and drive solutions in compliance with the international IEC 62443-2-4 standards. The integration projects, verified on the basis of two standard solutions in the oil & gas processing industry and in a waste incineration plant, have been certified in conformity with IEC 62443-2-4 and -3-3 and were implemented using the Simatic PCS 7 process control system. The projects involved process automation, drive solutions and comprehensive security measures and functions designed to deliver secure plant operation. The certification has a whole range of advantages to offer for customers: plant operators benefit from the precise definition of requirements, the implementation of standardized automation solutions and processes, and from the availability of documentation in conformance with standards. This documentation provides a vital foundation for verifying compliance with the technical requirements of the IT Security Act and other cyber security standards, for the sustainable improvement of IT and OT system security, and for guaranteeing the security of general supplies. The system solutions are used in sectors involving a critical infrastructure, such as waste management and the oil and gas industry.