- Ninety-four new trains will replace the 1970s-built Piccadilly line fleet
- New trains will be state-of-the-art, with more space, air conditioning, walk-through carriages and improved accessibility
- Vital investment will support both London and the wider UK economy – helping to create jobs around the country
Transport for London (TfL) and Siemens Mobility have today unveiled the detailed design of the new generation Tube trains for the Piccadilly line, which will soon be in production to replace the existing 1970s fleet.
Siemens Mobility is investing twelve million euros in the further modernization of its long-established production site in Vienna-Simmering: Together with Vienna's City Economic Councillor Peter Hanke, the groundbreaking ceremony for the construction project took place on Monday, March 1. The investment will focus on the construction of a new train commissioning hall, the expansion of digitalized production, and the optimization of production workflows. This will further increase the competitiveness of the site and secure local jobs and local value creation. Passenger coaches and metro trains are built at the historic Siemens Mobility plant, for example the new night trains for ÖBB or metro trains for Vienna, Munich, Riyadh or Bangkok. ÖBB's popular Railjets were also manufactured here. At the Vienna plant, Siemens Mobility employs about 1,200 people, manufactures about 450 rail vehicles per year and currently trains a total of 88 apprentices.
In a live broadcast between Berlin and London on Thursday, March 4, 2021, Transport for London and Siemens Mobility unveiled the design of the new London Piccadilly line tube trains. 94 state-of-the-art tube trains will replace the current fleet of the Piccadilly line, which was built in the 1970s. The new generation of trains will offer passengers more spacious, air-conditioned walk-through carriages and improved accessibility. The trains are scheduled to be in service on the Piccadilly line from 2025.
- ÖBB and Siemens Mobility show first painted car body
- New Nightjet trainsets enter service in 2022
- ÖBB aiming at greater passenger comfort and privacy
ÖBB and Siemens Mobility presented the first painted car body and exterior design for the new generation of the Nightjet in Vienna today. The new, ultra-modern trains will enter service near the end of 2022 and will first be used on connections from Austria and Germany to Italy. The first 13 trainsets have already been called up by ÖBB from a framework agreement with Siemens Mobility, and a further 20 trains are expected to be called up this year.
- One environment for planning, booking and settlement of multimodal travel
- Travel efficiently, comfortably, and sustainably
- Open ecosystem for all mobility providers
Siemens Mobility will sign a contract in the Netherlands with the joint venture RiVier (NS, HTM and RET) to develop a countrywide, intelligent Mobility as a Service (MaaS) platform. The MaaS platform to be delivered in the autumn will allow providers to integrate travel planning. The technological core of the MaaS platform is supplied by Siemens Mobility subsidiaries Hacon and eos.uptrade.
Polish
provider of transport and logistics services Laude Smart Intermodal S.A. has
just expanded its fleet with the most modern locomotive in Europe: the Vectron
MS. The vehicle colored in pink was handed over in Poznan Franowo near Posen on
February 3
rd, 2021. It is the 50
th Vectron locomotive
from Siemens Mobility in the hands of Polish carriers.
- Order for double-decker Desiro HC trains and single-decker Mireo trains
DB Regio Bayern has ordered 31 regional trains from Siemens Mobility. The trains will serve on routes between Munich, Passau and Regensburg. Siemens Mobility will be delivering 25 double-decker Desiro HC trainsets and six single-decker Mireo trainsets. Passenger service with the new trains is planned to begin with the timetable change in December 2024.
- Largest service order for Siemens Mobility from Deutsche Bahn
- IS 600 revision for 40 ICE 4 trains
Deutsche Bahn (DB) has awarded Siemens Mobility a contract for the revision of 40 trains of the series 412 ICE 4. This is the largest service order ever awarded to Siemens Mobility by Deutsche Bahn. The contract also includes an option for the revision of 50 additional series 412 trains. IS 600 revisions are required for new high-speed trains operated by Deutsche Bahn when they have reached a mileage of 1.65 million kilometers. The work will be carried out beginning in mid-2021 in the “Expert House” service area of the Siemens Mobility Test and Validation Center in Wegberg-Wildenrath, in the state of North Rhine-Westphalia, Germany.
In May 2011, the German national railway company concluded a framework agreement with Siemens Mobility for up to 300 trainsets. At this time the largest train contract that Siemens has ever won in its corporate history.
The ICE 4 sets new standards in intercity traffic. A unique train concept has been developed, that means it can be individually adapted to the requirements of various transport tasks. The modular drive concept is based on independent Powercars with identical traction technology, resulting in more flexibility than ever before. High operational availability is guaranteed by a large number of reliable systems with high redundancy.
All in all, DB will be receiving 1,511 cars with which it can configure 50 12-car, 50 13-car and 37 7-car trainsets.
In addition, Deutsche Bahn has awarded Siemens Mobility a contract for the revision of 40 ICE 4 trains.