The products in Siemens Mobility trains meet the
highest cyber security standards. This was recently confirmed by TÜV SÜD, which
approved Siemens Mobility Rolling Stock with the IEC 62443 4-1 certificate.
This award confirms, 18 months after the IEC 62443 2-4 / 3-3 certification, the cyber
security throughout the entire product development process.
Media representatives got a first-hand impression of the new Vienna Metro during a test drive on the 14th April 2021 – in the presence of Public Transport City Councillor Peter Hanke, Wiener-Linien Managing Director Günter Steinbauer and Siemens Mobility CEO Arnulf Wolfram. After the successful approval of operation, the so-called 'X-Wagen' will be in use for all Viennese on the four lines U1 to U4 from 2022. With the completion of the new U5 in 2026, the new vehicles will also be running fully automatically.
S-Bahn Berlin GmbH has signed a framework contract with the consortium of Stadler Pankow GmbH and Siemens for the delivery of up to 1,380 vehicles. A firm order was placed for the first 106 trains. The 85 four-section and 21 two-section trains have a high triple-digit million-euro order volume. S-Bahn Berlin, a subsidiary of Deutsche Bahn, plans to use the new trains on the Ringbahn lines (S 41 and S 42) as well as on the system's southeastern feeder lines S 47, S 46 and S 8. These lines comprise roughly one-third of the entire S-Bahn network in Berlin. The first ten vehicles will be ready to enter service as of 2020. Subsequently, all remaining vehicles will be delivered continuously to the Berlin system up to 2023. The vehicles will be manufactured and assembled at the Berlin plant operated by Stadler Pankow GmbH.
The national carrier Czech Railways (České dráhy – ČD) continues to modernize its fleet serving long-distance domestic and international lines. The consortium of Siemens Mobility and Škoda Transportation has won the tender for 20 Viaggio Comfort nine-car non-traction units including control cars, designed for a maximum operating speed of 230 km/h. The cars will be delivered from 2024 to 2026 and the order is valued at around half a billion EUR.
- Consortium of Siemens and Škoda Transportation commissioned
- Cars combine efficiency with enhanced passenger experience
- Order volume around half a billion EUR
The national carrier Czech Railways (České dráhy – ČD) continues to modernize its fleet serving long-distance domestic and international lines. The consortium of Siemens Mobility and Škoda Transportation has won the tender for 20 Viaggio Comfort nine-car non-traction units including control cars, designed for a maximum operating speed of 230 km/h. The cars will be delivered from 2024 to 2026 and the order is valued at around half a billion EUR.
Siemens Mobility and DB Systemtechnik have signed a cooperation agreement to modernize a locomotive of the series 101 with an upgraded Siemens ETCS solution Trainguard 200 Onboard Unit system. The locomotive is part of DB Systemtechnik’s fleet and is used for test- and acceptance runs. It will now be upgraded to the European train control system ETCS level 2. At its core, the project aims to develop an interface solution that can be easily implemented for subsequent retrofitting and integration of ETCS and LZB into the vehicle architecture, independent of the train manufacturer. With this technical integration solution, a major step towards the successful retrofitting of entire fleets in the context of the Digital Rail for Germany program is made. Siemens Mobility has demonstrated its retrofit experiences and capabilities already in various retrofit projects throughout Switzerland, Great Britain, Spain and Germany.
- Siemens Mobility launches MoComp – a consolidated catalog for its propulsion-related rail vehicle components and systems
- MoComp portfolio can now be obtained directly by any customer worldwide
- Products will help customers operate rail vehicles over entire life cycle
Siemens Mobility is pleased to announce the launch of MoComp, a consolidated and single source that will for the first-time display and make available to all customers the diverse Siemens Mobility portfolio of rail vehicle components. MoComp will offer the complete range of electrical and mechanical components, and system solutions for modern rail vehicles. This includes pantographs, propulsion systems, bogies, brakes, and onboard power supplies. The offerings showcased by MoComp will provide rolling stock producers, OEMs, and operators the opportunity to take advantage of the very best products on the market, as they look to maintain their rail vehicles over the entire life cycle.
- Siemens Mobility and VTG Rail Europe collaborate to innovate rail freight transport
- Contract covers a one-year trial to prove the system’s operational capability
- Brake Monitoring System has European-wide market potential due to time and cost savings for rail-bound freight transport
Siemens Mobility GmbH and VTG Rail Europe GmbH signed a contract to test the innovative Brake Monitoring System (BMS) for automated brake testing of freight trains to prove the system’s operational capability. The BMS ensures an automatic brake test on each wagon of a train. The expected efficiencies generated for freight operators will result in a great market potential across Europe.
- The two awarded contracts are worth $190M.
- Upgrades will improve the rail capacity, efficiency and enhance passenger experience.
Siemens Mobility has been awarded two contracts worth around AU $190M by the New South Wales (NSW) Government in Australia to significantly upgrade the rail network in metropolitan Sydney, one of the busiest networks in the southern hemisphere. This work will improve the overall efficiency and capacity of the rail network. The total contract consists of two key packages, including the introduction of a new Traffic Management System (TMS) along with the upgrading of the Sydney Trains’ network conventional signalling to a digital ETCS-L2 train control system.