- CBTC to be
installed on the Johor Bahru-Singapore Rapid
Transit System
- First case
where CBTC technology is used on a cross border link
- Rail line will
ease current congestion, improve cross-border connectivity, and bolster
economic activity in the region.
Siemens
Mobility has been awarded a contract by RTS Operations to design, install and
commission a Communications-Based Train Control (CBTC) signaling system and
Platform Screen Door System on the Johor Bahru-Singapore Rapid Transit (RTS)
Link. This will be the first ever case of CBTC technology being used on a cross
border rail link. The 4 km system connecting Johor Bahru, Malaysia and
Woodlands, Singapore will be operated by RTS Operations, a joint venture between
Singapore rail operator SMRT and Malaysian public transport firm Prasarana.
Once completed, the RTS Link will be able to transport an estimated 10,000 passengers an
hour in each direction, helping ease current congestion at existing border
entry points, improving cross-border connectivity and bolstering economic
activity in the region. The line will also be equipped with GoA 4, the highest grade
of automation that allows for trains to be automatically controlled and
operated.
- HMH,
s.r.o is the manufacturer of the MIREL, a train protection system for Slovakia,
Czech Republic, Hungary, and Poland
- Acquisition
strengthens Siemens Mobility's position as a leading rail infrastructure provider in Europe
Siemens Mobility has completed the
acquisition of HMH, s.r.o., a Slovakian-based technology company, that offers
the MIREL national train protection system for Slovakia, Czech Republic, Hungary,
and Poland. With this acquisition, Siemens
Mobility is now able to offer a complete train protection portfolio covering
the Eastern European rail corridors. HMH will remain based in Bratislava,
Slovakia, and will be integrated into Siemens Mobility’s Rail Infrastructure
business unit.
- More space for locomotive production and service business
- Floor area to be increased by around 30,000 m2
- New capacities to meet growing demand
Siemens
Mobility is expanding its manufacturing and services facility in Munich-Allach
in order to meet the growing demand for locomotives and services. The factory
will be enlarged to 80,000 m2 from its current 50,000 m2
to provide additional capacities for processing new orders, optimizing
production and logistics flows within the facility, and add more office space.
- Presentation of framework agreement with Siemens
Mobility worth €400 Million for further ETCS expansion
- ETCS enables shorter headways and greater reliability
Siemens
Mobility and ÖBB (Austrian Federal Railways) are digitizing the Austrian rail
network to further enhance the attractiveness of public transport. ÖBB is aiming
to double the capacity of Austria’s entire rail system by 2040 to cope with
increasing passenger numbers. This goal is now a bit closer: The most modern
technology for railway operations – the digital European Train Control System ETCS – has now been implemented and commissioned on the 57-kilometer route
between Linz and Vöcklabruck. The system controls distances between trains, as
well as their direction and speed in real time. This enables the route to carry
more passengers and freight, and ensures that the trains run more reliably,
punctually, and safely.
Siemens Mobility and Cattron presented the
next development phase of the government-funded research project Autonomous
Tram in Depot today at InnoTrans 2022: remote train operation (RTO). The world
premiere marks the next critical milestone for RTO in the project and was
successfully presented today to the project organizer TÜV Rheinland at the
depot of the public transportation company ViP Verkehrsbetrieb Potsdam GmbH.
- First CBTC project in India with GoA 4, the highest grade of automation
- Will allow for trains to be automatically controlled and operated
- Automated signaling and train operations will provide greater availability and enhance operations and passenger experience
Siemens Mobility and Siemens Limited India is partnering with Bengaluru Metro Rail Corporation Limited (BMRCL) to implement a comprehensive set of automated train solutions for phase 2 of the Bengaluru metro expansion project. This will be the first CBTC project in India with GoA 4, the highest grade of automation that allows for trains to be automatically controlled and operated. Siemens Mobility will install its communications-based train control (CBTC) system across 18.8 km of the Yellow Line, which will feature electronic interlockings, an automatic train protection and supervision system, as well as a telecommunication system. The automated signaling and train operations will allow BMRCL to run trains 90 seconds apart, providing greater availability and an enhanced passenger experience.
- €110 million contract to provide a fully automated yard management system
and maintenance services for the Kijfhoek marshalling yard
- Automated
and digital systems will optimize yard operations and improve efficiency,
reliability, and safety
- Kijfhoek is the
largest freight yard in the Netherlands and a vital link
between the Rotterdam ports and major industrial areas in Europe
Siemens Mobility has been
awarded a €110 million contract by ProRail B.V. to modernize and
optimize the Kijfhoek freight railyard, the largest yard in the
Netherlands and a vital link between the Rotterdam ports and major industrial
areas in Europe. This contract includes
providing a state-of-the-art fully automated system to manage yard operations and
15 years of maintenance services. Located south-east of
Rotterdam, the Kijfhoek marshalling yard encompasses 50 hectares, with 14 arrival
tracks, 41 classification tracks and 12 stabling tracks.
- First X-Wagen
metro now running on the U3 line – more trains follow
in the summer
- Innovative
digital passenger information and guidance system displays real-time
information above each door
- New air-free brake system
- Greater
comfort and security, optimal accessibility
The X-Wagen metro has
initiated passenger service on the Wiener Linien. After undergoing extensive
tests and receiving its operating permit, the first train of the new metro
generation officially began service on the U3 line this morning. The train’s
inaugural run was accompanied by Vienna City Councilor Peter Hanke and numerous
project participants from Wiener Linien and Siemens Mobility, among others.
- Depot to be expanded to 87,550 m²
- New capacity for meeting growing demand
- 100% system availability thanks to digitalized depot operation
- Creation of attractive jobs in the region
- Up to 250 employees at the location in 2026
Siemens Mobility is investing approximately €150 million to expand its service depot in
Dortmund-Eving to 87,550 m² to meet the growing demand for rail services.
Plans call for constructing an additional 12,300 m² service hall
with storage facility, offices, and workshops to handle the maintenance of
trains up to 400 meters long. Construction
of the new building is scheduled to begin in 2024 and be completed by 2026. The
Siemens Mobility depot in Dortmund previously had a total area of
70,000 m² and will cover 157,550 m² when the project is
completed.
- Automated signaling and electrification systems to be installed on commuter Lines 8 and 9 in São Paulo
- Will provide greater availability, enhanced operations, improved sustainability, and better passenger experience
Siemens Mobility has been awarded two contracts by ViaMobilidade Linhas 8 e 9 to upgrade and modernize the São Paulo metro network. ViaMobilidade is part of the Brazilian infrastructure company CCR Mobilidade and are responsible for all urban mobility projects for the CCR Group in the country. Siemens Mobility will equip Line 8 with an automated signaling system and will install new electrification and traction power systems on both Line 8 and 9. The renewal of both lines will provide for greater availability, enhanced operations, increased sustainability, and an improved passenger experience. These contracts build on the already well-established relationship Siemens Mobility has with the concessionaire and the São Paulo metropolitan transportation network.