Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens Mobility to provide CBTC and automated train technology for Bengaluru Metro 

“Siemens Mobility is excited to partner with Bengaluru Metro Rail on this groundbreaking project that will provide this new rail line with the highest grade of signaling technology and automation services, said Michael Peter, CEO of Siemens Mobility. “Our state of the art CBTC signaling at GoA 4 will allow trains to operate driverless, as they will be automatically controlled and supervised without any onboard intervention. This will deliver a truly modern system featuring superior availability, reliability and passenger experience.”
Bengaluru is the capital of the Indian state of Karnataka and its urban area population is estimated at more than 12 million. Bengaluru is widely regarded as the "Silicon Valley” or IT capital of India because of its role as the nation's leading IT exporter. 
The Bengaluru metro system, commonly called the Namma Metro, is being built in stages. Phase 1 was made operational in June 2017 and has a daily ridership of 450,000. The system covers 42.3 km and serves 40 stations, with lines running north/south and east/west. The currently under construction Phase 2, plans to cover 72.1 km and add two new lines that will further extend the system on its existing grid. The 18.8 km on the Yellow Line that will be equipped with Siemens Mobility CBTC technology will have 16 elevated stations. 
The Siemens Mobility high-performance CBTC system lets operators maximize their network capacity and throughput. The radio-based technology provides real-time data on vehicle position and speed conditions, allowing system operators to safely increase the number of vehicles on a rail line. Additionally, the technology precisely locates each train on the tracks and controls speed, improving safety for riders and employees, while also providing the ability for continuous updates on system status that results in fewer delays and up-to-date travel information.
The Siemens Mobility CBTC solution is the most extensively deployed automatic train control system and is used by operators around the world, like Sao Paulo, Paris, Beijing, Singapore, and New York.

For this press release

Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2020, which ended on September 30, 2020, Siemens Mobility posted revenue of €9.1 billion and had around 38,500 employees worldwide. Further information is available at: www.siemens.com/mobility.
Read more
Reference Number: HQMOPR202012096091EN

Contact

Chris Mckniff

Siemens Mobility GmbH

+1 646-715-6423