For the first time in many decades, a private company began planning and developing a fast intercity connection in the United States in 2012. The new Florida East Coast Railway will operate up to 16 pairs of trains from Miami Central Station via Fort Lauderdale to West Palm Beach.
In 2014, the Departments of Transportation of California, Illinois and Maryland ordered an initial lot of 34 Charger locomotives from Siemens, with an option for a total of 222 locomotives. The contract back then was valued at approximately €165 million ($225 million). Due to orders from other states as well as by the private rail operator All Aboard Florida, the total number of Chargers ordered amounts to 81 in 2017. The locomotives are deployed in corridors of the US states for regional and mainline trains travelling for Caltrains (California) as Amtrak Pacific Surfliner, in Washington as Amtrak Cascades and in Maryland with the regional network MARC. Under the "Brightline" brand, ten Chargers are being deployed in high-speed rail services between Miami and West Palm Beach; Orlando is due to follow at a later date.
China's megacities alone are home to more than 260 million people. These gigantic conurbations have recently undergone rapid growth of almost two percent per year, and are suffering increasing traffic problems caused by the soaring rate of car use. Hence the correspondingly strong demand for solutions for the further development of urban rail transport. The Nanjing customer has now commissioned Siemens to equip metro Ninghe Line with the CBTC automatic train protection system Trainguard MT. The contract includes the CBTC trackside equipment for the 36 kilometer line as well as the ATC equipment of the 24 trains. In the long term more than ten metro lines will be built in Nanjing – of which five alone will or already been feature Siemens signaling technology.Siemens can look back on a long partnership in China with the Nanjing Metro Corporation. Siemens equipped metro line 1, which started running in 2005 and is now 47 kilometers long, as well as metro line 2 in 2010. Line 2 serves 26 stations and forms the east-west tangent of the city of Nanjing in eastern China. Following the extension of the city's metro with line 2, the rail network now covers 85 kilometers. Line 10, Nangjing's first cross-Yangtze river metro line was put into operation on July 1, 2014. Its first phase runs 23.6 kilometers with 14 stations. The latest Nanjing metro line fitted with signaling technology from Siemens is Nanjing Metro Line 3, which went on public operation on April 1, 2015.
Siemens AG is constructing a modern and sustainably designed Siemens Campus Erlangen in the southern part of the city of Erlangen, Germany. By 2030, the company's research center in the south of the city will have been transformed step-by-step into one of Siemens' most advanced locations worldwide. Future-oriented office, research and laboratory jobs will be located on the campus. Equipped with the most advanced building and energy technologies, it will be developed over the long term into Siemens' first CO
2-neutral location worldwide. A new urban residential and living environment will arise on the campus grounds. Siemens will be part of the community as never before. Designed by the Frankfurt architects KSP Jürgen Engel Architekten, the campus's open plan will link the company and society and provide a basis for the exchange of ideas.
The construction project has a planned investment volume of some €500 million and will cover an area of 54 hectares. Siemens Campus Erlangen underscores the company's long-term commitment to its Erlangen location and will be a symbol of innovative power for employees and for the region. The project was planned and designed in close cooperation with the state of Bavaria and the city of Erlangen.
The discovery of the dynamo-electric principle has brought about greater changes to the way our society lives than practically any other scientific breakthrough. By inventing the dynamo machine, not only did Werner von Siemens help bring about the advent of electrical machinery, he was also instrumental in accelerating and facilitating industrial processes. Seen from the perspective of society, this completely changed accepted concepts of time and mobility.
The Velaro D is the fourth generation of high-speed trains that Siemens has developed on the basis of the Velaro platform. Deutsche Bahn AG (DB) classifies the train as the new Series 407 ICE 3 (predecessors: Series 403 and Series 406 ICE 3). In December 2013, Germany's Federal Railway Authority (EBA) approved the trains' operation – also in multiple-unit or so-called double-traction mode – on the Deutsche Bahn rail network. Passenger operation started on December 21, 2013.
Authorization for operation in single-traction mode in France was granted in April 2015. Since June 2015 the trains have been travelling to Paris in regular passenger operation. In addition to Germany and France, the Velaro D is also intended for cross-border operation in Belgium.
Since 2007, trains based on the Velaro platform have operated with high reliability for more than one billion kilometers in China, Russia, Spain and Turkey – equal to roughly 25,000 times around the globe.
In May 2014 Siemens, together with the public utilities of Mainz, Linde and the RheinMain University of Applied Sciences, has laid the foundation stone for a new type of energy storage system. Now, time has come: By pressing a symbolic button, the Chairman of the Board of Linde Group, Dr. Wolfgang Büchele, Siemens board member Professor Siegfried Russwurm, two board members of Stadtwerke Mainz AG, Detlev Höhne and Dr. Tobias Brosze, and Professor Dr. Detlev Reymann, President of RheinMain University, officially launched a hydrogen production plant at the Energiepark Mainz on July 2, 2015. With the support of the German Federal Ministry of Economics and Technology as part of the Energy Storage Funding Initiative the 17-million-project could be realized. The system, equipped with an electrolyzer from Siemens, will convert surplus electricity from wind farms to hydrogen from now on. In this way, it will be possible to store electricity from renewable sources over longer periods of time. With a peak rating of up to 6 megawatts the plant is the largest of its kind in the world.
The principle of electrolysis has been tried and tested for decades. What is special about the Mainz system is that it involves highly dynamic PEM high-pressure electrolysis which is particularly suitable for high current density and can react within milliseconds to sharp increases in power generation from wind and solar sources. In this electrolyzer a proton exchange membrane (PEM) separates the two electrodes at which oxygen and hydrogen are formed. On the front and back of the membrane are precious-metal electrodes that are connected to the positive and negative poles of the voltage source. This is where the water is split. The system in Mainz will thus have a capacity relevant for bottlenecks in the grid and small wind farms.
Siemens will deliver 1,140 commuter rail carriages to the British capital. This is the largest order that Siemens has ever won in Great Britain and one of the biggest orders for Siemens' global rolling stock business. The first Desiro City train for the Thameslink network in Greater London was delivered and entered service in June 2016. By the end of 2018, a total of 115 trains will have been delivered. Siemens will take over the complete long-term servicing and maintenance for this new fleet of trains. The Thameslink north-south commuter route runs through London, connecting Bedford, located to the north east of the capital, with Brighton, on the south coast.
Introducing a high capacity, high frequency service of longer trains, extended platforms and new stations, the project is regarded as one of the largest rail infrastructure projects in the UK.
The first passenger train will roll through the Gotthard Base Tunnel early June 2016. Siemens has supplied the tunnel control and fire protection systems for the world's longest railway tunnel. The sophisticated safety system has over 200,000 sensors, and places maximum demands on logistics and data processing.The control system controls and monitors all installations completely automatically. The tunnel is fitted with sensors, control electronics and surveillance equipment. This includes video cameras in the multifunction points, which are connected by optical fiber cables to two tunnel control centers located at the north and south entrances. Siemens has installed a tunnel control system in each center, each system acting as a reserve for the other. The movement of each train is recorded, and displayed in the control center. The system controls the entire infrastructure, which has 3,200 kilometers of electrical cables and 2,600 kilometers of data cables. It detects a door that has not been closed properly or a light that has failed. When required, the ventilation system is activated, the light at the next emergency stop point is switched on, and the doors are opened automatically. What is actually happening is seen on screen by the around 60 employees on duty in the centers. "Events" are classified according to five alarm stages. The system provides information and decision-making steps for each stage to help the head of operations. Sensors check the trains for overheated brakes and leaks before they enter the tunnel and without requiring them to stop. However, the main task of the new system is to maintain availability. The maintenance periods, such as close-down times and spare parts requirement, can be efficiently planned with a new tool.It goes without saying that safety is paramount in a tunnel where in the near future more than 200 trains a day will barrel through the tubes at speeds up to 250 km/h. The tubes are connected every 300 meters by crosscuts that allow train passengers to escape to the other tube in case of a fire. Each tube has two emergency-stop stations 600 meters in length which allows the evacuation of up to 1,000 passengers.
Copenhagen's S-tog (commuter rail system) is the backbone of the capital's public mass transit network. It carries around 350,000 passengers a day - and that number is growing all the time. This reflects the growth in the metropolitan area around the Danish capital where more than one fifth of the entire population of Denmark now lives. So, in the space of six years, Siemens will equip Copenhagen's entire commuter rail network with the Trainguard MT train control system which uses Communications-Based Train Control (CBTC) to automate operation. This has made it possible to reduce train headways from 120 seconds to 70 seconds within the inner-city area.
The first phase; the newly opened 25 kilometer section of Line A runs from the suburb of Hillerod in the north to Jaegersborg east of the capital and will be used by more than 70.000 commuters a day. Once the complete network is open, up to 84 trains an hour will travel on the core network - equivalent to more than 1 million passengers per year. The remaining phases will enter passenger service in the coming years.