- Industrial Connectivity Lab opens at the Erlangen site
- Test environment for industrial connectivity technologies
- 5G, WLAN, RTLS, and RFID: Users test application scenarios and interoperability in industrial conditions
The technology company Siemens has opened a new test laboratory for industrial connectivity technologies at its Erlangen site. Embedded in the Siemens Technology Center on the Erlangen campus, the Industrial Connectivity Lab offers 300 square meters of space for extensive testing of any connectivity solution in industrial environments: Industrial WLAN, 5G, real-time localization systems (RTLS), and radio frequency identification (RFID).
Nuremberg, November 14 to November 16, 2023
- Infrastructure for private industrial 5G networks with a focus on automation applications
- The solution is already in use at Siemens plants and pilot customers like Salzgitter AG
- 5G is crucial for mobile robots, autonomous logistics, driverless transport systems, and edge devices
For the first time, the technology company Siemens is launching a private infrastructure developed in-house for the 5G mobile communications standard. The solution enables industrial companies to build their own local 5G networks that will provide optimal support for automation applications. "By building their own 5G networks, industrial companies are launching the next stage of connected production," says Axel Lorenz, CEO of Process Automation at Siemens. "5G is crucial for applications like mobile robots, autonomous logistics, and driverless transport systems in factories. Siemens' private 5G infrastructure also gives users sole control over the data in their 5G network at all times, and they can custom-configure the network for their applications."
- eXplore Live at Deloitte’s The Smart Factory @ Wichita helps companies experience the future of smart manufacturing and the power of digitalization using the Siemens Xcelerator portfolio
- New dedicated space allows Siemens, Deloitte and other collaborators to bring suppliers and customers together to work towards engineering excellence
Siemens
Digital Industries Software today announced the opening of eXplore Live at The Smart
Factory @ Wichita, an experience center convened by Deloitte that marries an
ecosystem of world-leading organizations with business strategy and
cutting-edge technology to demonstrate Industry 4.0. Located on Wichita State
University’s Innovation Campus, The Smart Factory includes a fully operational
production line and experiential labs for developing and exploring innovative
capabilities of smart manufacturing.
- Transmission of Profinet IO packets via a private 5G network
- VXLAN as transmission technology embeds Profinet protocol
- Use of a central control system for multiple mobile participants reduces energy and maintenance costs
Siemens enables the transmission of Profinet IO
via a private 5G network, which allows data to be transmitted in real time for
industrial applications. This is made possible by the VXLAN (Virtual Extensible
LAN) transmission technology in the Scalance 5G routers and security appliances
from Siemens. VXLAN embeds the Profinet IO protocol, which is transmitted in
Layer 2, into Layer 3 packets, which allows them to be transmitted across
network boundaries. Since Layer 2 communication now takes place via 5G, a
central controller can communicate with decentralized I/O modules on mobile
devices such as automated guided vehicles (AGVs) via Profinet in a private 5G
network and no local controls have to be used on the individual AGVs. This
saves costs and reduces maintenance. At the Hannover Messe, visitors can see
this innovation at the booth of the organization "5G-ACIA" in Hall 9.
This year, the 1.4 million square meter Deutsche Messe exhibition site in Hanover, Germany will become 5G-ready. Deutsche Messe, which organizes international capital goods trade shows, has obtained a frequency allocation in the 3.7-3.8 GHz range from the Bundesnetzagentur (Federal Network Agency) and will set up one of the largest 5G zones in Europe, spanning 30 halls and buildings as well as the entire open-air ground. Siemens is playing a very specific role in this achievement. As one of the key exhibitors at the HANNOVER MESSE, Siemens is setting up a private 5G campus network with a focus on industrial use in one of the exhibition halls in Hanover. The network can be used by exhibitors during trade shows and, outside of trade show times, can be used by companies for tests and field trials.
- Scalance MUM856-1 connects local industrial applications to public 5G, 4G, and 3G mobile wireless networks
- Router supports future-oriented applications such as remote access via public 5G networks or the connection of mobile devices such as automated guided vehicles in industry
- Robust version in IP65 housing for use outside the control cabinet
- Prototypes of Siemens 5G infrastructure for private networks already in use at several sites
The Scalance
MUM856-1 – the first industrial 5G router from Siemens – is available now. The
device connects local industrial applications to public 5G, 4G (LTE), and 3G
(UMTS) mobile wireless networks. The router can be used to remotely monitor and
service plants, machines, control elements, and other industrial devices via a public
5G network – flexibly and with high data rates. Demand for this type of
solution is growing in industry. In addition, the device can be integrated into
private 5G networks. The Scalance MUM856-1 therefore supports future-oriented
applications such as mobile robots in manufacturing, autonomous vehicles in
logistics or augmented reality applications for service technicians. Thanks to
a robust IP65 housing, the router can also be used outside the control cabinet,
for example under harsh conditions in production or in outdoor facilities in
the water industry.
- Mercedes-Benz and Siemens to expand the digitalization of sustainable production methods, expanding a long-standing successful cooperation in the field of engineering and production
- Partnership to develop innovative solutions for the qualification of employees, digitalization and for increasing energy efficiency in production
Mercedes-Benz and Siemens plan to cooperate on advancing digitalization and automation in the automotive industry, supported by the State of Berlin. Mercedes-Benz AG aims to digitize its production processes. Siemens, a leading supplier in the field of automation, industrial software and smart infrastructure, will bring its expertise and technologies to the partnership to develop highly flexible, efficient and sustainable automotive production together with Mercedes-Benz.
- „Infinite opportunities from infinite data“ is this year's trade fair motto
- Leveraging the full potential of data from merging the virtual and physical worlds
- "Digitalization knows no end"
- Expansion of the portfolio for edge computing in industry
Under the motto "Infinite opportunities from infinite data", Siemens is demonstrating at the "Digital Enterprise Virtual Experience" at Hannover Messe 2021 how the merging of the physical and virtual worlds enables industrial enterprises to act flexibly and sustainably, as they are facing huge challenges: The Covid 19 pandemic has changed markets and requirements almost overnight. Added to this are the growing individualization and the urgent need for more sustainability. This can only be mastered with the help of digitalization and automation. Siemens brings together the data generated in this process in a continuous cycle between the virtual and physical worlds. This enables companies to better understand and use data. Traditional silos between previously separate industrial domains are breaking down and new opportunities for sustainable and flexible production are being created. This enables employees in industrial enterprises to make appropriate decisions based on data or, for example, to react a lot faster to changes such as suddenly increased resource consumption.
T-Systems and Siemens today announced a partnership to offer new end-to-end solutions that combine their respective capabilities in Information Technology (IT), Telecommunications (TC) and Operational Technology (OT). The joint solutions will cover enterprise business applications like Enterprise Resource Planning (ERP), Customer Relationship Management (CRM), Supply Chain Management (SCM) and Manufacturing Engineering Systems (MES), with TC solutions helping to enable real-time interaction and collaboration and OT solutions covering shop floor-based driving engineering, production or operation processes. The new solutions can help companies leverage a full range of technologies, which have the potential to reinvent German industry, including Cloud, 5G and Edge Computing.