Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens makes first industrial 5G router available 

The Scalance MUM856-1 – the first industrial 5G router from Siemens – is available now. The device connects local industrial applications to public 5G, 4G (LTE), and 3G (UMTS) mobile wireless networks.

The Scalance MUM856-1 – the first industrial 5G router from Siemens – is available now. The device connects local industrial applications to public 5G, 4G (LTE), and 3G (UMTS) mobile wireless networks.

To ensure the powerful connection of Ethernet-based subnetworks and automation devices, the Scalance MUM856-1 supports Release 15 of the 5G standard. The device offers high bandwidths of up to 1000 Mbps for the downlink and up to 500 Mbps for the uplink – providing high datarates for data-intensive applications such as the remote implementation of firmware updates. Thanks to IPv6 support, the devices can also be implemented in modern communication networks. Various security functions are included in order to monitor data traffic and protect against unauthorized access: for example, an integrated firewall as well as authentication of communication devices and encryption of data transmission via VPN. If there is no available 5G network, the device switches automatically to 4G or 3G networks. The first release version of the router has an EU radio license; other versions with different licenses are in preparation. With the Sinema Remote Connect management platform for VPN connections, users can access remote plants or machines easily and securely – even if they are integrated in other networks. The software also offers easy management and autoconfiguration of the devices. 

Successful use of prototypes for private 5G networks

Besides connectivity to public networks, Scalance MUM856-1 also supports integration into private local 5G campus networks. Siemens is testing this use case in their own Automotive Showroom and Test Center in a prototype of a standalone 5G test network, which is based on Siemens components. The 5G infrastructure used here comprises a 5G core, a distributed unit, and several radio units. Siemens has also built another prototype of a private 5G infrastructure in its plant in Amberg, and their Karlsruhe plant will be equipped soon. In these systems, Siemens is relying exclusively on its own independently developed products and solutions. In addition, Siemens is currently implementing private network technology for a 5G campus network with a focus on industrial use in one of the Deutsche Messe AG exhibition halls in Hanover. This private 5G network will be ready for use in early September. The network can be used by exhibitors during trade shows and, outside of trade show times, can be used by companies for tests and field trials.

Background info:

In industry, in addition to the need for local wireless connectivity, there is increasing demand for remote access to machines and plants. In these cases, communication is usually over long distances. Public mobile networks can be used to access devices that are located at a considerable distance, for example in other countries.In addition, service technicians can connect to the machines they need to service via the mobile network while on the go. Public 5G networks are therefore an important element of remote access and remote servicing solutions. They can be used, for example, to provide users with very high bandwidths in urban areas with small radio cells and high frequencies. In rural areas, radio cells have to cover a large area, which is why lower frequencies are used. Particularly at the edges of radio cells, for example for LTE or UMTS, there are often significant losses in terms of both the bandwidth and stability of the communication connection. And it is exactly in these remote areas where stable bandwidth transmission is required for remote servicing or video transmission, for example for water stations. With innovative 5G communications technologies, considerably more bandwidth with greater reliability is available at the edges of radio cells and the average data rate for users within a radio cell increases. The router was launched last November at SPS 2020 - https://sie.ag/39bOwoy
You can find more information on Siemens@Achema Pulse here:
www.siemens.com/achema

For this press release

Press Folders

Follow us on Social Media

Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Read more
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2020, which ended on September 30, 2020, the Siemens Group generated revenue of €55.3 billion and net income of €4.2 billion. As of September 30, 2020, the company had around 293,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: HQDIPR202106076224EN

Contact

David Petry

Siemens AG

+49 173 537 1050