- Industrial Connectivity Lab opens at the Erlangen site
- Test environment for industrial connectivity technologies
- 5G, WLAN, RTLS, and RFID: Users test application scenarios and interoperability in industrial conditions
The technology company Siemens has opened a new test laboratory for industrial connectivity technologies at its Erlangen site. Embedded in the Siemens Technology Center on the Erlangen campus, the Industrial Connectivity Lab offers 300 square meters of space for extensive testing of any connectivity solution in industrial environments: Industrial WLAN, 5G, real-time localization systems (RTLS), and radio frequency identification (RFID).
- Infrastructure for private industrial 5G networks with a focus on automation applications
- The solution is already in use at Siemens plants and pilot customers like Salzgitter AG
- 5G is crucial for mobile robots, autonomous logistics, driverless transport systems, and edge devices
For the first time, the technology company Siemens is launching a private infrastructure developed in-house for the 5G mobile communications standard. The solution enables industrial companies to build their own local 5G networks that will provide optimal support for automation applications. "By building their own 5G networks, industrial companies are launching the next stage of connected production," says Axel Lorenz, CEO of Process Automation at Siemens. "5G is crucial for applications like mobile robots, autonomous logistics, and driverless transport systems in factories. Siemens' private 5G infrastructure also gives users sole control over the data in their 5G network at all times, and they can custom-configure the network for their applications."
- New innovation hub for research at Siemens in Garching, Germany
- Joint research facility with Technical University of Munich in Garching’s “Isar Valley”
- Modern and open work environments in a digitally planned, sustainable building
Just nine months after construction began, a
topping-out ceremony is being celebrated for the new Siemens Technology Center
at the research campus in the university town of Garching, Germany, near
Munich. As a result, this new building – which was planned digitally and is
being built to meet stringent sustainability requirements – has thus now
reached an important milestone on the journey to Siemens’ future research activities in the
Munich area. With its modern work environments, this facility will serve as an
innovation hub that provides space for inspiration and new ideas. At this center,
more than 450 researchers from Siemens’ “Technology” unit will collaborate on
technologies of the future with around 150 employees and students from the
Technical University of Munich (TUM).
- eXplore Live at Deloitte’s The Smart Factory @ Wichita helps companies experience the future of smart manufacturing and the power of digitalization using the Siemens Xcelerator portfolio
- New dedicated space allows Siemens, Deloitte and other collaborators to bring suppliers and customers together to work towards engineering excellence
Siemens
Digital Industries Software today announced the opening of eXplore Live at The Smart
Factory @ Wichita, an experience center convened by Deloitte that marries an
ecosystem of world-leading organizations with business strategy and
cutting-edge technology to demonstrate Industry 4.0. Located on Wichita State
University’s Innovation Campus, The Smart Factory includes a fully operational
production line and experiential labs for developing and exploring innovative
capabilities of smart manufacturing.
- Transmission of Profinet IO packets via a private 5G network
- VXLAN as transmission technology embeds Profinet protocol
- Use of a central control system for multiple mobile participants reduces energy and maintenance costs
Siemens enables the transmission of Profinet IO
via a private 5G network, which allows data to be transmitted in real time for
industrial applications. This is made possible by the VXLAN (Virtual Extensible
LAN) transmission technology in the Scalance 5G routers and security appliances
from Siemens. VXLAN embeds the Profinet IO protocol, which is transmitted in
Layer 2, into Layer 3 packets, which allows them to be transmitted across
network boundaries. Since Layer 2 communication now takes place via 5G, a
central controller can communicate with decentralized I/O modules on mobile
devices such as automated guided vehicles (AGVs) via Profinet in a private 5G
network and no local controls have to be used on the individual AGVs. This
saves costs and reduces maintenance. At the Hannover Messe, visitors can see
this innovation at the booth of the organization "5G-ACIA" in Hall 9.
This year, the 1.4 million square meter Deutsche Messe exhibition site in Hanover, Germany will become 5G-ready. Deutsche Messe, which organizes international capital goods trade shows, has obtained a frequency allocation in the 3.7-3.8 GHz range from the Bundesnetzagentur (Federal Network Agency) and will set up one of the largest 5G zones in Europe, spanning 30 halls and buildings as well as the entire open-air ground. Siemens is playing a very specific role in this achievement. As one of the key exhibitors at the HANNOVER MESSE, Siemens is setting up a private 5G campus network with a focus on industrial use in one of the exhibition halls in Hanover. The network can be used by exhibitors during trade shows and, outside of trade show times, can be used by companies for tests and field trials.
- Scalance MUM856-1 connects local industrial applications to public 5G, 4G, and 3G mobile wireless networks
- Router supports future-oriented applications such as remote access via public 5G networks or the connection of mobile devices such as automated guided vehicles in industry
- Robust version in IP65 housing for use outside the control cabinet
- Prototypes of Siemens 5G infrastructure for private networks already in use at several sites
The Scalance
MUM856-1 – the first industrial 5G router from Siemens – is available now. The
device connects local industrial applications to public 5G, 4G (LTE), and 3G
(UMTS) mobile wireless networks. The router can be used to remotely monitor and
service plants, machines, control elements, and other industrial devices via a public
5G network – flexibly and with high data rates. Demand for this type of
solution is growing in industry. In addition, the device can be integrated into
private 5G networks. The Scalance MUM856-1 therefore supports future-oriented
applications such as mobile robots in manufacturing, autonomous vehicles in
logistics or augmented reality applications for service technicians. Thanks to
a robust IP65 housing, the router can also be used outside the control cabinet,
for example under harsh conditions in production or in outdoor facilities in
the water industry.
- Mercedes-Benz and Siemens to expand the digitalization of sustainable production methods, expanding a long-standing successful cooperation in the field of engineering and production
- Partnership to develop innovative solutions for the qualification of employees, digitalization and for increasing energy efficiency in production
Mercedes-Benz and Siemens plan to cooperate on advancing digitalization and automation in the automotive industry, supported by the State of Berlin. Mercedes-Benz AG aims to digitize its production processes. Siemens, a leading supplier in the field of automation, industrial software and smart infrastructure, will bring its expertise and technologies to the partnership to develop highly flexible, efficient and sustainable automotive production together with Mercedes-Benz.
- Corporate real estate management now also for external customers
- Renting, development and consulting in focus
- Intelligent real estate in close cooperation with other Siemens units
Siemens Real Estate (SRE) has been managing Siemens' real estate portfolio for more than 20 years and, as a versatile and future-oriented corporate real estate manager, has repeatedly adapted to the challenges of the market. Effective immediately, SRE will make the expertise it has acquired available to external clients for the first time. Companies that do not yet have their own professional real estate management will thus have access to SRE's knowledge and experience in the three product groups of consulting, renting and real estate and location development.