Control rooms of process engineering plants are usually
as old as the plant itself, often 30 years and more. Today, digital
transformation is placing new demands on automation: Simatic PCS neo is a brand-new system software, which
offers companies in the process industry unique opportunities in the age of
digitalization. Main features include global web-based collaboration in
engineering and operation and intuitive handling representing all relevant
information in a single workbench.
Let the good times roll: Starting September 21, about six million people from all around the world will be enjoying themselves at the Oktoberfest in Munich for two weeks. Traditionally, Siemens supplies drives and control systems as well as energy distribution for the festival's rides. Automation solutions from Siemens also control special beer pipelines – the only ones of its kind worldwide –that supply the Hacker, Winzerer Faehndl and Braeurosl festival tents with their tasty Oktoberfest brews. Because many breweries use Siemens technologies within their brewing process, Siemens doesn't only ensure fresh beer at the Oktoberfest.
Siemens Water Solutions successfully installed and started up a Zimpro® wet air oxidation (WAO) system at a global petrochemical company’s olefins plant in the Southern U.S.
The order, received in November 2017, is the second Zimpro® wet air oxidation system supplied to the customer. The first system was supplied in 2004.
The Zimpro® WAO system will treat spent caustic generated in the production of ethylene by destroying odorous and high chemical oxygen demand (COD) pollutants. The system also generates an effluent that can be safely neutralized and sent to a biological treatment plant, where it is further treated for discharge.
Siemens Water Solutions addresses water and wastewater needs of the oil and gas industry with a portfolio that includes physical and chemical separation, biological treatment, and complex hydrothermal technologies.
New research from Siemens Financial services explains how manufacturers are in a race against time to gain competitive advantage from Industry 4.0 investment, before the “tipping point” of majority adoption. A must-read for future focused manufacturing financial managers, the Whitepaper explains how Finance 4.0 solutions are providing practical methods of helping companies to urgently invest in Industry 4.0 and gain early mover advantage.
On March 2nd, 2017, German Chancellor Angela Merkel, Egyptian President Abdel Fattah El-Sisi, Siemens CEO Joe Kaeser and further high-ranking representatives witnessed the symbolic inauguration of the first phase of Siemens' megaproject in Egypt. The event marked an important milestone towards the completion of the project.
In collaboration with the Egyptian Ministry of Electricity and Renewable Energy, Siemens and its consortium partners, Orascom Construction and Elsewedy Electric, announced on July 24, 2018 the completion of the Egypt Megaproject in record time. The parties celebrated the combined cycle commissioning and the start of operations at the Beni Suef, Burullus and New Capital power plants. The stations will add a total of 14.4 gigawatts (GW) of power generation capacity to Egypt's national grid, enough power to supply up to 40 million people with reliable electricity. With this milestone, Egypt and Siemens have set a new world record for execution of modern, fast-track power projects, delivering 14.4 GW of power in only 27.5 months. A single combined cycle power plant block with a capacity of 1,200 megawatts typically takes approximately 30 months for construction. For the Egypt Megaproject Siemens in parallel built twelve of these blocks in record time and connected them to the grid.
Following the delivery of several Siemens SGT5-8000H gas turbines, the first steam turbine for the Egypt Megaproject began its journey in December 2016 from the Siemens factory in Muelheim to the power plant Beni Suef in Egypt. The main components of the 670-ton cargo were lifted with a heavy-duty crane from the production hall onto a transport vessel standing by at the plant's inland harbor facilities. The vessel transported the SST-5000 steam turbine from Muelheim to the deep-water port of Antwerp where it was loaded onto a heavy cargo ship and transported to Egypt.
After the steam turbines installation, the waste heat from the gas turbines will be used to produce steam that will then drive the steam turbine, thus increasing the overall power output and efficiency of the power plant. In total, Siemens will deliver twelve SST-5000 steam turbines for the Egyptian power plants Beni Suef, Burullus and New Capital. All of these steam turbines will be manufactured at the Siemens factory in Muelheim.
Scandinavia is the first region in the world to rely increasingly on battery-powered and thus environmentally-friendly technologies in the shipbuilding industry. After "Ampere", the world's first electrical ferry in Norway, and a follow-up order of the Finnish shipping company FinFerries, Siemens has now received an order from Norwegian ferry operator Fjord1. Ampere was put into operation in Norway in May 2015, and has traveled a distance equivalent to more than 1.5 times around the equator. With the change from diesel propulsion to battery, Norwegian ship owner Norled has reduced the cost of fuel by 60 percent. Now Siemens has tailor-made a suitable technical solution for Fjord1. With this contract, the first four battery-driven ferries in the world will run on technology developed and manufactured by Siemens.
"Elektra" - the newest member of the electric ferry fleet: In June 2017, the Elektra began regular operation between Nauvo and Parainen in the Turku archipelago. Battery packs, which are charged via the land-based charging stations in the harbor for use by the ferry, serve as the primary source of energy, with Diesel engines used as emergency power units. The Elektra is also Europe's largest car ferry. At nearly 98 meters long and 16 meters wide, the Elektra can transport up to 90 cars per trip. The ferry purchased by FinFerries will now be traveling this route every 15 minutes. The batteries will be charged in roughly five minutes while cars move off and onto the ferry. The two lithium-ion batteries each have a capacity of 530 kWh.
For many holiday-makers, a cruise on board a luxury liner is right up at the top of their wish list. No wonder that the leisure cruising market has been booming for many years. In the past year alone, more than 20 million cruise passengers embarked in locations around the world – and the trend is upwards. This year saw the launch of the Aida shipping company's ninth ship fitted out with automation technology from Siemens.
Siemens AG is constructing a modern and sustainably designed Siemens Campus Erlangen in the southern part of the city of Erlangen, Germany. By 2030, the company's research center in the south of the city will have been transformed step-by-step into one of Siemens' most advanced locations worldwide. Future-oriented office, research and laboratory jobs will be located on the campus. Equipped with the most advanced building and energy technologies, it will be developed over the long term into Siemens' first CO
2-neutral location worldwide. A new urban residential and living environment will arise on the campus grounds. Siemens will be part of the community as never before. Designed by the Frankfurt architects KSP Jürgen Engel Architekten, the campus's open plan will link the company and society and provide a basis for the exchange of ideas.
The construction project has a planned investment volume of some €500 million and will cover an area of 54 hectares. Siemens Campus Erlangen underscores the company's long-term commitment to its Erlangen location and will be a symbol of innovative power for employees and for the region. The project was planned and designed in close cooperation with the state of Bavaria and the city of Erlangen.
The discovery of the dynamo-electric principle has brought about greater changes to the way our society lives than practically any other scientific breakthrough. By inventing the dynamo machine, not only did Werner von Siemens help bring about the advent of electrical machinery, he was also instrumental in accelerating and facilitating industrial processes. Seen from the perspective of society, this completely changed accepted concepts of time and mobility.
In May 2014 Siemens, together with the public utilities of Mainz, Linde and the RheinMain University of Applied Sciences, has laid the foundation stone for a new type of energy storage system. Now, time has come: By pressing a symbolic button, the Chairman of the Board of Linde Group, Dr. Wolfgang Büchele, Siemens board member Professor Siegfried Russwurm, two board members of Stadtwerke Mainz AG, Detlev Höhne and Dr. Tobias Brosze, and Professor Dr. Detlev Reymann, President of RheinMain University, officially launched a hydrogen production plant at the Energiepark Mainz on July 2, 2015. With the support of the German Federal Ministry of Economics and Technology as part of the Energy Storage Funding Initiative the 17-million-project could be realized. The system, equipped with an electrolyzer from Siemens, will convert surplus electricity from wind farms to hydrogen from now on. In this way, it will be possible to store electricity from renewable sources over longer periods of time. With a peak rating of up to 6 megawatts the plant is the largest of its kind in the world.
The principle of electrolysis has been tried and tested for decades. What is special about the Mainz system is that it involves highly dynamic PEM high-pressure electrolysis which is particularly suitable for high current density and can react within milliseconds to sharp increases in power generation from wind and solar sources. In this electrolyzer a proton exchange membrane (PEM) separates the two electrodes at which oxygen and hydrogen are formed. On the front and back of the membrane are precious-metal electrodes that are connected to the positive and negative poles of the voltage source. This is where the water is split. The system in Mainz will thus have a capacity relevant for bottlenecks in the grid and small wind farms.