- Siemens to supply fluorine gas-free blue GIS medium-voltage switchgear to Liechtensteinische Kraftwerke (LKW)
- Climate-neutral insulation gas Clean Air replaces the greenhouse gas SF6 and dispenses with all other fluorinated gases
- Investment in climate protection and supply security in Liechtenstein
Liechtensteinische Kraftwerke
(LKW) has chosen sustainable medium-voltage switchgear from Siemens. The new
5-field NXPLUS C 24 system from the environmentally friendly blue GIS portfolio
of Siemens Smart Infrastructure was commissioned by the customer at the
Wiesengasse West substation in Schaan, Liechtenstein. This makes LKW one of the
first grid operators to convert an entire medium-voltage switchgear
installation to the climate-friendly insulating gas Clean Air.
- Global campus in Zug to reduce carbon footprint
- Target in line with company-wide sustainability program
Siemens Smart Infrastructure plans to transform its global headquarters in Zug, Switzerland, into a carbon neutral location by 2023. To achieve this, a comprehensive renovation of an existing building on Theilerstrasse 1c will commence in May 2021 for a period of two years. Siemens has earmarked around EUR 63 million (CHF 70 million) for the refurbishment works.
- Each level of the S-building is ventilated using a separate HVAC
system to ensure 100% fresh air
- This system helps the hospital to comply with more stringent energy
standards and ventilation requirements
- Lighting, air conditioning and access control are managed from a
single user-friendly interface using the Desigo CC system
- Technology ecosystem and energy equipment to provide optimum support
for healthcare personnel
Siemens has finished installing a
leading-edge HVAC system in the new S-building which has extended the A.S.Z.
(general city hospital) campus in Aalst, Belgium. The building technology
experts have also supplied the CCTV and access control systems. All air
conditioning, ventilation and security functions have been brought together in
the Siemens management system, Desigo CC. This makes it much easier to operate
for both healthcare personnel and patients, thereby providing more comfortable
rooms and reducing energy consumption at the same time. Siemens is therefore
helping the A.S.Z. in Aalst to meet the Belgian Supreme Council of Health's
increasingly stringent requirements and standards for energy efficiency in
buildings.
- EWE NETZ installs fluorine gas-free blue GIS medium-voltage switchgear from Siemens in Brake, Germany
- Investment in climate protection and supply security in the region
- Climate-friendly insulation gas “Clean Air” replaces fluorine gas
Siemens Smart
Infrastructure has supplied EWE NETZ GmbH, which operates highly-efficient power
grids in Germany, with its latest environmentally-friendly switchgear
technology. EWE NETZ has now completed a new medium-voltage switchgear
installation in Brake in the Wesermarsch region of Lower Saxony, which includes
seven fluorine gas-free NXPLUS C 24 circuit-breaker panels from Siemens’ green blue
GIS portfolio. This makes EWE NETZ one of the first grid operators in Germany
to switch to the climate-friendly insulation gas Clean Air for an entire
medium-voltage switchgear installation.
- Charging infrastructure for 14 new electric buses
- Fast charging units at three terminal stations
- Charging infrastructure and digital depot management solution at the bus depot
Siemens has been awarded a contract by Bernmobil, the Swiss capital’s public transport company, to supply charging infrastructure solutions for the operation of 14 new electric buses. These are to be deployed on Lines 19 and 21 beginning in early 2023. The project includes fast charging units at three terminal stations as well as charging infrastructure for the Eigerplatz bus depot. To optimize operations, a cloud-based depot management solution from Siemens will be used as software-as-a-service.
- Storage enabled intelligent microgrid concept to accelerate decarbonization and significantly increase renewables share
- Energy storage system enables greater energy independence
- Frequency regulation increases Madeira’s grid resilience
- Plant to provide blackstart capability to the 60 kV level
Siemens Smart
Infrastructure, in partnership with Fluence, are working to help the Portuguese
island of Madeira gain greater energy independence and grid resilience using
renewable energy. Madeira’s energy provider, Empresa de Electricidade da
Madeira (EEM), awarded a Siemens and Fluence consortium a contract to install a
22,5 MVA / 15,6 MVh battery storage plant which will be integrated into an
islanded microgrid concept.The project will enable
EEM to optimize its renewable energy integration, significantly contributing to
increasing the share of renewable power to around 50 percent in its energy mix.
As a result, the island can reduce its fuel consumption over the next two to
three years, while gaininggreater energy independencewithout
affecting energy quality or grid stability.
- Frame sizes 1,200 A, 1,600 A and 2,000 A
- Enhanced safety features
- Fully integrated communication and measurement features
- Smart features for planning and operation
Siemens has developed new, highly flexible
molded case circuit breaker (MCCB) frame sizes for high current applications to
perfectly address the needs of switchgear manufacturers and panel builders in
an environment, characterized by increasing complexity, digitalization, and
cost pressures. The new 3VA UL Large Frame MCCBs enable users to implement
powerful, safe, and smart systems while allowing them to improve and greatly
simplify their work processes. These 3VA UL Large Frame
MCCBs can be used worldwide. The 1,200 A and 1,600 A frame sizes meet the
requirements of IEC and UL standards. This is particularly advantageous for
manufacturers who are producing systems destined for global markets. The new 2,000
A frame is designed exclusively for the UL market. The new frame sizes will be available
in both thermal-magnetic and electronic trip unit versions. Molded case switch (MCS)
variants will also be offered.