Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens to build one of Europe’s largest shore power connections in Kiel

This photo shows the Ostseekai in Kiel. By the end of 2023, Ostuferhafen Kiel will be able to supply several passenger as well as cargo ships with shorepower simultaneously.

SEEHAFEN KIEL GmbH & Co. KG (PORT OF KIEL, Germany) has commissioned Siemens AG with the construction of two additional SIHARBOR shore power plants at Kiel’s Ostuferhafen. The construction project with a total investment value of approximately €17 million comprises a 50/60 Hz shore power plant for cruise ships and ferries and a 50 Hz shore power plant for ferries. It makes it possible to generate the electricity ships need while they are in port using renewable energies on shore instead of diesel generators on board. The new shore power connection will be one of the largest installations of its kind in Europe. After completion of the project at the end of 2023, the port of Kiel will be able to supply green power to six ships simultaneously at all of its major passenger, cargo and ferry terminals. 
“Connecting ships to shore power has enormous economic and environmental impact. Ships save expensive fuel, new business models open up for port operators, and port staff and residents benefit from a significant reduction in noise and pollution,” explained Markus Mildner, CEO of Siemens eMobility. For Siemens, the contract includes execution planning, delivery, assembly, cabling and commissioning of all plant and structural components required for the operation of the shore power plants, the necessary structural, civil and hydraulic engineering work, and overall commissioning of the system.

Cooperation with PORT OF KIEL enters next phase 

Siemens won the new contract following an EU-wide invitation to tender and a negotiation procedure with a preliminary qualification competition. “Siemens had already been a strong partner for us in an earlier shore power project. And once again, they submitted the most economical bid. We look forward to working with Siemens again,” said Dr. Dirk Claus, Managing Director of SEEHAFEN KIEL GmbH & Co. KG. The new shore power plant at Ostuferhafen continues the joint success story between Siemens and PORT OF KIEL: The existing shore power plants at Ostseekai and Schwedenkai as well as at Norwegenkai were also built by Siemens. 

Two plants with up to three supply options 

The construction project at Ostuferhafen includes two shore power plants able to supply up to three seagoing vessels simultaneously. The first of the two shore power plants is designed to supply up to two ferry or cruise ships and connects four berths at Ostuferhafen to shore power. It has a capacity of 16 MVA and can supply cruise ships and ferries with a frequency of 50 or 60 Hz and a voltage of 6.6 kV or 11 kV. The second shore power plant with a grid frequency of 50 Hz is designed exclusively for cargo and RoRo vessels and supplies two berths with a voltage of 6.6 kV or 11 kV, up to a maximum capacity of 5 MVA. 

Zero-emission future 

The expansion of the shore power infrastructure is one of the high-priority projects of PORT OF KIEL. It has long pursued a clear sustainability strategy aimed at becoming carbon neutral by 2030. In addition to its own transition to sustainable energy sources and innovative solutions for climate protection, the port also wants to use its shore power infrastructure to create incentives for shipping companies to save carbon emissions when their vessels are in port. “Shore power is a key part of our sustainability effort. Beginning in 2024/25, we hope to use our supply infrastructure for six ships to have around 80 percent of all ships plugged in while berthed,” Claus added. In addition to CO2 savings, connecting ships to shore power while they are at berth also results in a significant reduction in noise and pollution.

For this press release

Press Folders

Follow us on Twitter

Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2021, which ended on September 30, 2021, the Siemens Group generated revenue of €62.3 billion and net income of €6.7 billion. As of September 30, 2021, the company had around 303,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland. As of September 30, 2021, the business had around 70,400 employees worldwide.
Read more
Reference Number: HQSIPR202205246465EN

Contact

Christian S. Wilson

Siemens AG

+49 172 1385608

Julia Reichel

SEEHAFEN KIEL GmbH & Co. KG

+49 431 9822-104