Siemens Mobility to install a 2,000 km state-of-the-art high-speed rail network that will connect 60 cities throughout the country with trains that can operate up to 230 km/h. The integrated system will create the 6ᵗʰ largest high-speed rail network in the world, and will provide 90% of Egyptians access to a modern, safe, and affordable transportation system. The fully electrified network will cut carbon emissions by 70% compared to current car or bus transport, further supporting Egypt’s efforts in transforming its mobility to a more sustainable one. Siemens Mobility will deliver 41 Velaro high-speed trains, 94 Desiro High Capacity regional train sets, and 41 Vectron freight locomotives. This contract also includes the development of eight depots and yards and 15 years of maintenance.
Siemens Mobility's Vectron locomotives are used for both freight and passenger service. During the development of the locomotive, the focus was on providing a future-proof design, investment security, environmental compatibility, fungibility, retrofitting capability and convertibility. The Vectron can be delivered as a purely electrical version for operating with alternating current (AC) or direct current (DC) power systems as well as a multisystem (MS) variant in the power classes 5.2 MW, 5.6 MW and 6.4 MW. Along with the desired national train control system, the locomotives can also be equipped with the latest European Train Control System (ETCS). The locomotives are built in the Siemens Mobility plant in Munich-Allach, Germany. For freight transport in Germany, Siemens Mobility also offers the Smartron standard locomotive and the Vectron Dual Mode, a combination of diesel and electric locomotive.
Deutsche Bahn
(DB) and Siemens Mobility are driving forward the climate-friendly transition
in transport and are testing the use of hydrogen for rail for the first time.
The aim is to test a completely new overall system consisting of a newly
developed train and a newly designed filling station.
Siemens Mobility has signed a follow up order to deliver 43 Velaro MS
highspeed trains (ICE 3neo) for Deutsche Bahn. Together with a previous order
from 2020, this will grow their ICE 3neo fleet to a total of 73 trains. The
first trains will already start passenger service at the end of 2022.
Challenges and opportunities in the energy systems require a new smart, more adaptable grid infrastructure. Today, power grid operation is a complex task: Volatile power generation and multi-directional power flows from distributed, increasingly renewable sources and prosumers call for a smarter approach. With digital solutions that connect the physical and digital worlds we integrate intelligence across the energy value chain in systems and operations. We help connect grids, buildings, and industries enhancing efficiency and sustainability. We shape grids that are reliable and resilient, that integrate and manage renewables and that operate increasingly autonomous. These responsive grids support the sustainable energy transition, help provide affordable energy to society and our customers to stay competitive in an ever changing world. During Europe´s largest energy related trade show Enlit, which took place in Milan, Italy, Siemens presented its technological solutions to these challenges.
Cities account for roughly 80 percent of the energy consumed worldwide and generate roughly 75 percent of all carbon emissions. With more than two-thirds of the world’s population predicted to live in urban areas by 2050, cities are coming under increasing pressure. Digitally connected smart cities can help overcome some of the most pressing challenges of our time, including clean water, adequate waste removal as well as reduced pollution caused by buildings. The Expo 2020 Dubai site, with infrastructure connected by Siemens digital technology, provides a blueprint for smart cities globally. As the Premier Partner for Infrastructure Digitalization at Expo 2020 Dubai, Siemens has digitally linked more than 130 buildings at a purpose-built site twice the size of Monaco.
Deutsche Bahn (DB) and Siemens Mobility have
developed the world’s first train that operates by itself in rail traffic. Dr.
Richard Lutz, CEO of DB, and Dr. Roland Busch, CEO of Siemens AG, together with
Dr. Peter Tschentscher, Mayor of Hamburg, presented the train on the 11th
October 2021 as it made its premiere run as part of the Digital S-Bahn Hamburg
project.
Since
October 2019, Siemens Mobility and ViP (Verkehrsbetrieb Potsdam GmbH) have been
jointly researching a fully automated tram depot. One year before, the
cooperation partners presented a test vehicle of an autonomous tram at
InnoTrans 2018. On this basis, the consortium started further research together
with the Karlsruhe Institute of Technology (KIT), the Institute for Climate
Protection, Energy and Mobility (IKEM) and Codewerk GmbH. The market readiness
of the autonomous tram in the depot is planned for 2026.
The three-year project called “AStriD” (Autonomous Tram in Depot) is funded by the Federal Ministry for Transportation and Digital Infrastructure (BMVI) as part of its “Modernity Fund” (mFUND) research initiative.
- Siemens Mobility and the State of Bavaria reach an agreement on the deployment of a hydrogen train
- Order as part of a technology partnership for the further development of the Mireo Plus H platform
Siemens Mobility and the State of Bavaria sign a Memorandum of Understanding for the provision of a hydrogen train. The agreement is made within the framework of a technology partnership for the further development of the Mireo Plus H platform. The hydrogen-powered two-car train can run on non-electrified rail lines and has a range of up to 800 kilometers. The well-known Mireo Plus H platform is being used but is being equipped with a new generation of batteries to further improve both performance and passenger comfort. The vehicle will be presented to the public in spring 2022. First test runs in Bavaria are planned for 2023, before the train officially enters passenger service in January 2024.