- Siemens has supplied 200 VersiCharge wallboxes and an intelligent charging management system to the Portuguese Infinity building
- The contract includes SICAM Dynamic Load Management, a solution to use grid capacity in an efficient way
- Hardware and software are part of Siemens Xcelerator, an open digital business platform that enables customers to accelerate their digital transformation
Siemens Smart Infrastructure has supplied and installed 200 VersiCharge wallboxes and an intelligent charging management
system to the Infinity building, one of the tallest residential sites in
Lisbon, Portugal.
- Siemens Mobility founds subsidiary Smart Train
Lease GmbH
- Innovative rental model for Mireo Smart trains offers
fast and flexible adjustment of fleet capacity
- State-of-the-art battery, hydrogen, and
electric multiple-unit trains including maintenance
Siemens Mobility has
founded the subsidiary Smart Train Lease GmbH to enable customers to flexibly
supplement their fleets with rented state-of-the-art battery, hydrogen, and
electric multiple-unit trains. The Mireo Smart trains from Siemens Mobility are
available at short notice, approved for operation, and meet all required
standards for modern regional passenger transport. By providing preconfigured
trains and additional services such as maintenance, this new offer provides an
economical alternative for quickly and flexibly expanding fleets. It also
enables customers to easily test innovative and sustainable rail technologies. Smart
Train Lease GmbH is initially offering this rental model in Germany and plans
to expand it throughout Europe in the medium term.
- Italian distribution system operator (DSO), Areti, to use Siemens technology to forecast grid congestion and request flexibility on MV and LV grids
- Set of algorithms developed by Siemens for RomeFlex project enables the Roman DSO to use flexibility to make the grid smarter, more resilient and future-proof
- With the RomeFlex project, Areti and Siemens will build on the experience gained from the EU Platone project
Siemens and Roman DSO, Areti, have announced their collaboration on the
RomeFlex project, which starting today will test the ability to manage congestion and
voltage volatility across the stressed power grids of Italy's capital city.
- Enhancing proven machine learning capabilities with generative AI creates a robust, comprehensive predictive maintenance solution that leverages the strengths of both.
- Using a conversational user interface, manufacturers can take proactive actions easily, saving both time and resources.
- New generative AI functionality in Senseye Predictive Maintenance makes predictive maintenance conversational.
Siemens is releasing a new generative
artificial intelligence (AI) functionality into its predictive maintenance
solution – Senseye Predictive Maintenance. This advance makes predictive
maintenance more conversational and intuitive. Through this new release of
Senseye Predictive Maintenance with generative AI functionality, Siemens will
make human-machine interactions and predictive maintenance faster and more
efficient by enhancing proven machine learning capabilities with generative AI.
- Leading electric two-wheel scooter brand expands adoption of software from the Siemens Xcelerator portfolio to help reduce design iterations, cycle times and explore the future of sustainable electric mobility solutions for the Indian market
- Expanded adoption of Product Lifecycle Management (PLM) solutions from Siemens Xcelerator now includes product engineering, virtual simulation and physical test for all existing and new vehicle platforms
Siemens Digital
Industries Software announced today that Ather Energy, one of India’s
foremost electric motorcycle brands, has expanded its adoption of the Siemens Xcelerator portfolio of
industry software to help the company reduce its design and engineering cycle
time, improve product
quality and achieve faster time to market.
First call for 70 trains from the 2023
framework agreement
Order worth more than €800 million
Consistent development of the Mireo
platform
Austrian Federal Railways (ÖBB) has ordered the first 70
trains from the framework agreement won by Siemens Mobility at the end of
summer 2023. The trains will be delivered in three different versions from late
2027 onwards. The trains are a further development of the in Europe successfully
established and proven Mireo electric multiple-units. Designed to operate at
speeds up to 160 km/h, the Mireos offer numerous amenities for passengers,
including air conditioning, WiFi service, barrier-free access, electrical plugs,
racks for skis and snowboards, capacity for buggies and wheelchairs near the
doors as well as space for bicycles. The cars will be wider than on previous
Mireos trains to further enhance the passenger experience of ÖBB customers.
And, for the first time, Siemens Mobility is designing the new trains with
inner bearing bogies as a single car concept.
Today, Siemens
Mobility – in partnership with RATP and d’Île-de-France Mobilités – announced
completion of the full automation of Paris Metro Line 4, which is now operated
exclusively using automatic driverless trains. Following a period of mixed
operation during which driver-operated trains ran alongside the automatic
trains, full automation of Line 4 is now a reality. As a leader in the
design and implementation of automated metro systems, Siemens Mobility was
chosen by RATP at the end of 2015 to automate Line 4, three years after the
successful project to automate Line 1 at the end of 2012. With 700,000
passenger each day, Line 4 is the French capital’s second busiest metro line.
Opened in 1908, the route now has 29 stations spread over 14 kilometers.
- Decarbonization program targets significant energy savings and 50 percent CO2 reduction at over 15 HEINEKEN breweries and malt houses worldwide by 2025
- Supports HEINEKEN’s global Net Zero Production roadmap, which aims to reach net zero in Scope 1 and 2 by 2030 and net zero across the full value chain by 2040
- Five-year performance and monitoring service contract from Siemens to ensure ongoing project optimization
- Scalable solution designed using an energy digital twin will optimize heating and cooling requirements in production and packaging processes
HEINEKEN, the world's most international
brewer, has selected Siemens as a partner for its global Net Zero Production roadmap,
as part of HEINEKEN’s ambitions to reach net zero in Scopes 1 and 2 across all
production sites by 2030.*
- Siemens and Salesforce are collaborating to help manufacturers increase service efficiency and create new revenue streams
- Teamcenter Service Lifecycle Management (SLM) app connects Siemens’ leading Teamcenter Product Lifecycle Management (PLM) with Salesforce Manufacturing Cloud and Service Cloud, enabling integrated, cross discipline collaboration that drive digital transformation
- The new AI-based SaaS integration helps manufacturers build feedback loops between service execution and product development, enabling continuous innovation
Siemens Digital Industries Software announced today the new
Teamcenter® SLM app on Salesforce AppExchange. Developed by Siemens in collaboration with
Salesforce, the app connects product engineering and product service operations
by bringing together the Teamcenter Service Lifecycle Management solution from
the Siemens Xcelerator portfolio of industry software with Salesforce Manufacturing Cloud and Salesforce Service Cloud. This new app enables manufacturers to adopt more
service-centric business models, improve the customer experience and increase
service revenue.
- New V6 software generation with new functions like a single positioner to reduce the load of the controller, and EtherNet/IP to allow third-party controllers to be connected
- Simulation via DriveSim Advanced enables virtual commissioning in advance, ensuring drive process requirements are met efficiently and cost-effectively
- New hardware architecture with functional enhancements like a second encoder interface and 3C3 (H2S and SO2) coating increases precision and robustness
Siemens is innovating the well-established Sinamics S210 servo drive system with a new hardware architecture and new V6 software generation that expand the system's range of applications. The servo drive system is especially suitable for applications with high dynamics in the power range between 50 W and 7 kW: for example, machines for packaging, pick & place applications, and digital printing.