Siemens Gas and Power has entered into an
agreement with Total, a broad energy group, to advance new concepts for green liquified
natural gas (LNG) production. As part of the contract, Siemens Gas and Power is
conducting studies to explore a variety of possible
liquefaction and power generation plant designs, with the ultimate goal of decarbonizing
the production of LNG.
- Green hydrogen project launched in May 2020
- Decarbonizing a paper factory by modernizing an existing combined heat and power plant in France
With the HYFLEXPOWER project, a consortium made up of Engie Solutions, Siemens Gas and Power, Centrax, Arttic, German Aerospace Center (DLR) and four European universities are implementing a project funded by the European Commission under the Horizon 2020 Framework Program for Research and Innovation (Grant Agreement 884229). The implementation of this project, the world's very first industrial-scale power-to-X-to-power1 demonstrator with an advanced hydrogen turbine, will be launched at Smurfit Kappa PRF’s site - a company specialized in manufacturing recycled paper - in Saillat-sur-Vienne, France. The purpose of this project is to prove that hydrogen can be produced and stored from renewable electricity and then added with up to 100 percent to the natural gas currently used with combined heat and power plants. For this an existing Siemens SGT-400 industrial gas turbine will be upgraded to convert stored hydrogen into electricity and thermal energy.
The information contained herein is not for
publication or distribution, directly or indirectly, in or into Australia or
any other jurisdiction where to do so would be prohibited by applicable law.
- Siemens AG to spin off 55 percent of Siemens Energy to Siemens shareholders
- Plans call for further reducing Siemens’ stake significantly within 12 to 18 months after spin-off’s effective date
- Siemens AG contractually obligated to ensure Siemens Energy’s autonomy and independence
- Siemens Energy to have strong capital and liquidity base; solid investment-grade rating targeted
- Initial listing of new shares planned for September 28, 2020
Siemens AG has today published key details of the spin-off of its energy business, together with the invitation to the Extraordinary Shareholders’ Meeting on July 9, 2020. Issuance of the spin-off report marks another key milestone in the creation of an independent, world-leading energy pure play. Siemens shareholders are to automatically receive one share of Siemens Energy AG for every two shares of Siemens AG. Fifty-five percent of Siemens Energy will be spun off to Siemens shareholders. Depending on the strategic and operational development of the two companies, Siemens AG intends to further reduce its stake in Siemens Energy significantly within 12 to 18 months. In addition, Siemens has placed itself under a contractual obligation to refrain from exercising a controlling influence over the new company in the future. Subject to approval by the Extraordinary Shareholders’ Meeting, plans call for the spin-off to take place, as announced, by the end of September 2020. The initial listing is to take place on September 28th, 2020.
- Siemens Gas and Power to supply three 33-MW industrial gas turbines to Ascend’s Decatur, Alabama facility
- The project will enable the chemical materials manufacturer to increase operating efficiency and reduce its environmental footprint
Siemens Gas and Power was recently selected to provide three 33-megawatt (MW) SGT-700 industrial gas turbines, including a Long-Term Program (LTP), with Ascend Performance Materials’ nylon intermediate and specialty chemicals facility in Decatur, Alabama. This project will allow Ascend Performance Materials to retire assets that currently provide process steam for the facility. The shift to gas turbines for steam generation is part of Ascend’s long-term sustainability strategy to improve its environmental footprint and accelerate the growth of expanding its core businesses.
- Two SGT-400 gas turbine compression packages sold for U.S. pipeline service
Siemens Gas and Power was awarded a contract to supply two SGT-400 gas turbine compression packages for Midcoast Energy, LLC’s CJ Express pipeline expansion project in east Texas. WHC Energy Services, supported by Universal Pegasus International, will be the engineering, procurement and contracting (EPC) provider for the pipeline expansion project.
- Cooperation aims to test renewable fuels at the Rya CHP plant located in the energy port of Gothenburg
- First phase with Göteborg Energi is to validate 3D-printed burners at the Rya plant
By 2030, the ambition is that all district heating in Gothenburg, Sweden, will be produced by renewable or recovered energy sources. With this in mind Göteborg Energi and Siemens have come together in a cooperation agreement with the aim of testing state-of-the-art gas turbine technology that enables the operation of renewable fuels in the Rya combined heat and power (CHP) plant, which is today powered by natural gas.
- Digital solutions provide for improved operational efficiency and reduced emissions
Siemens will equip Lalitpur Power Generation Company Limited (LPGCL), a Bajaj Group company, with advanced digital solutions for its power plant located in Lalitpur, Uttar Pradesh, India.
- Gas turbine rotor exchange allows for increased output and efficiency
- Control system upgraded to latest version of SPPA-T3000
The Dunamenti Power Plant in Százhalombatta, Hungary, is the largest gas-fired power plant in the country with a capacity of 794 megawatts (MW), making it a major source of reliable electricity in Hungary. Recently, in collaboration with the customer and plant owner, MET Asset Management AG, and within the scope of an overhaul project, Siemens Gas and Power replaced the entire rotor of the plant's SGT5-2000E gas turbine and installed a new, state-of-the-art SPPA-T3000 control system.
- First order from Asia for HL-class gas turbine
- New power plant with a capacity of more than one gigawatt
- Efficiency rating of more than 63 percent
Siemens will set up a high-efficiency HL-class power island for a new combined cycle power plant (CCPP) in South Korea. This will be the first two state-of-the-art HL-class gas turbines that Siemens will supply to a customer in Asia. The new plant, which will be built in Yeoju, in South Korea’s Gyeonggi Province, will run on regasified liquefied natural gas (LNG) and offer a generating capacity of more than one gigawatt. With a maximum efficiency rating of more than 63 percent the gas turbine will allow the power station to get the most out of the valuable LNG for electricity generation, enabling especially economical and environmentally friendly operation. The customer is South Korean EPC SK Engineering & Construction Co., Ltd., which is constructing the entire plant for the independent power producer Yeoju Energy Services.
- Power plants Termoeléctrica del Sur, de Warnes, and Entre Ríos inaugurated in August and September
- Upgrade to combined cycle power plants increase the generation capacity by one gigawatt
- Expansion provides reliable energy supply and will allow export of value-added products
With the official inauguration of the Termoeléctrica de Warnes power plant in mid-September, all three power plants in Bolivia were inaugurated within a few weeks in August and September. Since the contract signing in 2016, Siemens has expanded Bolivia’s three largest thermal power plants to efficient combined cycle mode. The power plants are owned and operated by Ende Andina SAM. Together, all three add more than one gigawatt of electrical power to its current maximum capacity and to the Bolivian national grid.