- Digitalization and automation solutions provide companies in discrete and process industries with the necessary flexibility for new conditions
- The Digital Enterprise Virtual Summit showcased concrete and future-oriented solutions
- The Digital Enterprise Virtual Summit had around 12,000 registrations from Customers and Partners with already 6,300 live attendees on the day of the event
The current situation creates major challenges for industrial companies worldwide – and shows that digitalized and highly automated production is more important than ever when it comes to gaining a competitive edge. This is the only way that companies can react to current and future challenges with the required degree of flexibility. Successful solutions were presented at the Digital Enterprise Virtual Summit by Siemens on July 16. As part of the conference, representatives from numerous companies from the discrete and process industries discussed strategies and technologies for future success under these new conditions. The focus was on topics such as the horizontal and vertical integration of the value chain with simulation and optimization from product creation through to servicing and from field level to the cloud. Other topics included online and remote solutions as well as edge and cloud computing, additive manufacturing, industrial 5G and artificial intelligence. The Digital Enterprise Virtual Summit had around 12,000 registrations from Customers and Partners with already 6,300 live attendees on the day of the event. The Summit is now also available to be viewed on demand at http://www.siemens.com/digital-enterprise-summit.
- Improvement of machine tool availability through predictive maintenance with Analyze MyMachine /Condition
- Analyze MyMachine /Condition for Sinumerik Edge creates a mechanical fingerprint of the machine tool
- Condition evaluation, analysis and comparison of all connected machines using the Mindsphere application
Siemens is extending its edge application Analyze MyMachine /Condition with a corresponding Mindsphere application and thus demonstrating how edge computing and cloud computing can be intelligently combined. The Sinumerik Edge Application Analyze MyMachine /Condition, which the company presented last year at the EMO, uses high-frequency CNC data to create the mechanical fingerprint of a machine tool. In the application, users can capture and evaluate various parameters such as stiffness, friction, and backlash in the individual axes with the help of flexibly configurable measurement series. The measurement results can then be visualized and compared with reference data.
- Sinumerik One Dynamics - three technology packages to increase the efficiency of CNC users when programming in the shopfloor and executing CAM-generated CNC programs
- Top Surface and Top Speed Plus for excellent motion control and perfect workpiece surfaces
With the software version NCU-SW 6.14, Siemens is launching three powerful technology packages exclusively for the CNC Sinumerik One. The Sinumerik One Dynamics packages are available in three different packages: One Dynamics Operate, One Dynamics 3-axis milling and One Dynamics 5-axis milling. The software functions contained in the technology packages support users from machine-oriented programming in the jobshop to high-performance machining of CAD-CAM-programmed workpieces with high surface quality.
- Simotics S-1FS2 in stainless steel housing with specific features for use in the pharmaceutical and F&B industries
- Servo planetary gearmotors Simotics S-1FK2 for optimum adjustment of speed, torque and mass inertia
- Simotics S-1FT2 in protection class IP67 with 26 bit encoder, higher rated speed and other selectable features
Siemens is adding new servo motors to its proven Sinamics S210 single-cable servo drive system, thereby expanding its range of applications. Specifically, for use in the pharmaceutical and food industries, the company is launching the Simotics S-1FS2, a motor version with a stainless-steel housing, the highest degree of protection IP67/IP69, and high-resolution 22-bit absolute multiturn encoders. The servo motor thus meets all hygienic conditions and can be used for mixing and stirring, air conditioning and ventilating, dosing and filling, as well as conveying, packaging and storing a wide variety of end products in the food and beverage sector and in the pharmaceutical industry.
- New software for omnidirectional control
- 360-degree freedom of movement for AGVs
- Innovative steering system implemented with ebm-papst
Siemens has expanded Simove, the scalable automation solution for Automated Guided Vehicle (AGV)
applications, to include functionality for omnidirectional control. The new software supports unrestricted freedom of movement for AGVs. Together with Simatic
Micro-Drive, the new member of the Siemens converter family specifically for
the safety extra-low voltage range, plant and machine builders can create universal
and flexible systems. Together with partner ebm-papst an initial application example has been realized: a steering system that uses Simatic Micro-Drive,
the universal Simatic controller and the new control software from Simove. The
compact steering system features a special gearbox where the speeds of both
motors in the steering system are overlaid. This means that the steering system
does not require moving cables. The result is 360-degree rotational movement of
the wheel and therefore of the system. In addition, the high transmission in the
driving and steering direction provides a high level of control accuracy for
the system. Thanks to the integrated safety functions of the Simatic Micro-Drive,
safe control and monitoring of the integrated motors is ensured at all times.
- Eight desalination plants with process automation, drive technology, process instrumentation and communication technology
- Total capacity of 240,000 cubic meters per day
- Order volume is a double-digit million Euro figure
Siemens has received a follow-up order from the A3C consortium (Rawafid Industrial, Advanced Water Technology, SETE and Al Fatah) to equip eight seawater desalination plants in Saudi Arabia with electrical equipment. The new plants for seawater desalination using the principle of reverse osmosis are spread along the West coast of Saudi Arabia. The total capacity of the plants will be 240,000 cubic meters per day, with a power consumption of just three kilowatts per cubic meter of produced water, which is below the usual value and will provide significant energy savings. The scope of supply from Siemens includes hardware and software engineering, power distribution, PCS7 automation, medium and low voltage converters, Industrial Ethernet communication technology and process instrumentation for eight reverse osmosis plants, plus plant commissioning. The project will follow a tight schedule, with commissioning planned from autumn 2019.
- New “Location Intelligence” software expands Simatic RTLS locating platform to include digital twin of performance
- Visualized real-time analyses create potential for optimization and facilitate rapid decision-making
- Provides customers with overview of material flow and order information
Siemens introduces new “Location Intelligence” software, which expands the Simatic RTLS (Real-Time Locating System) locating platform to include the digital twin of performance. The web-based software analyzes and visualizes dynamic data, processes events, and can be addressed directly from local ERP (Enterprise Resource Planning) or MES (Manufacturing Execution System) systems. The intelligence acquired based on position data provides the user with a comprehensive overview of material flow, order information or possible problem areas.
- Siemens presents liquid-cooled, robust power conversion system based on proven Sinamics S120 platform
- Grid converter comes with certification in accordance to VDE-AR-N 4110 and with validated simulation model for easy project planning, optimization and integration into the power grid
With Sinamics PCS, Siemens presents a new power conversion system for battery storage applications. The Sinamics PCS grid converter makes locally generated battery power usable for industrial and public power grids. Sinamics PCS controls the charging and discharging process of the battery and helps to handle load peaks and grid disturbances via the battery storage, to store the electricity in an energy- and cost-efficient manner and to bring the energy stored in batteries efficiently and reliably into the grid.
- Siemens drives forward digital transformation in the machine tool industry with a brand new Sinumerik generation
- Sinumerik ONE enables seamless interaction between virtual and real world for significantly increased productivity in the production and use of machine tools
- Scalable CNC-portfolio for highest performance requirements and optimum surface quality
With Sinumerik ONE, the first digital native CNC, Siemens is driving forward digital transformation in the machine tool industry. The new controller works with software to create the machine controller and associated digital twin from one engineering system and thus contributes to the seamless integration of hardware and software. Thanks to its seamless interaction between virtual and real world as well as high-performance hardware, Sinumerik ONE is setting new standards in terms of productivity, performance and digitalization. It is the future-proof CNC for machine tools in the increasingly digital world of manufacturing. Both machine manufacturers and machine operators benefit from the universal digital twin for the product, production and performance.
Control rooms of process engineering plants are usually
as old as the plant itself, often 30 years and more. Today, digital
transformation is placing new demands on automation: Simatic PCS neo is a brand-new system software, which
offers companies in the process industry unique opportunities in the age of
digitalization. Main features include global web-based collaboration in
engineering and operation and intuitive handling representing all relevant
information in a single workbench.